<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1062 only ROM boot loader works no RAM program run with sdphost USB in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1062-only-ROM-boot-loader-works-no-RAM-program-run-with/m-p/2146876#M34891</link>
    <description>&lt;P&gt;I have struggle several days to get my custom design&amp;nbsp;MIMXRT1062DVJ6B MCU to do its fisrt program run. Unfortunately the only thing how works is the ROM boor loader response and the RAM load. I have try several ways through use the and I show 2 different cases here&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/tree/main/failure_start_RAM_at_blank_MIMXRT1062" target="_blank"&gt;https://github.com/ollewelin/delta_robot/tree/main/failure_start_RAM_at_blank_MIMXRT1062&lt;/A&gt;&lt;BR /&gt;For my hardware here:&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/SCH_3x_motor_driver_V2_1.pdf" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/SCH_3x_motor_driver_V2_1.pdf&lt;/A&gt;&lt;BR /&gt;The first test was a Minimal loop.bin file I try to load to 0x20000000&lt;BR /&gt;The program should only setup a stackpointer and a resetvector then the next instruction is to loop to itself&lt;BR /&gt;see log&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/loop_log.txt" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/loop_log.txt&lt;/A&gt;&lt;BR /&gt;The end up failure responde:&lt;BR /&gt;sdphost -u 0x1fc9,0x0135 -- error-status&lt;BR /&gt;Status (HAB mode) = 1450735702 (0x56787856) Hab Is Disabled (Unlocked).&lt;BR /&gt;Response status = 858993459 (0x33333333) NO DESCRIPTION.&lt;BR /&gt;The other example was a blinky test made by MCUXpresso IDE generated this&lt;BR /&gt;evkbmimxrt1060_iled_blinky_iled_blinky.map at&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/evkbmimxrt1060_iled_blinky_iled_blinky.map" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/evkbmimxrt1060_iled_blinky_iled_blinky.map&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And the memory setup log here:&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/MIMXRT1062xxxxB_part.xml" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/MIMXRT1062xxxxB_part.xml&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Same sad response this try as many other setup I tried a week now&lt;/P&gt;&lt;P&gt;sdphost -u 0x1fc9,0x0135 -- error-status&lt;BR /&gt;Status (HAB mode) = 1450735702 (0x56787856) Hab Is Disabled (Unlocked).&lt;BR /&gt;Response status = 858993459 (0x33333333) NO DESCRIPTION.&lt;BR /&gt;See log&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/Log_test_evkbmimxrt1060_iled_blinky_iled_blinky.txt" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/Log_test_evkbmimxrt1060_iled_blinky_iled_blinky.txt&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;This is my last try to get some help then I through out this and go for other hardware chip instead. Best Regards Olle Welin&lt;BR /&gt;olle2welin@yahoo.com&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Aug 2025 11:46:18 GMT</pubDate>
    <dc:creator>OlleWelin</dc:creator>
    <dc:date>2025-08-05T11:46:18Z</dc:date>
    <item>
      <title>MIMXRT1062 only ROM boot loader works no RAM program run with sdphost USB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1062-only-ROM-boot-loader-works-no-RAM-program-run-with/m-p/2146876#M34891</link>
      <description>&lt;P&gt;I have struggle several days to get my custom design&amp;nbsp;MIMXRT1062DVJ6B MCU to do its fisrt program run. Unfortunately the only thing how works is the ROM boor loader response and the RAM load. I have try several ways through use the and I show 2 different cases here&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/tree/main/failure_start_RAM_at_blank_MIMXRT1062" target="_blank"&gt;https://github.com/ollewelin/delta_robot/tree/main/failure_start_RAM_at_blank_MIMXRT1062&lt;/A&gt;&lt;BR /&gt;For my hardware here:&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/SCH_3x_motor_driver_V2_1.pdf" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/SCH_3x_motor_driver_V2_1.pdf&lt;/A&gt;&lt;BR /&gt;The first test was a Minimal loop.bin file I try to load to 0x20000000&lt;BR /&gt;The program should only setup a stackpointer and a resetvector then the next instruction is to loop to itself&lt;BR /&gt;see log&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/loop_log.txt" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/loop_log.txt&lt;/A&gt;&lt;BR /&gt;The end up failure responde:&lt;BR /&gt;sdphost -u 0x1fc9,0x0135 -- error-status&lt;BR /&gt;Status (HAB mode) = 1450735702 (0x56787856) Hab Is Disabled (Unlocked).&lt;BR /&gt;Response status = 858993459 (0x33333333) NO DESCRIPTION.&lt;BR /&gt;The other example was a blinky test made by MCUXpresso IDE generated this&lt;BR /&gt;evkbmimxrt1060_iled_blinky_iled_blinky.map at&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/evkbmimxrt1060_iled_blinky_iled_blinky.map" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/evkbmimxrt1060_iled_blinky_iled_blinky.map&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And the memory setup log here:&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/MIMXRT1062xxxxB_part.xml" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/MIMXRT1062xxxxB_part.xml&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Same sad response this try as many other setup I tried a week now&lt;/P&gt;&lt;P&gt;sdphost -u 0x1fc9,0x0135 -- error-status&lt;BR /&gt;Status (HAB mode) = 1450735702 (0x56787856) Hab Is Disabled (Unlocked).&lt;BR /&gt;Response status = 858993459 (0x33333333) NO DESCRIPTION.&lt;BR /&gt;See log&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&lt;A href="https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/Log_test_evkbmimxrt1060_iled_blinky_iled_blinky.txt" target="_blank"&gt;https://github.com/ollewelin/delta_robot/blob/main/failure_start_RAM_at_blank_MIMXRT1062/Log_test_evkbmimxrt1060_iled_blinky_iled_blinky.txt&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;This is my last try to get some help then I through out this and go for other hardware chip instead. Best Regards Olle Welin&lt;BR /&gt;olle2welin@yahoo.com&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Aug 2025 11:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1062-only-ROM-boot-loader-works-no-RAM-program-run-with/m-p/2146876#M34891</guid>
      <dc:creator>OlleWelin</dc:creator>
      <dc:date>2025-08-05T11:46:18Z</dc:date>
    </item>
  </channel>
</rss>