<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Example Code for USB Data Transfer with DMA on MIMXRT1040</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-Code-for-USB-Data-Transfer-with-DMA-on-MIMXRT1040/m-p/2128781#M34642</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245206"&gt;@akash347&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have any examples that implement the USB stack integrated with DMA. As mentioned in the following &lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT106x-USB-DMA-Scatter-Gather/m-p/2013041" target="_self"&gt;community post&lt;/A&gt;, we have examples for both DMA and USB separately, and the integration would have to be done by the developer.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Fri, 04 Jul 2025 20:23:31 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2025-07-04T20:23:31Z</dc:date>
    <item>
      <title>Example Code for USB Data Transfer with DMA on MIMXRT1040</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-Code-for-USB-Data-Transfer-with-DMA-on-MIMXRT1040/m-p/2128647#M34639</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working on USB communication using the MIMXRT1040 and would like to implement data transfer using DMA for better throughput. I've gone through the SDK examples, but I couldn't find a dedicated example showcasing USB with DMA integration.&lt;/P&gt;&lt;P&gt;Could you please let me know if:&lt;/P&gt;&lt;P&gt;There are any existing example codes for USB data transfer using DMA on the MIMXRT1040?&lt;/P&gt;&lt;P&gt;If not, can such an example be made available or shared?&lt;/P&gt;&lt;P&gt;Any guidance or pointers to documentation/resources would also be highly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jul 2025 11:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-Code-for-USB-Data-Transfer-with-DMA-on-MIMXRT1040/m-p/2128647#M34639</guid>
      <dc:creator>akash347</dc:creator>
      <dc:date>2025-07-04T11:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: Example Code for USB Data Transfer with DMA on MIMXRT1040</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-Code-for-USB-Data-Transfer-with-DMA-on-MIMXRT1040/m-p/2128781#M34642</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245206"&gt;@akash347&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have any examples that implement the USB stack integrated with DMA. As mentioned in the following &lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT106x-USB-DMA-Scatter-Gather/m-p/2013041" target="_self"&gt;community post&lt;/A&gt;, we have examples for both DMA and USB separately, and the integration would have to be done by the developer.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jul 2025 20:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-Code-for-USB-Data-Transfer-with-DMA-on-MIMXRT1040/m-p/2128781#M34642</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-07-04T20:23:31Z</dc:date>
    </item>
  </channel>
</rss>