<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT600 FlexSPI extra clk when reading using LoopbackFromSckPad or DQS</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2128692#M34640</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I'm facing the exact same problem. When reading 32bit from FPGA over QSPI. It works using the "kFLEXSPI_ReadSampleClkLoopbackInternally" read strobe. The LUT entry is the following:&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 12 /* bits */&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 1 /* cycles */&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 4 /* bytes */&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0&lt;BR /&gt;&lt;BR /&gt;It writes the 12bit address: 3*4bits, then 1*4bits of dummy cycle, following with 32bit = 8*4bit read data.&lt;BR /&gt;This is a sum of 3+1+8=12 SCK clocks in SDR mode&lt;BR /&gt;&lt;BR /&gt;When enabling "&lt;STRONG&gt;kFLEXSPI_ReadSampleClkExternalInputFromDqsPad&lt;/STRONG&gt;" an additional 6 SCK clocks are appended after the read data clocks and before CS is asserted high. The read data is valid, but we lose 50% of our throughput.&lt;BR /&gt;&lt;BR /&gt;Is there any solution to this problem?&lt;/P&gt;</description>
    <pubDate>Fri, 04 Jul 2025 13:50:43 GMT</pubDate>
    <dc:creator>stollg</dc:creator>
    <dc:date>2025-07-04T13:50:43Z</dc:date>
    <item>
      <title>RT600 FlexSPI extra clk when reading using LoopbackFromSckPad or DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2045627#M33489</link>
      <description>&lt;P&gt;Running example&amp;nbsp;evkmimxrt685_flexspi_octal_polling_transfer, on EVK685&lt;BR /&gt;Running from RAM, semihost for debug.&lt;BR /&gt;&lt;BR /&gt;When running command Read Jedec ID, opcode 0x9F in SPI 1-1-1 for read 3 bytes,&lt;BR /&gt;when using kFLEXSPI_ReadSampleClkLoopbackFromSckPad or&amp;nbsp;kFLEXSPI_ReadSampleClkExternalInputFromDqsPad, extra byte is read, while when using&amp;nbsp;kFLEXSPI_ReadSampleClkLoopbackInternally, only requested 3 bytes are read.&lt;BR /&gt;&lt;BR /&gt;see attached logic capture, and source code:&lt;BR /&gt;&lt;BR /&gt;kFLEXSPI_ReadSampleClkLoopbackFromSckPad, 4 bytes are read, while requesting only 3:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RD_Jedec_ID_src_clk_from_pad_option_0x2.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/324332i22670DFC56F395EF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RD_Jedec_ID_src_clk_from_pad_option_0x2.PNG" alt="RD_Jedec_ID_src_clk_from_pad_option_0x2.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RD_Jedec_ID_src_clk_from_pad_option_0x2.PNG&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;kFLEXSPI_ReadSampleClkLoopbackInternally, only 3 bytes are read:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RD_Jedec_ID_src_clk_internally.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/324333iDAC923309D8C239A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RD_Jedec_ID_src_clk_internally.PNG" alt="RD_Jedec_ID_src_clk_internally.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RD_Jedec_ID_src_clk_internally.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;  &lt;/P&gt;</description>
      <pubDate>Mon, 17 Feb 2025 15:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2045627#M33489</guid>
      <dc:creator>DanielNis</dc:creator>
      <dc:date>2025-02-17T15:44:02Z</dc:date>
    </item>
    <item>
      <title>Re: RT600 FlexSPI extra clk when reading using LoopbackFromSckPad or DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2045628#M33490</link>
      <description />
      <pubDate>Mon, 17 Feb 2025 15:44:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2045628#M33490</guid>
      <dc:creator>DanielNis</dc:creator>
      <dc:date>2025-02-17T15:44:31Z</dc:date>
    </item>
    <item>
      <title>Re: RT600 FlexSPI extra clk when reading using LoopbackFromSckPad or DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2045629#M33491</link>
      <description />
      <pubDate>Mon, 17 Feb 2025 15:44:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2045629#M33491</guid>
      <dc:creator>DanielNis</dc:creator>
      <dc:date>2025-02-17T15:44:47Z</dc:date>
    </item>
    <item>
      <title>Re: RT600 FlexSPI extra clk when reading using LoopbackFromSckPad or DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2080256#M34009</link>
      <description>&lt;P&gt;Verify that the ROM API and LUT (Lookup Table) configurations are correct. The LUT entries should match the expected command sequences for your flash memory.&lt;BR /&gt;The extra read might be dummy cycles from the LUT.&lt;/P&gt;
&lt;P&gt;On the configuration on the&amp;nbsp;&lt;SPAN&gt;kFLEXSPI_ReadSampleClkExternalInputFromDqsPad the device expects external DQS signal provided from the memory so if it is not supplied then errors on the comunication is expected.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Omar&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Apr 2025 23:27:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2080256#M34009</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-04-14T23:27:48Z</dc:date>
    </item>
    <item>
      <title>Re: RT600 FlexSPI extra clk when reading using LoopbackFromSckPad or DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2128692#M34640</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I'm facing the exact same problem. When reading 32bit from FPGA over QSPI. It works using the "kFLEXSPI_ReadSampleClkLoopbackInternally" read strobe. The LUT entry is the following:&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 12 /* bits */&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 1 /* cycles */&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 4 /* bytes */&lt;BR /&gt;&amp;nbsp;- kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0&lt;BR /&gt;&lt;BR /&gt;It writes the 12bit address: 3*4bits, then 1*4bits of dummy cycle, following with 32bit = 8*4bit read data.&lt;BR /&gt;This is a sum of 3+1+8=12 SCK clocks in SDR mode&lt;BR /&gt;&lt;BR /&gt;When enabling "&lt;STRONG&gt;kFLEXSPI_ReadSampleClkExternalInputFromDqsPad&lt;/STRONG&gt;" an additional 6 SCK clocks are appended after the read data clocks and before CS is asserted high. The read data is valid, but we lose 50% of our throughput.&lt;BR /&gt;&lt;BR /&gt;Is there any solution to this problem?&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jul 2025 13:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2128692#M34640</guid>
      <dc:creator>stollg</dc:creator>
      <dc:date>2025-07-04T13:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: RT600 FlexSPI extra clk when reading using LoopbackFromSckPad or DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2135212#M34728</link>
      <description>&lt;P&gt;Hi Omar,&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LUT match expected operands and sequence.&lt;BR /&gt;&lt;/SPAN&gt;Your answer doesn't explain why on using RT685EVK with FlexSPI example, setting&amp;nbsp;&lt;BR /&gt;#define EXAMPLE_FLEXSPI_RX_SAMPLE_CLOCK kFLEXSPI_ReadSampleClkLoopbackInternally&lt;/P&gt;&lt;P&gt;or:&lt;BR /&gt;#define EXAMPLE_FLEXSPI_RX_SAMPLE_CLOCK kFLEXSPI_ReadSampleClkLoopbackFromSckPad&lt;BR /&gt;&lt;BR /&gt;with same operation sequence,&amp;nbsp;&lt;BR /&gt;with&amp;nbsp;ClkLoopbackFromSckPad settings, we are getting extra 8 clocks, which is the failure,&lt;BR /&gt;and with&amp;nbsp;ClkLoopbackInternally settings, clock count is as expected.&lt;BR /&gt;&lt;BR /&gt;see attached pictures, and zip files with source code using&amp;nbsp;evkmimxrt685_flexspi_octal_polling_transfer_cm33 example.&lt;BR /&gt;&lt;BR /&gt;Please escalate this issue to R&amp;amp;D.&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LUT_status" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/347911iB13F0DA1A973076F/image-size/large?v=v2&amp;amp;px=999" role="button" title="LUT_status.PNG" alt="LUT_status" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;LUT_status&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Src_Clk_LoopbackFromSckPad" style="width: 741px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/347909i06C6B0B082892318/image-size/large?v=v2&amp;amp;px=999" role="button" title="ReadJedecID_SPI_1s_1s_1s_RT685EVK_Src_Clk_LoopbackFromSckPad.PNG" alt="Src_Clk_LoopbackFromSckPad" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Src_Clk_LoopbackFromSckPad&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Src_Clk_internally" style="width: 681px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/347910i30AB064037C6F398/image-size/large?v=v2&amp;amp;px=999" role="button" title="ReadJedecID_SPI_1s_1s_1s_RT685EVK_Src_Clk_internally.PNG" alt="Src_Clk_internally" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Src_Clk_internally&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Dan&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 19:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT600-FlexSPI-extra-clk-when-reading-using-LoopbackFromSckPad-or/m-p/2135212#M34728</guid>
      <dc:creator>DanielNis</dc:creator>
      <dc:date>2025-07-16T19:24:14Z</dc:date>
    </item>
  </channel>
</rss>