<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: question about the wifi_nxp middleware... in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2126935#M34621</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please see below comments from my side.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Middleware should be same if you use the same version SDK(e.g 25.03) for both RT1060 and RT1170, please check with the same baseline, it should be workable.&lt;/LI&gt;
&lt;LI&gt;It is very certain that there has been a major version update from 2.16 to 25.03, the latest one is more mature.&lt;/LI&gt;
&lt;/UL&gt;</description>
    <pubDate>Wed, 02 Jul 2025 06:51:05 GMT</pubDate>
    <dc:creator>Sam_Gao</dc:creator>
    <dc:date>2025-07-02T06:51:05Z</dc:date>
    <item>
      <title>question about the wifi_nxp middleware...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2125000#M34591</link>
      <description>&lt;P&gt;I am working with the MIMXRT1060EVK and MIMXRT1170EVKB, running with&amp;nbsp;SDK_2_16_000_EVK-MIMXRT1060 and&amp;nbsp;SDK_25_03_00_MIMXRT1170-EVKB.&amp;nbsp; For both of these boards I am using the same SDIO-based WiFi modem, but I see significant differences between the two directories.&lt;/P&gt;&lt;P&gt;I realize they are different SOCs (1060 vs 1170) but fundamentally the code at the wifi_nxp level should (AFAIK) be the same.&amp;nbsp; There are significant differences, and it appears to me that the code under the 1170 tree is more mature than that of the 1060 tree.&amp;nbsp; Can someone explain why they are so different?&amp;nbsp; Is the 1060 SDK just not as up-to-date as the 1170 tree?&lt;/P&gt;&lt;P&gt;I ask because if it is at all possible, I'd like to not have to use two different source trees for the same WiFi functionality.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone from NXP support explain this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 21:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2125000#M34591</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2025-06-27T21:36:31Z</dc:date>
    </item>
    <item>
      <title>Re: question about the wifi_nxp middleware...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2125823#M34603</link>
      <description>Can someone from NXP comment on this?&lt;BR /&gt;I guess the question is: can I use the wifi_nxp middleware and work it to run with the iMXRT1060?</description>
      <pubDate>Mon, 30 Jun 2025 18:34:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2125823#M34603</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2025-06-30T18:34:45Z</dc:date>
    </item>
    <item>
      <title>Re: question about the wifi_nxp middleware...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2126935#M34621</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please see below comments from my side.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Middleware should be same if you use the same version SDK(e.g 25.03) for both RT1060 and RT1170, please check with the same baseline, it should be workable.&lt;/LI&gt;
&lt;LI&gt;It is very certain that there has been a major version update from 2.16 to 25.03, the latest one is more mature.&lt;/LI&gt;
&lt;/UL&gt;</description>
      <pubDate>Wed, 02 Jul 2025 06:51:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2126935#M34621</guid>
      <dc:creator>Sam_Gao</dc:creator>
      <dc:date>2025-07-02T06:51:05Z</dc:date>
    </item>
    <item>
      <title>Re: question about the wifi_nxp middleware...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2127321#M34623</link>
      <description>&lt;P&gt;Great news!&amp;nbsp; Thanks for responding...&lt;/P&gt;&lt;P&gt;So, when I attempt to build the latest SDK for the 1060 (actually for the EVK-MIMXRT1060), the latest available version is 2.16.00. So what is my best approach?&amp;nbsp; Will the SDK builder somehow build newer versions or should I just attempt to use the wifi_nxp directory from the 1170 when building for the 1060?&lt;/P&gt;&lt;P&gt;Thanks much for responding!!&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 14:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2127321#M34623</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2025-07-02T14:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: question about the wifi_nxp middleware...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2127341#M34624</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233161"&gt;@Sam_Gao&lt;/a&gt;&amp;nbsp; I just took a shot at rebuilding my 1060 code (from SDK2.16) with the 1170's (SDK25.03) middleware/wifi_nxp.&amp;nbsp; I had to make a few small adjustments, but so far (only 10 minutes into my test run), it appears to be working.&amp;nbsp; So far so good...&lt;/P&gt;&lt;P&gt;Thanks much,&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 14:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2127341#M34624</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2025-07-02T14:52:44Z</dc:date>
    </item>
    <item>
      <title>Re: question about the wifi_nxp middleware...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2129212#M34651</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It depends on actual SW/HW and your requirment.&lt;/P&gt;
&lt;P&gt;Yes. It only supports SDK2.16.0 if you select 'RT1060-EVK' board, but you will get a newer version if you have 'RT1060-EVK&lt;STRONG&gt;B&lt;/STRONG&gt;'.&amp;nbsp;The SDK version is related to the Hardware.&lt;/P&gt;
&lt;P&gt;You can use the latest SDK and port them into the hardware RT1060-EVK.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 09:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2129212#M34651</guid>
      <dc:creator>Sam_Gao</dc:creator>
      <dc:date>2025-07-07T09:37:27Z</dc:date>
    </item>
    <item>
      <title>Re: question about the wifi_nxp middleware...</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2129483#M34659</link>
      <description>Ok, I didn't realize there was a 'B' version for that board. Regardless (referring to my last post), I was able to use the latest wifi_nxp with my older 1060 SDK. Thanks!</description>
      <pubDate>Mon, 07 Jul 2025 17:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/question-about-the-wifi-nxp-middleware/m-p/2129483#M34659</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2025-07-07T17:48:44Z</dc:date>
    </item>
  </channel>
</rss>