<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックOpenH264 Decoding Performance Issue on MIMXRT1176 with RTSP IP Camera</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OpenH264-Decoding-Performance-Issue-on-MIMXRT1176-with-RTSP-IP/m-p/2122888#M34561</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the MIMXRT1176 controller to receive H.264 video data over Ethernet from an IP camera via RTSP. The camera is configured to stream at 4 fps with a resolution of 352×240.&lt;/P&gt;&lt;P&gt;I’m using the OpenH264 decoder to decode the H.264 stream. However, I observe that decoding is significantly slower — the display frame rate is only around 1 fps, even though the camera is sending 4 fps.&lt;/P&gt;&lt;P&gt;I’ve confirmed that frames are being received correctly over RTSP using the LIVE555 stack.&lt;/P&gt;&lt;P&gt;How can I improve the H.264 decoding performance using OpenH264 on the RT1176? Is there any optimization suggestion, or are there known limitations?&lt;/P&gt;&lt;P&gt;Any suggestions or best practices would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Pavanakumar A. G.&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jun 2025 07:29:36 GMT</pubDate>
    <dc:creator>Pavankumar1</dc:creator>
    <dc:date>2025-06-25T07:29:36Z</dc:date>
    <item>
      <title>OpenH264 Decoding Performance Issue on MIMXRT1176 with RTSP IP Camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OpenH264-Decoding-Performance-Issue-on-MIMXRT1176-with-RTSP-IP/m-p/2122888#M34561</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the MIMXRT1176 controller to receive H.264 video data over Ethernet from an IP camera via RTSP. The camera is configured to stream at 4 fps with a resolution of 352×240.&lt;/P&gt;&lt;P&gt;I’m using the OpenH264 decoder to decode the H.264 stream. However, I observe that decoding is significantly slower — the display frame rate is only around 1 fps, even though the camera is sending 4 fps.&lt;/P&gt;&lt;P&gt;I’ve confirmed that frames are being received correctly over RTSP using the LIVE555 stack.&lt;/P&gt;&lt;P&gt;How can I improve the H.264 decoding performance using OpenH264 on the RT1176? Is there any optimization suggestion, or are there known limitations?&lt;/P&gt;&lt;P&gt;Any suggestions or best practices would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Pavanakumar A. G.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 07:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OpenH264-Decoding-Performance-Issue-on-MIMXRT1176-with-RTSP-IP/m-p/2122888#M34561</guid>
      <dc:creator>Pavankumar1</dc:creator>
      <dc:date>2025-06-25T07:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: OpenH264 Decoding Performance Issue on MIMXRT1176 with RTSP IP Camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OpenH264-Decoding-Performance-Issue-on-MIMXRT1176-with-RTSP-IP/m-p/2123078#M34562</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222340"&gt;@Pavankumar1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;It is recommended that you start with the project (h264_freertos_cm7) in the SDK, which reads H.264 video from the SD card and decodes it.&lt;/P&gt;
&lt;P&gt;Our colleague measured the performance on RT1060 before, RT1170 will be better, the bottleneck should not be on the MCU side:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Gavin_Jia_0-1750846778319.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/344624i61A8B5FB5FDC0B4B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Gavin_Jia_0-1750846778319.png" alt="Gavin_Jia_0-1750846778319.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Gavin_Jia_0-1750846778319.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 10:20:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OpenH264-Decoding-Performance-Issue-on-MIMXRT1176-with-RTSP-IP/m-p/2123078#M34562</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2025-06-25T10:20:03Z</dc:date>
    </item>
  </channel>
</rss>