<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is the SEMC required for/involved in L1 DCache Management and/or FlexSPI? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-the-SEMC-required-for-involved-in-L1-DCache-Management-and-or/m-p/2122205#M34555</link>
    <description>&lt;P&gt;I am currently battling the clock tree of the RT1021. Since I am using FlexSPI as instruction memory this is a bit complicated as I cannot freely reconfigure the clock tree at will (and I don't want to move the code to SRAM if I can avoid that).&lt;/P&gt;&lt;P&gt;Anyway, in my configuration I don't need the SEMC for anything obvious (there is no SDRAM etc. in use). Therefore I would like to disable it with CLOCK_DisableClock(kCLOCK_Semc) (which is also generated by MCUXpresso in clock_config.c but guarded by&amp;nbsp;ifndef SKIP_SYSCLK_INIT). However, when I do disable it, a call to SCB_InvalidateDCache_by_Addr() (its second DSB instruction to be precise) with an address inside the FlexSPI's range causes the MCU to lock up (i.e., GDB loses connection).&lt;/P&gt;&lt;P&gt;If I do not disable SEMC, the cache invalidation works fine (and it has also worked fine in the past with other clock configurations). I don't think the cache line alignment is a problem here as there is no relevant data near the invalidated address.&lt;/P&gt;&lt;P&gt;Naturally tweaking the clock tree is delicate and this could be just a coincidence but I want to make sure without testing it specifically myself:&lt;/P&gt;&lt;P&gt;Is the SEMC core in the RT102x in any way related to cache management functions outside its own memory range (8000_0000 - DFFF_FFFF) that could explain this behavior?&lt;/P&gt;&lt;P&gt;I take care to not touch the branch in the clock tree feeding the FlexSPI root clock after the bootrom has configured it from FCFB.&lt;/P&gt;</description>
    <pubDate>Tue, 24 Jun 2025 11:32:19 GMT</pubDate>
    <dc:creator>stefanct</dc:creator>
    <dc:date>2025-06-24T11:32:19Z</dc:date>
    <item>
      <title>Is the SEMC required for/involved in L1 DCache Management and/or FlexSPI?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-the-SEMC-required-for-involved-in-L1-DCache-Management-and-or/m-p/2122205#M34555</link>
      <description>&lt;P&gt;I am currently battling the clock tree of the RT1021. Since I am using FlexSPI as instruction memory this is a bit complicated as I cannot freely reconfigure the clock tree at will (and I don't want to move the code to SRAM if I can avoid that).&lt;/P&gt;&lt;P&gt;Anyway, in my configuration I don't need the SEMC for anything obvious (there is no SDRAM etc. in use). Therefore I would like to disable it with CLOCK_DisableClock(kCLOCK_Semc) (which is also generated by MCUXpresso in clock_config.c but guarded by&amp;nbsp;ifndef SKIP_SYSCLK_INIT). However, when I do disable it, a call to SCB_InvalidateDCache_by_Addr() (its second DSB instruction to be precise) with an address inside the FlexSPI's range causes the MCU to lock up (i.e., GDB loses connection).&lt;/P&gt;&lt;P&gt;If I do not disable SEMC, the cache invalidation works fine (and it has also worked fine in the past with other clock configurations). I don't think the cache line alignment is a problem here as there is no relevant data near the invalidated address.&lt;/P&gt;&lt;P&gt;Naturally tweaking the clock tree is delicate and this could be just a coincidence but I want to make sure without testing it specifically myself:&lt;/P&gt;&lt;P&gt;Is the SEMC core in the RT102x in any way related to cache management functions outside its own memory range (8000_0000 - DFFF_FFFF) that could explain this behavior?&lt;/P&gt;&lt;P&gt;I take care to not touch the branch in the clock tree feeding the FlexSPI root clock after the bootrom has configured it from FCFB.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jun 2025 11:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-the-SEMC-required-for-involved-in-L1-DCache-Management-and-or/m-p/2122205#M34555</guid>
      <dc:creator>stefanct</dc:creator>
      <dc:date>2025-06-24T11:32:19Z</dc:date>
    </item>
    <item>
      <title>Re: Is the SEMC required for/involved in L1 DCache Management and/or FlexSPI?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-the-SEMC-required-for-involved-in-L1-DCache-Management-and-or/m-p/2122562#M34557</link>
      <description>&lt;P&gt;To disable SEMC you can enable SKIP_SYSCLK_INIT macro. To disable cache on SEMC you need to configure the SEMC as non-cachable on the MPU through BOARD_ConfigMPU().&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jun 2025 22:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-the-SEMC-required-for-involved-in-L1-DCache-Management-and-or/m-p/2122562#M34557</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-06-24T22:44:11Z</dc:date>
    </item>
  </channel>
</rss>