<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックparallel CSI camera on MIMXRT1170-EVKB</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2090682#M34218</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to connect a parallel CSI camera to the MIMXRT1170-EVKB using the flexIO. Is there an app note or a project using a parallel camera specifically on the&amp;nbsp;MIMXRT1170-EVKB board? are all the required IOs accessible on the Arduino connectors?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for your help,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Zohar&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 01 May 2025 15:18:05 GMT</pubDate>
    <dc:creator>zohargolan</dc:creator>
    <dc:date>2025-05-01T15:18:05Z</dc:date>
    <item>
      <title>parallel CSI camera on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2090682#M34218</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to connect a parallel CSI camera to the MIMXRT1170-EVKB using the flexIO. Is there an app note or a project using a parallel camera specifically on the&amp;nbsp;MIMXRT1170-EVKB board? are all the required IOs accessible on the Arduino connectors?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for your help,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Zohar&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 15:18:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2090682#M34218</guid>
      <dc:creator>zohargolan</dc:creator>
      <dc:date>2025-05-01T15:18:05Z</dc:date>
    </item>
    <item>
      <title>Re: parallel CSI camera on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2090757#M34219</link>
      <description>&lt;P&gt;Please refer to this application note:&amp;nbsp;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12686.pdf?_gl=1*s9r3y1*_gcl_aw*R0NMLjE3NDM0NDMxMzIuQ2p3S0NBanctcWlfQmhCeEVpd0FreHZia0J3bzRDMVpyelBVQjFZY0p5Qk1XN1VTbkZjNV9maWVoRWVybWF1OWRrU2ZoYlJxLVREckl4b0NpVlVRQXZEX0J3RQ..*_ga*MTM2OTg5NTE0LjE3MTg0MDM4Njk.*_ga_WM5LE0KMSH*MTc0NjEzNTYwMi42NjguMS4xNzQ2MTM1Njg2LjAuMC4w" target="_blank"&gt;Using FlexIO to emulate Parallel Camera Interface on i.MX RT&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 22:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2090757#M34219</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-05-01T22:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: parallel CSI camera on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2090765#M34221</link>
      <description>&lt;P&gt;Thank you Omar for your reply,&lt;/P&gt;&lt;P&gt;I did saw this application note, but my question was if I can run it on the&amp;nbsp;&lt;SPAN&gt;MIMXRT1170-EVKB board. Do I have all the required IOs going to the Arduino connectors?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Zohar&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 22:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2090765#M34221</guid>
      <dc:creator>zohargolan</dc:creator>
      <dc:date>2025-05-01T22:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: parallel CSI camera on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2091681#M34233</link>
      <description>&lt;P&gt;It depends how many pins you need, FlexIO2 only is available on the EVK arduino port on GPIO_AD_00 to GPIO_AD_13 as well as GPIO_AD28 to GPIO_AD31. Please refer to the EVKB schematics.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 20:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2091681#M34233</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-05-05T20:35:16Z</dc:date>
    </item>
    <item>
      <title>Re: parallel CSI camera on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2095553#M34276</link>
      <description>&lt;P&gt;Thank you Omar,&lt;/P&gt;&lt;P&gt;It turned out I dont have the pins I need on the Arduino connectors. In order to get to those pins I will have to do heavy rework to the EVK.&lt;/P&gt;&lt;P&gt;I will use the MIPI interface instead (with a custom parallel to MIPI adapter)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Zohar&lt;/P&gt;</description>
      <pubDate>Mon, 12 May 2025 13:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/parallel-CSI-camera-on-MIMXRT1170-EVKB/m-p/2095553#M34276</guid>
      <dc:creator>zohargolan</dc:creator>
      <dc:date>2025-05-12T13:51:45Z</dc:date>
    </item>
  </channel>
</rss>