<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX RT1064 - LPSPI Maximum FIFO Size in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1064-LPSPI-Maximum-FIFO-Size/m-p/915843#M3390</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was reading through the datasheet regarding LPSPI registers and found where the FIFO size is set.&amp;nbsp; The "parameter register (PARAM)" has two 8-bit fields that represent "maximum number of words in the receive FIFO, which is 2^RXFIFO" or "2^TXFIFO".&amp;nbsp; As I read this, it implies an unreasonably large maximum FIFO size.&amp;nbsp; The default value for both TX and RX is 4 which is a FIFO size of 16 words.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking further, the "FIFO control register (FCR)" includes 4-bit fields for FIFO watermark values.&amp;nbsp; This allows for a maximum watermark value of 15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, simple question:&amp;nbsp; Is the maximum LPSPI FIFO size for the RT10xx 16 words?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jun 2019 15:35:18 GMT</pubDate>
    <dc:creator>nbgatgi</dc:creator>
    <dc:date>2019-06-28T15:35:18Z</dc:date>
    <item>
      <title>iMX RT1064 - LPSPI Maximum FIFO Size</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1064-LPSPI-Maximum-FIFO-Size/m-p/915843#M3390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was reading through the datasheet regarding LPSPI registers and found where the FIFO size is set.&amp;nbsp; The "parameter register (PARAM)" has two 8-bit fields that represent "maximum number of words in the receive FIFO, which is 2^RXFIFO" or "2^TXFIFO".&amp;nbsp; As I read this, it implies an unreasonably large maximum FIFO size.&amp;nbsp; The default value for both TX and RX is 4 which is a FIFO size of 16 words.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking further, the "FIFO control register (FCR)" includes 4-bit fields for FIFO watermark values.&amp;nbsp; This allows for a maximum watermark value of 15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, simple question:&amp;nbsp; Is the maximum LPSPI FIFO size for the RT10xx 16 words?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 15:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1064-LPSPI-Maximum-FIFO-Size/m-p/915843#M3390</guid>
      <dc:creator>nbgatgi</dc:creator>
      <dc:date>2019-06-28T15:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMX RT1064 - LPSPI Maximum FIFO Size</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1064-LPSPI-Maximum-FIFO-Size/m-p/915844#M3391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="307979" data-username="nbgatgi" href="https://community.nxp.com/people/nbgatgi"&gt;Nick Guzzardo&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;Q1)&amp;nbsp; Is the maximum LPSPI FIFO size for the RT10xx 16 words?&lt;BR /&gt;-- Yes, it's.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2019 02:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1064-LPSPI-Maximum-FIFO-Size/m-p/915844#M3391</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-07-01T02:39:12Z</dc:date>
    </item>
  </channel>
</rss>