<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Facing Error in NXP RT1170EVKB Compilation Errror in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2060776#M33748</link>
    <description>&lt;P&gt;i thought to design some model and replace the demo model with that designed model, means I am running some model using kaldi and replacing the run model files with the demo&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Mar 2025 00:07:09 GMT</pubDate>
    <dc:creator>shubhamosh12</dc:creator>
    <dc:date>2025-03-13T00:07:09Z</dc:date>
    <item>
      <title>Facing Error in NXP RT1170EVKB Compilation Errror</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2057077#M33672</link>
      <description>&lt;P&gt;I am running the demo example successfully, but when I am trying to run my own model, I am facing this issue. Also, when I am running the code on another platform on Ubuntu, I am not able to get these files, which are shown in error. Facing this issue for the last 3 weeks after even after trying every method&lt;/P&gt;&lt;P&gt;Building target: evkbmimxrt1170_maestro_sync.axf&lt;BR /&gt;Invoking: MCU Linker&lt;BR /&gt;arm-none-eabi-gcc -nostdlib -L"E:\new\evkbmimxrt1170_maestro_sync\vit\CortexM7\Lib" -L"E:\new\evkbmimxrt1170_maestro_sync\voice_seeker\lib" -Xlinker -no-warn-rwx-segments -Xlinker -Map="evkbmimxrt1170_maestro_sync.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m7 -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -T evkbmimxrt1170_maestro_sync_Release.ld -o "evkbmimxrt1170_maestro_sync.axf" ./xip/dcd.o ./xip/evkbmimxrt1170_flexspi_nor_config.o ./xip/fsl_flexspi_nor_boot.o ./xip/xmcd.o ./voice_seeker/ARM_CortexM7/rdsp_utilities_public/rdsp_memory_utils_public/RdspMemoryUtilsPublic.o ./voice_seeker/ARM_CortexM7/rdsp_utilities_public/rdsp_memory_utils_public/memcheck.o ./utilities/str/fsl_str.o ./utilities/debug_console/fsl_debug_console.o ./utilities/fsl_assert.o ./utilities/fsl_memcpy.o ./utilities/fsl_shell.o ./startup/boot_multicore_slave.o ./startup/startup_mimxrt1176_cm7.o ./source/app_streamer.o ./source/cmd.o ./source/main.o ./source/sdmmc_config.o ./source/semihost_hardfault.o ./source/streamer_pcm.o ./source/stt_processor.o ./source/vit_proc.o ./source/voice_seeker.o ./sdmmc/sd/fsl_sd.o ./sdmmc/osa/fsl_sdmmc_osa.o ./sdmmc/host/usdhc/non_blocking/fsl_sdmmc_host.o ./sdmmc/common/fsl_sdmmc_common.o ./maestro/src/utils/src/file_utils.o ./maestro/src/utils/src/general_utils.o ./maestro/src/utils/src/maestro_logging.o ./maestro/src/elements/audio_proc.o ./maestro/src/elements/audio_sink.o ./maestro/src/elements/audio_src.o ./maestro/src/elements/file_sink.o ./maestro/src/elements/mem_src.o ./maestro/src/elements/process_sink.o ./maestro/src/devices/audio_sink_default.o ./maestro/src/devices/audio_src_default.o ./maestro/src/core/src/pad.o ./maestro/src/core/src/pipeline.o ./maestro/src/core/src/streamer.o ./maestro/src/core/src/streamer_element.o ./maestro/src/core/src/streamer_msg.o ./freertos/freertos-kernel/portable/MemMang/heap_4.o ./freertos/freertos-kernel/portable/GCC/ARM_CM4F/port.o ./freertos/freertos-kernel/croutine.o ./freertos/freertos-kernel/event_groups.o ./freertos/freertos-kernel/list.o ./freertos/freertos-kernel/queue.o ./freertos/freertos-kernel/stream_buffer.o ./freertos/freertos-kernel/tasks.o ./freertos/freertos-kernel/timers.o ./fatfs/source/fsl_sd_disk/fsl_sd_disk.o ./fatfs/source/diskio.o ./fatfs/source/ff.o ./fatfs/source/ffsystem.o ./fatfs/source/ffunicode.o ./drivers/fsl_anatop_ai.o ./drivers/fsl_cache.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_common_arm.o ./drivers/fsl_dcdc.o ./drivers/fsl_dmamux.o ./drivers/fsl_edma.o ./drivers/fsl_flexio.o ./drivers/fsl_flexio_i2s.o ./drivers/fsl_flexio_i2s_edma.o ./drivers/fsl_gpc.o ./drivers/fsl_gpio.o ./drivers/fsl_lpi2c.o ./drivers/fsl_lpuart.o ./drivers/fsl_mu.o ./drivers/fsl_pdm.o ./drivers/fsl_pdm_edma.o ./drivers/fsl_pgmc.o ./drivers/fsl_pmu.o ./drivers/fsl_sai.o ./drivers/fsl_sai_edma.o ./drivers/fsl_semc.o ./drivers/fsl_soc_src.o ./drivers/fsl_usdhc.o ./device/system_MIMXRT1176_cm7.o ./component/uart/fsl_adapter_lpuart.o ./component/serial_manager/fsl_component_serial_manager.o ./component/serial_manager/fsl_component_serial_port_uart.o ./component/osa/fsl_os_abstraction_free_rtos.o ./component/lists/fsl_component_generic_list.o ./component/i2c/fsl_adapter_lpi2c.o ./component/gpio/fsl_adapter_igpio.o ./codec/port/wm8962/fsl_codec_wm8962_adapter.o ./codec/port/fsl_codec_adapter.o ./codec/fsl_codec_common.o ./codec/fsl_codec_i2c.o ./codec/fsl_wm8962.o ./board/board.o ./board/clock_config.o ./board/hardware_init.o ./board/pin_mux.o ./CMSIS/DSP/Source/WindowFunctions/WindowFunctions.o ./CMSIS/DSP/Source/TransformFunctions/TransformFunctions.o ./CMSIS/DSP/Source/TransformFunctions/TransformFunctionsF16.o ./CMSIS/DSP/Source/SupportFunctions/SupportFunctions.o ./CMSIS/DSP/Source/SupportFunctions/SupportFunctionsF16.o ./CMSIS/DSP/Source/StatisticsFunctions/StatisticsFunctions.o ./CMSIS/DSP/Source/StatisticsFunctions/StatisticsFunctionsF16.o ./CMSIS/DSP/Source/SVMFunctions/SVMFunctions.o ./CMSIS/DSP/Source/SVMFunctions/SVMFunctionsF16.o ./CMSIS/DSP/Source/QuaternionMathFunctions/QuaternionMathFunctions.o ./CMSIS/DSP/Source/MatrixFunctions/MatrixFunctions.o ./CMSIS/DSP/Source/MatrixFunctions/MatrixFunctionsF16.o ./CMSIS/DSP/Source/InterpolationFunctions/InterpolationFunctions.o ./CMSIS/DSP/Source/InterpolationFunctions/InterpolationFunctionsF16.o ./CMSIS/DSP/Source/FilteringFunctions/FilteringFunctions.o ./CMSIS/DSP/Source/FilteringFunctions/FilteringFunctionsF16.o ./CMSIS/DSP/Source/FastMathFunctions/FastMathFunctions.o ./CMSIS/DSP/Source/FastMathFunctions/FastMathFunctionsF16.o ./CMSIS/DSP/Source/DistanceFunctions/DistanceFunctions.o ./CMSIS/DSP/Source/DistanceFunctions/DistanceFunctionsF16.o ./CMSIS/DSP/Source/ControllerFunctions/ControllerFunctions.o ./CMSIS/DSP/Source/ComplexMathFunctions/ComplexMathFunctions.o ./CMSIS/DSP/Source/ComplexMathFunctions/ComplexMathFunctionsF16.o ./CMSIS/DSP/Source/CommonTables/CommonTables.o ./CMSIS/DSP/Source/CommonTables/CommonTablesF16.o ./CMSIS/DSP/Source/BayesFunctions/BayesFunctions.o ./CMSIS/DSP/Source/BayesFunctions/BayesFunctionsF16.o ./CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctions.o ./CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.o -Wl,--start-group -lVIT_CM7_v04_11_00 -lvoiceseeker_no_aec -Wl,--end-group&lt;BR /&gt;C:/nxp/MCUXpressoIDE_24.12.148/ide/plugins/com.nxp.mcuxpresso.tools.win32_24.12.0.202407110909/tools/bin/../lib/gcc/arm-none-eabi/13.2.1/../../../../arm-none-eabi/bin/ld.exe: ./source/stt_processor.o: in function `STT_Initialize':&lt;BR /&gt;E:\new\evkbmimxrt1170_maestro_sync\Release/../source/stt_processor.c:25:(.text.STT_Initialize+0xe): undefined reference to `vosk_model_new'&lt;BR /&gt;C:/nxp/MCUXpressoIDE_24.12.148/ide/plugins/com.nxp.mcuxpresso.tools.win32_24.12.0.202407110909/tools/bin/../lib/gcc/arm-none-eabi/13.2.1/../../../../arm-none-eabi/bin/ld.exe: E:\new\evkbmimxrt1170_maestro_sync\Release/../source/stt_processor.c:31:(.text.STT_Initialize+0x24): undefined reference to `vosk_recognizer_new'&lt;BR /&gt;C:/nxp/MCUXpressoIDE_24.12.148/ide/plugins/com.nxp.mcuxpresso.tools.win32_24.12.0.202407110909/tools/bin/../lib/gcc/arm-none-eabi/13.2.1/../../../../arm-none-eabi/bin/ld.exe: E:\new\evkbmimxrt1170_maestro_sync\Release/../source/stt_processor.c:34:(.text.STT_Initialize+0x3a): undefined reference to `vosk_model_free'&lt;BR /&gt;C:/nxp/MCUXpressoIDE_24.12.148/ide/plugins/com.nxp.mcuxpresso.tools.win32_24.12.0.202407110909/tools/bin/../lib/gcc/arm-none-eabi/13.2.1/../../../../arm-none-eabi/bin/ld.exe: ./source/stt_processor.o: in function `STT_Process':&lt;BR /&gt;E:\new\evkbmimxrt1170_maestro_sync\Release/../source/stt_processor.c:49:(.text.STT_Process+0x1c): undefined reference to `vosk_recognizer_accept_waveform'&lt;BR /&gt;C:/nxp/MCUXpressoIDE_24.12.148/ide/plugins/com.nxp.mcuxpresso.tools.win32_24.12.0.202407110909/tools/bin/../lib/gcc/arm-none-eabi/13.2.1/../../../../arm-none-eabi/bin/ld.exe: E:\new\evkbmimxrt1170_maestro_sync\Release/../source/stt_processor.c:51:(.text.STT_Process+0x24): undefined reference to `vosk_recognizer_result'&lt;BR /&gt;Memory region Used Size Region Size %age Used&lt;BR /&gt;BOARD_FLASH: 32284 B 64 MB 0.05%&lt;BR /&gt;SRAM_DTC_cm7: 10992 B 256 KB 4.19%&lt;BR /&gt;SRAM_ITC_cm7: 0 GB 256 KB 0.00%&lt;BR /&gt;SRAM_OC1: 751644 B 768 KB 95.58%&lt;BR /&gt;NCACHE_REGION: 0 GB 256 KB 0.00%&lt;BR /&gt;SRAM_OC_ECC1: 0 GB 64 KB 0.00%&lt;BR /&gt;SRAM_OC_ECC2: 0 GB 64 KB 0.00%&lt;BR /&gt;BOARD_SDRAM: 0 GB 64 MB 0.00%&lt;BR /&gt;collect2.exe: error: ld returned 1 exit status&lt;BR /&gt;make[1]: *** [makefile:91: evkbmimxrt1170_maestro_sync.axf] Error 1&lt;BR /&gt;make: *** [makefile:82: all] Error 2&lt;BR /&gt;"make -r -j12 all" terminated with exit code 2. Build might be incomplete.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 13:09:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2057077#M33672</guid>
      <dc:creator>shubhamosh12</dc:creator>
      <dc:date>2025-03-06T13:09:00Z</dc:date>
    </item>
    <item>
      <title>Re: Facing Error in NXP RT1170EVKB Compilation Errror</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2060766#M33747</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247700"&gt;@shubhamosh12&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am very sorry for the delayed response!&lt;/P&gt;
&lt;P&gt;I can see that you are working with the maestro_sync library and therefore with VIT. How are you replacing the demo's model with yours? Have you found out something else in the meantime to share?&lt;/P&gt;
&lt;P&gt;Thank you!&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Mar 2025 23:24:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2060766#M33747</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-03-12T23:24:55Z</dc:date>
    </item>
    <item>
      <title>Re: Facing Error in NXP RT1170EVKB Compilation Errror</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2060776#M33748</link>
      <description>&lt;P&gt;i thought to design some model and replace the demo model with that designed model, means I am running some model using kaldi and replacing the run model files with the demo&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Mar 2025 00:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2060776#M33748</guid>
      <dc:creator>shubhamosh12</dc:creator>
      <dc:date>2025-03-13T00:07:09Z</dc:date>
    </item>
    <item>
      <title>Re: Facing Error in NXP RT1170EVKB Compilation Errror</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2074506#M33969</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247700"&gt;@shubhamosh12&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I saw that you are using a Vosk&amp;nbsp; model based on Kaldi. But seems that we do not have integration guidelines available. I am sorry for the trouble. I look to undefined references to some source files related to vosk. Have you tried to manually link your source files using the MCUXpresso IDE? For example&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_0-1743802882705.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/331459i3C60812FE041D7A7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diego_charles_0-1743802882705.png" alt="diego_charles_0-1743802882705.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Fri, 04 Apr 2025 21:41:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2074506#M33969</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-04-04T21:41:35Z</dc:date>
    </item>
    <item>
      <title>Re: Facing Error in NXP RT1170EVKB Compilation Errror</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2074542#M33970</link>
      <description>thank you, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/89833"&gt;@diego_charles&lt;/a&gt;&lt;BR /&gt;Yes, it's not exactly Vosk, but thanks for replying. I cannot build and flash just one last thing I am facing now.&lt;BR /&gt;&lt;BR /&gt;When I open the putty, just a black screen comes up. I tried hello world; there I can see hello world on Putty, but on mine, nothing is coming. On pressing the Z key, some noise is coming, so can you tell me in usb_sync how this happens, like help, or see whether I am doing right or something wrong is going on? And Can you tell me how to reset the console windows? somehow i cut the screen; now i able to see only one screen running code, no warnings, etc. can you tell how to reset that</description>
      <pubDate>Sat, 05 Apr 2025 00:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Facing-Error-in-NXP-RT1170EVKB-Compilation-Errror/m-p/2074542#M33970</guid>
      <dc:creator>shubhamosh12</dc:creator>
      <dc:date>2025-04-05T00:54:51Z</dc:date>
    </item>
  </channel>
</rss>