<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックUsing i3c with i2c</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-i3c-with-i2c/m-p/2038124#M33374</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I'm connecting the WM8904 to the I3C bus from the RT685 using the MIMXRT685-EVK and controlling it via I2C.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Please tell me about the settings and processing for PUR in that case.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; [Question] 1) Is it possible to control the WM8904 using only I3CSDA and SCL and use P2_31 PUR as SWO?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; It seems possible to set it up, but is it okay to set it up like this?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; 2) When using P2_31 as PUR, is it correct to understand that it's okay to leave P2_31 unconnected as long as SDA is pulled up (e.g. 2.2kΩ)?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 05 Feb 2025 01:19:38 GMT</pubDate>
    <dc:creator>teruteru5678</dc:creator>
    <dc:date>2025-02-05T01:19:38Z</dc:date>
    <item>
      <title>Using i3c with i2c</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-i3c-with-i2c/m-p/2038124#M33374</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I'm connecting the WM8904 to the I3C bus from the RT685 using the MIMXRT685-EVK and controlling it via I2C.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Please tell me about the settings and processing for PUR in that case.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; [Question] 1) Is it possible to control the WM8904 using only I3CSDA and SCL and use P2_31 PUR as SWO?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; It seems possible to set it up, but is it okay to set it up like this?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; 2) When using P2_31 as PUR, is it correct to understand that it's okay to leave P2_31 unconnected as long as SDA is pulled up (e.g. 2.2kΩ)?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 01:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-i3c-with-i2c/m-p/2038124#M33374</guid>
      <dc:creator>teruteru5678</dc:creator>
      <dc:date>2025-02-05T01:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: Using i3c with i2c</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-i3c-with-i2c/m-p/2040722#M33417</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243734"&gt;@teruteru5678&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is possible about your question if you only want to use I2C instead, also the PUR IO port can be used as SWO if both SCL and SDA are pulled up(R413, R414 is DNP as default) in that time.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Feb 2025 08:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-i3c-with-i2c/m-p/2040722#M33417</guid>
      <dc:creator>Sam_Gao</dc:creator>
      <dc:date>2025-02-10T08:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: Using i3c with i2c</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-i3c-with-i2c/m-p/2042420#M33440</link>
      <description>&lt;P&gt;Sorry for the late reply.&lt;BR /&gt;Thank you for your reply.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 08:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-i3c-with-i2c/m-p/2042420#M33440</guid>
      <dc:creator>teruteru5678</dc:creator>
      <dc:date>2025-02-12T08:34:56Z</dc:date>
    </item>
  </channel>
</rss>