<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Initialize SDRAM with 166 MHZ via DCD in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Initialize-SDRAM-with-166-MHZ-via-DCD/m-p/2034635#M33312</link>
    <description>Thanks for the feedback. Seems to work &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;</description>
    <pubDate>Mon, 27 Jan 2025 15:09:24 GMT</pubDate>
    <dc:creator>Masmiseim</dc:creator>
    <dc:date>2025-01-27T15:09:24Z</dc:date>
    <item>
      <title>Initialize SDRAM with 166 MHZ via DCD</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Initialize-SDRAM-with-166-MHZ-via-DCD/m-p/2028878#M33202</link>
      <description>&lt;P&gt;&lt;BR /&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;We are trying to initialize the SDRAM (16 bit) with DCD, except for the clock everything seems to work quite well. But we are not able to set the required 166 MHz. The clock is always set to 198 MHz. Do you have an example for 166 MHz?&lt;BR /&gt;I have attached our current configuration.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 09:08:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Initialize-SDRAM-with-166-MHZ-via-DCD/m-p/2028878#M33202</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2025-01-16T09:08:01Z</dc:date>
    </item>
    <item>
      <title>Re: Initialize SDRAM with 166 MHZ via DCD</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Initialize-SDRAM-with-166-MHZ-via-DCD/m-p/2029333#M33212</link>
      <description>&lt;P&gt;Please use this configuration for 166Mhz clock.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_0-1737068763905.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/319969i4CEE65BBFDEC4CA4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_0-1737068763905.png" alt="Omar_Anguiano_0-1737068763905.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This will set the SEMC with this source and this divider.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_1-1737068794372.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/319970i05E1145BEA6A99A1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_1-1737068794372.png" alt="Omar_Anguiano_1-1737068794372.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 23:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Initialize-SDRAM-with-166-MHZ-via-DCD/m-p/2029333#M33212</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-01-16T23:06:50Z</dc:date>
    </item>
    <item>
      <title>Re: Initialize SDRAM with 166 MHZ via DCD</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Initialize-SDRAM-with-166-MHZ-via-DCD/m-p/2034635#M33312</link>
      <description>Thanks for the feedback. Seems to work &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;</description>
      <pubDate>Mon, 27 Jan 2025 15:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Initialize-SDRAM-with-166-MHZ-via-DCD/m-p/2034635#M33312</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2025-01-27T15:09:24Z</dc:date>
    </item>
  </channel>
</rss>