<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMx RT1180 using HyperRam in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033724#M33299</link>
    <description>&lt;P&gt;Thanks Diego, i will try but this is only a test. i must use hyper ram with debugger but i want to understand why all example for M7 present oin SDK works only with internal ram, isn't checked wirh flash or external ram? i understand that the mcu is not released in this date but, as me i need to check the mcu to decide if use nxp or another brand, and i have a lot of problem for simple things..&lt;/P&gt;&lt;P&gt;anyway if you have a chance to use an 1180 board and test it runtime shuld &lt;SPAN&gt;appreciate.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Simone&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 24 Jan 2025 07:50:45 GMT</pubDate>
    <dc:creator>SimoneColomboWEG</dc:creator>
    <dc:date>2025-01-24T07:50:45Z</dc:date>
    <item>
      <title>iMx RT1180 using HyperRam</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033282#M33292</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i'm going to use HyperRam on EVK 700-50577 rev C1 ( core M7 ) because my eval code is too large for DTC and ITC but when the program is downloaded after few times crash.&lt;/P&gt;&lt;P&gt;i've attached a simple program to test it.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Simone&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jan 2025 15:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033282#M33292</guid>
      <dc:creator>SimoneColomboWEG</dc:creator>
      <dc:date>2025-01-23T15:44:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMx RT1180 using HyperRam</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033358#M33293</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245877"&gt;@SimoneColomboWEG&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Thank you for your interest on our RT1180!&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I do not have an RT1180 to test with me, as I am not part of the NPI process of the RT1180,&amp;nbsp; so I can not&amp;nbsp; reproduce this issue on my bench. For this particular time,&amp;nbsp; I advice to contact your dedicated NXP representative, to get more dedicated help.&lt;/P&gt;
&lt;P&gt;I still checked your project, and&amp;nbsp; I saw that you linked your application to the HyperRAM address space, I wonder if the issue you are reporting can be reproduced all the time. But I&amp;nbsp; suggest you to check with the XMCD that the MCUxpresso Secure Provisioning embeds when programming your image.&amp;nbsp; With the tool, you can generate a bootable image and program over LPUART1 or USB1. Below a reference picture.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_0-1737654358310.png" style="width: 733px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/321119iCB2EDF0BEEBE71D1/image-dimensions/733x213?v=v2" width="733" height="213" role="button" title="diego_charles_0-1737654358310.png" alt="diego_charles_0-1737654358310.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;diego_charles_0-1737654358310.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I hope this helps you!&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jan 2025 17:49:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033358#M33293</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-01-23T17:49:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMx RT1180 using HyperRam</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033724#M33299</link>
      <description>&lt;P&gt;Thanks Diego, i will try but this is only a test. i must use hyper ram with debugger but i want to understand why all example for M7 present oin SDK works only with internal ram, isn't checked wirh flash or external ram? i understand that the mcu is not released in this date but, as me i need to check the mcu to decide if use nxp or another brand, and i have a lot of problem for simple things..&lt;/P&gt;&lt;P&gt;anyway if you have a chance to use an 1180 board and test it runtime shuld &lt;SPAN&gt;appreciate.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Simone&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jan 2025 07:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033724#M33299</guid>
      <dc:creator>SimoneColomboWEG</dc:creator>
      <dc:date>2025-01-24T07:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: iMx RT1180 using HyperRam</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033969#M33303</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245877"&gt;@SimoneColomboWEG&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your reply, I understand your feeling, agian we appreaciate your interest.&lt;/P&gt;
&lt;P&gt;Let me check and discuss about this situation. I want to know which SDK release and toolchain you are using, could you let know that?&lt;/P&gt;
&lt;P&gt;Update: maybe this will help to explain the issue:&amp;nbsp; see&amp;nbsp; RAW/POR image switch from the new MCUXpresso&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/evkmimxrt1180/gettingStarted/topics/bootable_image_generation.html" target="_blank"&gt;https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/evkmimxrt1180/gettingStarted/topics/bootable_image_generation.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jan 2025 23:17:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMx-RT1180-using-HyperRam/m-p/2033969#M33303</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-01-24T23:17:42Z</dc:date>
    </item>
  </channel>
</rss>