<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB CDC VCOM User defined device example consecutive RX fail in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-VCOM-User-defined-device-example-consecutive-RX-fail/m-p/2029041#M33203</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Ah, I see, in that case I'll keep a workaround in place.&lt;/P&gt;&lt;P&gt;Thanks for the fast reply, you've saved me a lot of debugging time!.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Cheers,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alex&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jan 2025 12:55:25 GMT</pubDate>
    <dc:creator>akspurr</dc:creator>
    <dc:date>2025-01-16T12:55:25Z</dc:date>
    <item>
      <title>USB CDC VCOM User defined device example consecutive RX fail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-VCOM-User-defined-device-example-consecutive-RX-fail/m-p/2028230#M33193</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Recently I worked through your very useful user defined device class application note, based on the cdc_vcom example: &lt;A href="https://www.nxp.com/docs/en/application-note/AN14169.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN14169.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The code is functioning as I would expect, except for when I modify the AppTask to receive multiple packets prior to sending a response back to the host.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;It seems that the USB stack forces a Send for every Recv, something which other users have noted (e.g&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ESC-character-in-virtual-com-port-example/m-p/1154247" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ESC-character-in-virtual-com-port-example/m-p/1154247&lt;/A&gt;).&lt;BR /&gt;&lt;BR /&gt;Is there a way to modify the stack to allow for multiple consecutive Recv?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alex&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jan 2025 10:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-VCOM-User-defined-device-example-consecutive-RX-fail/m-p/2028230#M33193</guid>
      <dc:creator>akspurr</dc:creator>
      <dc:date>2025-01-15T10:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC VCOM User defined device example consecutive RX fail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-VCOM-User-defined-device-example-consecutive-RX-fail/m-p/2028513#M33197</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245587"&gt;@akspurr&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, the stack is designed to do a send after every receive by design, so no modifications should be made to the USB stack to prevent this behavior.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jan 2025 20:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-VCOM-User-defined-device-example-consecutive-RX-fail/m-p/2028513#M33197</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-01-15T20:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC VCOM User defined device example consecutive RX fail</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-VCOM-User-defined-device-example-consecutive-RX-fail/m-p/2029041#M33203</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Ah, I see, in that case I'll keep a workaround in place.&lt;/P&gt;&lt;P&gt;Thanks for the fast reply, you've saved me a lot of debugging time!.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Cheers,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alex&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 12:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-VCOM-User-defined-device-example-consecutive-RX-fail/m-p/2029041#M33203</guid>
      <dc:creator>akspurr</dc:creator>
      <dc:date>2025-01-16T12:55:25Z</dc:date>
    </item>
  </channel>
</rss>