<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Instability in RT1170 inputs in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Instability-in-RT1170-inputs/m-p/2025740#M33151</link>
    <description>&lt;P&gt;I am working with the ADC of the i.MXRT 1170.&lt;/P&gt;&lt;P&gt;To do my test I am using the Fully-Differencial Amplifier circuit shown in Figure_1. In this configuration, I get 1.6V in both outputs positive and negative (the input is shortcircuited and connected to GND). If I do not connect anything else to this circuit the output is pretty stable (20.9mV of noise p-p): Figure_2 shows the noise in the output. This noise has been measured with a 200MHz Bandwith oscilloscope.&lt;/P&gt;&lt;P&gt;Then, I have connected te output of this circuit to the balls L13 and M15 of the i.MX RT1170. First I have configured this pins as analog inputs with the keeper option selected. At the moment I connect the outputs of the amplifier circuit to the processor the signal begins to oscililate. Figure_3 shows the signal measured at that moment in a test-point near the pin L13 of the processor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried with other pins,&amp;nbsp; and other configurations (digital input, analog input, with pull-up, with pull-down, with keeper). I get the same result with all configurations: the signal begins to oscilate at the moment I connect it to the processor and it is stable when I disconect the processor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would appreciate a lot If someone could shed light in this issue.&lt;/P&gt;</description>
    <pubDate>Fri, 10 Jan 2025 10:56:02 GMT</pubDate>
    <dc:creator>ibravo</dc:creator>
    <dc:date>2025-01-10T10:56:02Z</dc:date>
    <item>
      <title>Instability in RT1170 inputs</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Instability-in-RT1170-inputs/m-p/2025740#M33151</link>
      <description>&lt;P&gt;I am working with the ADC of the i.MXRT 1170.&lt;/P&gt;&lt;P&gt;To do my test I am using the Fully-Differencial Amplifier circuit shown in Figure_1. In this configuration, I get 1.6V in both outputs positive and negative (the input is shortcircuited and connected to GND). If I do not connect anything else to this circuit the output is pretty stable (20.9mV of noise p-p): Figure_2 shows the noise in the output. This noise has been measured with a 200MHz Bandwith oscilloscope.&lt;/P&gt;&lt;P&gt;Then, I have connected te output of this circuit to the balls L13 and M15 of the i.MX RT1170. First I have configured this pins as analog inputs with the keeper option selected. At the moment I connect the outputs of the amplifier circuit to the processor the signal begins to oscililate. Figure_3 shows the signal measured at that moment in a test-point near the pin L13 of the processor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried with other pins,&amp;nbsp; and other configurations (digital input, analog input, with pull-up, with pull-down, with keeper). I get the same result with all configurations: the signal begins to oscilate at the moment I connect it to the processor and it is stable when I disconect the processor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would appreciate a lot If someone could shed light in this issue.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jan 2025 10:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Instability-in-RT1170-inputs/m-p/2025740#M33151</guid>
      <dc:creator>ibravo</dc:creator>
      <dc:date>2025-01-10T10:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: Instability in RT1170 inputs</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Instability-in-RT1170-inputs/m-p/2026083#M33158</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245417"&gt;@ibravo&lt;/a&gt;,&lt;BR /&gt;I understand that you are currently using an EVK. In order to support you better, can you provide me the specific EVK where you are testing?&lt;BR /&gt;Also, I understand that you are using a test point as a reference, in order to try a pinpoint if this causes the issue, can you use a GND pin instead a test point?&lt;BR /&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jan 2025 22:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Instability-in-RT1170-inputs/m-p/2026083#M33158</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-01-10T22:14:07Z</dc:date>
    </item>
  </channel>
</rss>