<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: FlexIO-based camera interface max PCLK frequency</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2003107#M32744</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243693"&gt;@powerfeatherdev&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The tested scenarios we have done are described on the following application note:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12686.pdf" target="_blank"&gt;Using FlexIO to emulate Parallel Camera Interface on i.MX RT&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Nov 2024 19:03:39 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2024-11-27T19:03:39Z</dc:date>
    <item>
      <title>FlexIO-based camera interface max PCLK frequency</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2000012#M32674</link>
      <description>&lt;P&gt;Hi, I'm currently looking into using the FlexIO-based camera interface example as a base for talking to another type of interface somewhat similar to it. That is, an interface where the device outputs a clock, and data access is synchronous to that clock.&lt;BR /&gt;&lt;BR /&gt;On the reference manual, there is a "FlexIO Application Information Section"&amp;nbsp; which states some&amp;nbsp; limits for specific FlexIO interface implementations. For example, for the SPI Master, it says:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Due to synchronization delays, the setup time for the serial input data is 1.5 FlexIO clock cycles, so the maximum baud rate is divide by 4 of the FlexIO clock frequency.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;However, for the&amp;nbsp;Camera Interface, it does not state such thing. So does that mean that the the PCLK be theoretically as high as the FlexIO base clock (120 MHz)?&lt;/P&gt;</description>
      <pubDate>Fri, 22 Nov 2024 10:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2000012#M32674</guid>
      <dc:creator>powerfeatherdev</dc:creator>
      <dc:date>2024-11-22T10:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: FlexIO-based camera interface max PCLK frequency</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2000390#M32679</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243693"&gt;@powerfeatherdev&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;That is correct, the maximum PCLK frequency is directly proportional to the maximum FlexIO peripheral clock.&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Nov 2024 21:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2000390#M32679</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-11-22T21:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: FlexIO-based camera interface max PCLK frequency</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2000526#M32681</link>
      <description>I see, so it can get up to 120 Mhz? Is this something that has been tested by NXP? I would test this myself, but the EVK that I bought apparently does not expose enough FlexIO pins to test this (RT1010).</description>
      <pubDate>Sun, 24 Nov 2024 03:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2000526#M32681</guid>
      <dc:creator>powerfeatherdev</dc:creator>
      <dc:date>2024-11-24T03:08:02Z</dc:date>
    </item>
    <item>
      <title>Re: FlexIO-based camera interface max PCLK frequency</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2001404#M32707</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243693"&gt;@powerfeatherdev&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This has not been properly tested by NXP, no. It is only the theoretical limit.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Nov 2024 22:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2001404#M32707</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-11-25T22:26:36Z</dc:date>
    </item>
    <item>
      <title>Re: FlexIO-based camera interface max PCLK frequency</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2001407#M32708</link>
      <description>&lt;P&gt;Hi Edwin, up to what speed was NXP able to push this? I think I might need at least 60 MHz.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Nov 2024 22:28:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2001407#M32708</guid>
      <dc:creator>powerfeatherdev</dc:creator>
      <dc:date>2024-11-25T22:28:50Z</dc:date>
    </item>
    <item>
      <title>Re: FlexIO-based camera interface max PCLK frequency</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2003107#M32744</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243693"&gt;@powerfeatherdev&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The tested scenarios we have done are described on the following application note:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12686.pdf" target="_blank"&gt;Using FlexIO to emulate Parallel Camera Interface on i.MX RT&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 19:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexIO-based-camera-interface-max-PCLK-frequency/m-p/2003107#M32744</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-11-27T19:03:39Z</dc:date>
    </item>
  </channel>
</rss>