<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックSAI_TxSetBitClockRate parameter questions</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SAI-TxSetBitClockRate-parameter-questions/m-p/2002352#M32725</link>
    <description>&lt;P&gt;I'm trying to set up SAI (send only, as master).&lt;BR /&gt;But I'm confused by the SAI_TxSetBitClockRate parameters, documented as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;/*!
 * brief Transmitter bit clock rate configurations.
 *
 * param base SAI base pointer.
 * param sourceClockHz, bit clock source frequency.
 * param sampleRate audio data sample rate.
 * param bitWidth, audio data bitWidth.
 * param channelNumbers, audio channel numbers.
 */
void SAI_TxSetBitClockRate(
    I2S_Type *base, uint32_t sourceClockHz, uint32_t sampleRate, uint32_t bitWidth, uint32_t channelNumbers)&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1) What is uint32_t channelNumbers?&lt;/STRONG&gt;&lt;BR /&gt;In the code this seems to be used as numberOfChannels (ie 2 for stereo):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;uint32_t bitClockFreq = sampleRate * bitWidth * channelNumbers;&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2) What is uint32_t sourceClockHz?&lt;BR /&gt;&lt;/STRONG&gt;Is this just the module's clock input, as generated by the clock tool, ie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define BOARD_BOOTCLOCKRUN_SAI1_CLK_ROOT              63529411UL&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Nov 2024 01:48:18 GMT</pubDate>
    <dc:creator>davenadler</dc:creator>
    <dc:date>2024-11-27T01:48:18Z</dc:date>
    <item>
      <title>SAI_TxSetBitClockRate parameter questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SAI-TxSetBitClockRate-parameter-questions/m-p/2002352#M32725</link>
      <description>&lt;P&gt;I'm trying to set up SAI (send only, as master).&lt;BR /&gt;But I'm confused by the SAI_TxSetBitClockRate parameters, documented as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;/*!
 * brief Transmitter bit clock rate configurations.
 *
 * param base SAI base pointer.
 * param sourceClockHz, bit clock source frequency.
 * param sampleRate audio data sample rate.
 * param bitWidth, audio data bitWidth.
 * param channelNumbers, audio channel numbers.
 */
void SAI_TxSetBitClockRate(
    I2S_Type *base, uint32_t sourceClockHz, uint32_t sampleRate, uint32_t bitWidth, uint32_t channelNumbers)&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1) What is uint32_t channelNumbers?&lt;/STRONG&gt;&lt;BR /&gt;In the code this seems to be used as numberOfChannels (ie 2 for stereo):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;uint32_t bitClockFreq = sampleRate * bitWidth * channelNumbers;&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2) What is uint32_t sourceClockHz?&lt;BR /&gt;&lt;/STRONG&gt;Is this just the module's clock input, as generated by the clock tool, ie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define BOARD_BOOTCLOCKRUN_SAI1_CLK_ROOT              63529411UL&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 01:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SAI-TxSetBitClockRate-parameter-questions/m-p/2002352#M32725</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2024-11-27T01:48:18Z</dc:date>
    </item>
    <item>
      <title>回复： SAI_TxSetBitClockRate parameter questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SAI-TxSetBitClockRate-parameter-questions/m-p/2002674#M32731</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/132425"&gt;@davenadler&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1) What is uint32_t channelNumbers?&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In the code this seems to be used as numberOfChannels (ie 2 for stereo):&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;gt;&amp;gt; Yes, you are right.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;2) What is uint32_t sourceClockHz?&lt;BR /&gt;&lt;/STRONG&gt;Is this just the module's clock input, as generated by the clock tool, ie&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;gt;&amp;gt; Yes.&amp;nbsp;&lt;/SPAN&gt;It is the clock frequency of the SAI peripheral. It is used to configure the appropriate BCLK.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 08:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SAI-TxSetBitClockRate-parameter-questions/m-p/2002674#M32731</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-11-27T08:46:50Z</dc:date>
    </item>
  </channel>
</rss>