<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMXRT1180 Memory debugging RW error or  encry? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1180-Memory-debugging-RW-error-or-encry/m-p/1992354#M32545</link>
    <description>&lt;P&gt;When debugging the MIMXRT1180-EVK board, if there are some errors in the program, the mcu seems to predict in advance and cause undetectable memory read and write errors (such as the function stack) that can't be debugged. Especially on OCRAM memory and HYPERRAM, even if the program is running properly, JLINK still cannot read out the correct value in memory. Including the Keil routine in the SDK will also appear, is this an IMXRT1180 encryption method? How do I get JLINK and OCRAM/HYPERRAM memory to work?&lt;/P&gt;</description>
    <pubDate>Tue, 12 Nov 2024 02:25:34 GMT</pubDate>
    <dc:creator>Haoxxxxxxxx</dc:creator>
    <dc:date>2024-11-12T02:25:34Z</dc:date>
    <item>
      <title>IMXRT1180 Memory debugging RW error or  encry?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1180-Memory-debugging-RW-error-or-encry/m-p/1992354#M32545</link>
      <description>&lt;P&gt;When debugging the MIMXRT1180-EVK board, if there are some errors in the program, the mcu seems to predict in advance and cause undetectable memory read and write errors (such as the function stack) that can't be debugged. Especially on OCRAM memory and HYPERRAM, even if the program is running properly, JLINK still cannot read out the correct value in memory. Including the Keil routine in the SDK will also appear, is this an IMXRT1180 encryption method? How do I get JLINK and OCRAM/HYPERRAM memory to work?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 02:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1180-Memory-debugging-RW-error-or-encry/m-p/1992354#M32545</guid>
      <dc:creator>Haoxxxxxxxx</dc:creator>
      <dc:date>2024-11-12T02:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1180 Memory debugging RW error or  encry?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1180-Memory-debugging-RW-error-or-encry/m-p/2001561#M32712</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;IMXRT1180 EVK&amp;nbsp;board is not yet available to the public, it only for beta key customers with dedicated channel both hardware and software, please contact you local FAE or sales for help, pleas feel free to tell us if you have any questions.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 03:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1180-Memory-debugging-RW-error-or-encry/m-p/2001561#M32712</guid>
      <dc:creator>Sam_Gao</dc:creator>
      <dc:date>2024-11-26T03:50:37Z</dc:date>
    </item>
  </channel>
</rss>