<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Debugging RT1176 with MCU-Link and GDB</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1989200#M32493</link>
    <description>&lt;P&gt;Hello, could you let me know what version is the RT1170 EVK or EVKB?&lt;/P&gt;
&lt;P&gt;In both cases the J1 could use the SWD with adapter to JTAG 20 pins.&lt;/P&gt;
&lt;P&gt;On the board EVKB:&lt;BR /&gt;Could use the J87 but need to put a jumper on JP5 to use the SWD 10 pins.&lt;/P&gt;
&lt;P&gt;On the board EVK:&lt;BR /&gt;The J16 is only for the debugger DFU and the J58 could use to the target MCU.&lt;/P&gt;
&lt;P&gt;I recommend do some test on these ports.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Wed, 06 Nov 2024 18:46:32 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2024-11-06T18:46:32Z</dc:date>
    <item>
      <title>Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1987927#M32473</link>
      <description>&lt;P&gt;Currently we've been using JLink for debugging our custom RT1176 based boards. Now we evaluate a switch to MCU-Link Base, but I'm facing problems during the connection.&lt;/P&gt;&lt;P&gt;The LinkServer application reports unconnected pins. But we verified the correct connection of the MCU Link Base pins on J2 (SWD interface):&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MCU-Link J2 pin 1 3V3 connected as VREF&lt;/LI&gt;&lt;LI&gt;MCU-Link J2 pin 3,5,7,9 GND connected&lt;/LI&gt;&lt;LI&gt;MCU-Link J2 pin 10 RST connected&lt;/LI&gt;&lt;LI&gt;MCU-Link J2 pin 4 SWD-CLK connected&lt;/LI&gt;&lt;LI&gt;MCU-Link J2 pin 2 SWD-IO connected&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;We're only not using MCU-Link J2 pin 6 SWO, which is left floating.&lt;/P&gt;&lt;P&gt;On the JLink-Base this setup works with the following command:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;JLinkGDBServer -endian little -noir -speed 4000 -port 2331 -device MIMXRT1176xxxA_M7 -if SWD -halt -reportuseraction&lt;/LI-CODE&gt;&lt;P&gt;Now we connect the MCU-Link instead and run the LinkServer with the following command:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;LinkServer -l 5 gdbserver   MIMXRT1176xxxxx:MIMXRT1170-EVK-CM7-ONLY&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This results in the following output:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;[116]DEBUG:asyncio: Using selector: EpollSelector
[504]INFO:launcher.cli.utils.funcs: Exact match for MIMXRT1176xxxxx:MIMXRT1170-EVK-CM7-ONLY found
[504]INFO:launcher.cli.utils.click: Selected device MIMXRT1176xxxxx:MIMXRT1170-EVK-CM7-ONLY
[505]DEBUG:launcher.core.redlinkserv: Starting redlinkserv: /usr/local/LinkServer_24.9.75/binaries/redlinkserv ['--port', '11111', '--telnetport', '12222', '--no-telnet-defaults']
[508]DEBUG:launcher.core.probeboot: Listing usb devices
[508]DEBUG:launcher.core.utils: Subprocess exec: lsusb []
[511]DEBUG:launcher.core.redlinkserv: Connecting to redlinkserv (localhost:12222)
[515]DEBUG:launcher.core.redlinkserv: Connected to redlinkserv
[515]DEBUG:launcher.core.redlinkserv: [read] 
[518]DEBUG:launcher.core.probeboot: Found 16 USB devices
[518]INFO:launcher.cli.utils.click: Getting available probes
[518]DEBUG:launcher.core.redlinkserv: [write] probelist
[1606]DEBUG:launcher.core.redlinkserv: [read-partial] b'Index = 1\nManufacturer = NXP Semiconductors\nDescription = MCU-LINK (r0BF) CMSIS-DAP V3.148\nSerial Number = QP1Q5X3JAG0LE\nVID:PID = 1FC9:0143\nPath = 0003:0012:00\n\n\n'
[1649]DEBUG:launcher.core.redlinkserv: [read] Index = 1
Manufacturer = NXP Semiconductors
Description = MCU-LINK (r0BF) CMSIS-DAP V3.148
Serial Number = QP1Q5X3JAG0LE
VID:PID = 1FC9:0143
Path = 0003:0012:00
[1649]INFO:launcher.cli.utils.click: Selected probe #1 QP1Q5X3JAG0LE (MCU-LINK (r0BF) CMSIS-DAP V3.148)
[1650]INFO:launcher.core.redlinkserv: MCU-Link firmware update `check`: local firmware [3.148] is the same as the version running on the selected probe ([QP1Q5X3JAG0LE] [MCU-LINK (r0BF) CMSIS-DAP V3.148])
Firmware update `check`: not required - the update can be performed using `forced` mode
[1650]DEBUG:launcher.core.redlinkserv: [write] probeopenbyindex 1
[1651]DEBUG:launcher.core.redlinkserv: [read-partial] b'Probe Handle 1 Open\n'
[1693]DEBUG:launcher.core.redlinkserv: [read] Probe Handle 1 Open
[1693]DEBUG:launcher.core.redlinkserv: [write] wireswdconnect 1
[1815]DEBUG:launcher.core.redlinkserv: [read-partial] b'Error: Wire Ack Fault - target connected?\n'
[1857]DEBUG:launcher.core.redlinkserv: [read] Error: Wire Ack Fault - target connected?
[1857]DEBUG:launcher.core.redlinkserv: [write] coreconfig 1
[1857]DEBUG:launcher.core.redlinkserv: [read-partial] b'Error: Wire not connected\n'
[1901]DEBUG:launcher.core.redlinkserv: [read] Error: Wire not connected
[1901]DEBUG:launcher.core.redlinkserv: [write] corelist 1
[1902]DEBUG:launcher.core.redlinkserv: [read-partial] b'Error: Wire Ack Fault - target connected?\n'
[1945]DEBUG:launcher.core.redlinkserv: [read] Error: Wire Ack Fault - target connected?
[1946]DEBUG:launcher.cli.cmd.gdbserver: Starting stubs
[1949]DEBUG:launcher.core.stub: Wrote stub XML: /tmp/tmpvi5emm95/crt_directory.xml
[1950]DEBUG:launcher.core.stub: Wrote stub XML: /tmp/tmpvi5emm95/part.xml
[1950]DEBUG:launcher.core.stub: Internal gdbserver (3333) ports: stub_port=13333, sh_stub_port=14444, stdout_port=15555
[1954]DEBUG:launcher.core.stub: GDB server args: ['--redlink-port', '11111', '--flash-dir', '/usr/local/LinkServer_24.9.75/binaries/Flash', '-x', '/tmp/tmpvi5emm95', '-pMIMXRT1176xxxxx', '--vendor', 'NXP', '-g', '--cache', 'dis', '--probeserial', 'QP1Q5X3JAG0LE', '--coreindex', '0', '--kill-server', '--server', 'localhost:13333', '--telnet', '14444', '--msg-port', '15555', '--connectscript', 'RT1170_connect_M7.scp', '--resetscript', 'RT1170_reset_M7.scp']
GDB server listening on port 3333 in debug mode (core cm7)
Semihosting server listening on port 4444 (core cm7)
[1960]DEBUG:launcher.core.stub: [stub (3333)] Ns: MCUXpresso IDE RedlinkMulti Driver v24.9 (Sep 19 2024 19:39:44 - crt_emu_cm_redlink build 802)&lt;/LI-CODE&gt;&lt;P&gt;Now we connect gdb to the port 3333 and get the following output of LinkServer. Then the application automatically closes.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;[343937]DEBUG:launcher.core.stub: Received connection to our GDB server (3333)
[343938]DEBUG:launcher.core.stub: Connected to stub's GDB port (13333)
[343938]INFO:launcher.cli.cmd.gdbserver: Connected to core cm7
[343938]DEBUG:launcher.core.stub: GDB (3333) -&amp;gt; stub (13333): b'+$qSupported:multiprocess+;swbreak+;hwbreak+;qRelocInsn+;fork-events+;vfork-events+;exec-events+;vContSupported+;QThreadEvents+;no-resumed+#df'
[343938]DEBUG:launcher.core.stub: [stub (3333)] Pc: (  0) Reading remote configuration
[343938]DEBUG:launcher.core.stub: [stub (3333)] Wc(03). No cache support.
[343938]DEBUG:launcher.core.stub: [stub (3333)] Nc: Found generic directory XML file in /tmp/tmpvi5emm95/crt_directory.xml
[343939]DEBUG:launcher.core.stub: [stub (3333)] Pc: (  5) Remote configuration complete
Nc: Reconnected to existing LinkServer process.
[344061]DEBUG:launcher.core.stub: [stub (3333)] Nc: Connecting to probe 1 core 0 (using server started externally) reports:
    'Ee(42). Could not connect to core.'
Nc: Retrying...
[345806]DEBUG:launcher.core.stub: [stub (3333)] Nc: Reconnected to existing LinkServer process.
[345938]DEBUG:launcher.core.stub: GDB (3333) -&amp;gt; stub (13333): b'$qSupported:multiprocess+;swbreak+;hwbreak+;qRelocInsn+;fork-events+;vfork-events+;exec-events+;vContSupported+;QThreadEvents+;no-resumed+#df'
[346426]DEBUG:launcher.core.stub: [stub (3333)] Nc: Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
[346549]DEBUG:launcher.core.stub: [stub (3333)] Wc: ============= SCRIPT: RT1170_connect_M7.scp =============
Wc: RT1170 Connect M7 Script
Wc: Error: Wire Ack Fault - target connected?
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: View cores on the DAP AP
Wc: Error: Wire Ack Fault - target connected?
Wc: Error: Wire not connected
[346549]DEBUG:launcher.core.stub: [stub (3333)] Wc: Error: Wire not connected
Wc: ============= END SCRIPT ================================
[346668]DEBUG:launcher.core.stub: [stub (3333)] Ed:02: Failed on connect: Ee(42). Could not connect to core.
Et:31: No connection to chip's debug port
Pc: (100) Target Operation Failed
[346669]DEBUG:launcher.core.stub: Stub socket closed (13333). Closing GDB socket (3333)
[346669]DEBUG:launcher.core.stub: Stub stdout socket closed (15555)
[346669]DEBUG:launcher.core.stub: GDB socket closed (3333). Closing stub socket (13333)
[346669]INFO:launcher.cli.cmd.gdbserver: Disconnected from core cm7
Gdbserver on port 3333 has closed
[346670]DEBUG:launcher.core.redlinkserv: [write] exit
[346670]DEBUG:launcher.core.redlinkserv: Waiting for redlinkserv to close
[346769]DEBUG:launcher.core.redlinkserv: Redlinkserv has closed&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this some setup issue on our side? The SWD interface to the RT1176 works in general, as verified via the JLink-Base debugger. But does the MCU-Link require some special setup? Or do we miss a certain parameter in our LinkServer call?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 11:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1987927#M32473</guid>
      <dc:creator>raddeh</dc:creator>
      <dc:date>2024-11-05T11:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1988353#M32485</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I reviewed the schematic and maybe have a confusion about the SWD interface. The Interface to debug reported on the schematic is the J6. the J2 must be the SWD to communicate to the LPC55s69 not for debug.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1730857989936.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308802i84AB03B6613AF0D5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1730857989936.png" alt="Pavel_Hernandez_0-1730857989936.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_1-1730858064731.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308803iB15A7C7268D02940/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_1-1730858064731.png" alt="Pavel_Hernandez_1-1730858064731.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Could you confirm using the J6?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 01:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1988353#M32485</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-11-06T01:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1988554#M32487</link>
      <description>&lt;P&gt;Yes, I'm using the J6 port (2x5 pin connector). I mistyped in the original post&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 07:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1988554#M32487</guid>
      <dc:creator>raddeh</dc:creator>
      <dc:date>2024-11-06T07:12:36Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1989200#M32493</link>
      <description>&lt;P&gt;Hello, could you let me know what version is the RT1170 EVK or EVKB?&lt;/P&gt;
&lt;P&gt;In both cases the J1 could use the SWD with adapter to JTAG 20 pins.&lt;/P&gt;
&lt;P&gt;On the board EVKB:&lt;BR /&gt;Could use the J87 but need to put a jumper on JP5 to use the SWD 10 pins.&lt;/P&gt;
&lt;P&gt;On the board EVK:&lt;BR /&gt;The J16 is only for the debugger DFU and the J58 could use to the target MCU.&lt;/P&gt;
&lt;P&gt;I recommend do some test on these ports.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 18:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1989200#M32493</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-11-06T18:46:32Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1989872#M32498</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196430"&gt;@Pavel_Hernandez&lt;/a&gt;&amp;nbsp;it is no EVK / EVK board, but a custom one.&lt;/P&gt;&lt;P&gt;On the custom board is a RT1176AVM8A and we use T6 (SWD-CLK), U7 (SWD-IO). But like I wrote in the first post: The SWD interface to our board does work with a JLink-Base debugger. The issue is the connection via the NXP MCU-Link. So the SWD ports are OK on the board&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 07:14:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1989872#M32498</guid>
      <dc:creator>raddeh</dc:creator>
      <dc:date>2024-11-07T07:14:51Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1990543#M32512</link>
      <description>&lt;P&gt;Hello, what is the IDE that has using? maybe the MCULink is not the issue, maybe need to delete de debug configuration.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1731016694061.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/309292iBA46B3F6B79DD732/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1731016694061.png" alt="Pavel_Hernandez_0-1731016694061.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you start a communication with the J-Link and the want to use the MCU-Link and the MCU-Link has LinkServer, will need eliminate the debug configuration, when you start again the debug session the IDE will find all the probes available.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 22:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1990543#M32512</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-11-07T22:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1990888#M32516</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196430"&gt;@Pavel_Hernandez&lt;/a&gt;&amp;nbsp;I'm not using any IDE. I'm using plain GDB and the NXP LinkServer application on a terminal. The JLink Debugger is not connected to the PC or the board when I trying the MCU-Link.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;MCU-Link probe connected via SWD-IO, SWD-CLK, RST, GND, VREF. Board powered and drawing nominal power.&lt;UL&gt;&lt;LI&gt;No other debugger connected to board or PC&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;Connected MCU-Link to Ubuntu20 PC and started LinkServer application&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;LinkServer -l 5 gdbserver   MIMXRT1176xxxxx:MIMXRT1170-EVK-CM7-ONLY&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Refer to original post for the output (first large code block) of the LinkServer on the terminal&lt;/LI&gt;&lt;LI&gt;Connect GDB to the GDB-server of LinkServer&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;arm-none-eabi-gdb bin/rt117x_test_cm7.elf -ex "target remote localhost:3333"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Now the LinkServer application prints out errors and closes (see second large code block in original post)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The error prints of LinkServer indicate "Wire not connected", but I know that the SWD-IO, SWD-CLK, RST, VREF and GND lines are connected: I measured them with a multimeter and the JLink Debugger is able to connect to the RT1176 core via the same cables and connectors if I attach it instead of the MCU-Link. So I'm not understanding what's happening here - is the MCU-Link trying to use JTAG? Does it need some additional line to the ones listed? Does it need some special jumper setting? Does it need a custom "target" script (but the Link doesn't need a custom script)? If it needs a custom script, where can I find documentation about it?&lt;/P&gt;&lt;P&gt;In general I've been unable to find much documentation about MCU-Link and the LinkServer application. All documentation assumes that one uses the NXP IDE with it and even the &lt;A href="https://www.nxp.com/docs/en/user-manual/UM11931.pdf" target="_self"&gt;User Manual&lt;/A&gt; isn't describing the options of LinkServer. The &amp;nbsp; product page does not list any documents. The &lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-mcu-link:GS-MCU-LINK?section=setting-up-mculink-with-3rd-party-ides" target="_self"&gt;Getting Started page&lt;/A&gt; is not describing much either. Is there some in-depth documentation that I couldn't find?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 07:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1990888#M32516</guid>
      <dc:creator>raddeh</dc:creator>
      <dc:date>2024-11-08T07:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1991219#M32521</link>
      <description>&lt;P&gt;Please post the SWD portion of your schematic.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 18:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1991219#M32521</guid>
      <dc:creator>Littell</dc:creator>
      <dc:date>2024-11-08T18:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1991285#M32526</link>
      <description>&lt;P&gt;Hello, I recommend reviewed the boot mode that the board is, and the boot config pins, then if that is good and the error still there, I recommend do a mass erase this error "Wire ACK Fault in DAP access" is command when the MCU could not be halted by the debugger.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank"&gt;RT board recovery for debugger connect issues - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Follow the steps with the SPT tool for linux.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 22:12:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1991285#M32526</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-11-08T22:12:28Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1991376#M32534</link>
      <description>&lt;P&gt;Something I noticed that may or may not be relevant: Your LinkServer command line is&lt;/P&gt;&lt;LI-CODE lang="c"&gt;LinkServer -l 5 gdbserver   MIMXRT1176xxxxx:MIMXRT1170-EVK-CM7-ONLY&lt;/LI-CODE&gt;&lt;P&gt;...which makes me think it's for an &lt;EM&gt;EVK&lt;/EM&gt;, not an &lt;EM&gt;EVKB&lt;/EM&gt;. &amp;nbsp;What happens if you use something like&lt;/P&gt;&lt;LI-CODE lang="c"&gt;LinkServer -l 5 gdbserver   MIMXRT1176xxxxx:MIMXRT1170-EVKB-CM7-ONLY&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;...instead? &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 10 Nov 2024 14:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1991376#M32534</guid>
      <dc:creator>Littell</dc:creator>
      <dc:date>2024-11-10T14:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1992891#M32550</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234959"&gt;@Littell&lt;/a&gt;It is neither a EVK nor a EVKB, as it's a custom board. But I tried with EVKB as cmd line parameter and encountered the same error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt; LinkServer -l 5 gdbserver   MIMXRT1176xxxxx:MIMXRT1170-EVKB
[115]DEBUG:asyncio: Using selector: EpollSelector
[502]INFO:launcher.cli.utils.funcs: Exact match for MIMXRT1176xxxxx:MIMXRT1170-EVKB found
[503]INFO:launcher.cli.utils.click: Selected device MIMXRT1176xxxxx:MIMXRT1170-EVKB
[503]DEBUG:launcher.core.redlinkserv: Starting redlinkserv: /usr/local/LinkServer_24.9.75/binaries/redlinkserv ['--port', '11111', '--telnetport', '12222', '--no-telnet-defaults']
[506]DEBUG:launcher.core.probeboot: Listing usb devices
[506]DEBUG:launcher.core.utils: Subprocess exec: lsusb []
[509]DEBUG:launcher.core.redlinkserv: Connecting to redlinkserv (localhost:12222)
[514]DEBUG:launcher.core.redlinkserv: Connected to redlinkserv
[514]DEBUG:launcher.core.redlinkserv: [read] 
[515]DEBUG:launcher.core.probeboot: Found 15 USB devices
[516]INFO:launcher.cli.utils.click: Getting available probes
[516]DEBUG:launcher.core.redlinkserv: [write] probelist
[1597]DEBUG:launcher.core.redlinkserv: [read-partial] b'Index = 1\nManufacturer = NXP Semiconductors\nDescription = MCU-LINK (r0BF) CMSIS-DAP V3.148\nSerial Number = QP1Q5X3JAG0LE\nVID:PID = 1FC9:0143\nPath = 0003:0013:00\n\n\n'
[1638]DEBUG:launcher.core.redlinkserv: [read] Index = 1
Manufacturer = NXP Semiconductors
Description = MCU-LINK (r0BF) CMSIS-DAP V3.148
Serial Number = QP1Q5X3JAG0LE
VID:PID = 1FC9:0143
Path = 0003:0013:00
[1638]INFO:launcher.cli.utils.click: Selected probe #1 QP1Q5X3JAG0LE (MCU-LINK (r0BF) CMSIS-DAP V3.148)
[1639]INFO:launcher.core.redlinkserv: MCU-Link firmware update `check`: local firmware [3.148] is the same as the version running on the selected probe ([QP1Q5X3JAG0LE] [MCU-LINK (r0BF) CMSIS-DAP V3.148])
Firmware update `check`: not required - the update can be performed using `forced` mode
[1640]DEBUG:launcher.core.redlinkserv: [write] probeopenbyindex 1
[1640]DEBUG:launcher.core.redlinkserv: [read-partial] b'Probe Handle 1 Open\n'
[1682]DEBUG:launcher.core.redlinkserv: [read] Probe Handle 1 Open
[1682]DEBUG:launcher.core.redlinkserv: [write] wireswdconnect 1
[1805]DEBUG:launcher.core.redlinkserv: [read-partial] b'Error: Wire Ack Fault - target connected?\n'
[1846]DEBUG:launcher.core.redlinkserv: [read] Error: Wire Ack Fault - target connected?
[1846]DEBUG:launcher.core.redlinkserv: [write] coreconfig 1
[1846]DEBUG:launcher.core.redlinkserv: [read-partial] b'Error: Wire not connected\n'
[1890]DEBUG:launcher.core.redlinkserv: [read] Error: Wire not connected
[1890]DEBUG:launcher.core.redlinkserv: [write] corelist 1
[1890]DEBUG:launcher.core.redlinkserv: [read-partial] b'Error: Wire Ack Fault - target connected?\n'
[1934]DEBUG:launcher.core.redlinkserv: [read] Error: Wire Ack Fault - target connected?
[1934]DEBUG:launcher.cli.cmd.gdbserver: Starting stubs
[1937]DEBUG:launcher.core.stub: Wrote stub XML: /tmp/tmp9ow2bmr7/crt_directory.xml
[1938]DEBUG:launcher.core.stub: Wrote stub XML: /tmp/tmp9ow2bmr7/part.xml
[1938]DEBUG:launcher.core.stub: Internal gdbserver (3333) ports: stub_port=13333, sh_stub_port=14444, stdout_port=15555
[1940]DEBUG:launcher.core.stub: GDB server args: ['--redlink-port', '11111', '--flash-dir', '/usr/local/LinkServer_24.9.75/binaries/Flash', '-x', '/tmp/tmp9ow2bmr7', '-pMIMXRT1176xxxxx', '--vendor', 'NXP', '-g', '--cache', 'dis', '--probeserial', 'QP1Q5X3JAG0LE', '--coreindex', '0', '--kill-server', '--server', 'localhost:13333', '--telnet', '14444', '--msg-port', '15555', '--connectscript', 'RT1170_connect_M7_wake_M4.scp', '--resetscript', 'RT1170_reset.scp']
GDB server listening on port 3333 in debug mode (core cm7)
Semihosting server listening on port 4444 (core cm7)
[1947]DEBUG:launcher.core.stub: [stub (3333)] Ns: MCUXpresso IDE RedlinkMulti Driver v24.9 (Sep 19 2024 19:39:44 - crt_emu_cm_redlink build 802)
[10823]DEBUG:launcher.core.stub: Received connection to our GDB server (3333)
[10823]DEBUG:launcher.core.stub: Connected to stub's GDB port (13333)
[10823]INFO:launcher.cli.cmd.gdbserver: Connected to core cm7
[10824]DEBUG:launcher.core.stub: GDB (3333) -&amp;gt; stub (13333): b'+$qSupported:multiprocess+;swbreak+;hwbreak+;qRelocInsn+;fork-events+;vfork-events+;exec-events+;vContSupported+;QThreadEvents+;no-resumed+#df'
[10824]DEBUG:launcher.core.stub: [stub (3333)] Pc: (  0) Reading remote configuration
[10824]DEBUG:launcher.core.stub: [stub (3333)] Wc(03). No cache support.
[10824]DEBUG:launcher.core.stub: [stub (3333)] Nc: Found generic directory XML file in /tmp/tmp9ow2bmr7/crt_directory.xml
Pc: (  5) Remote configuration complete
[10824]DEBUG:launcher.core.stub: [stub (3333)] Nc: Reconnected to existing LinkServer process.
[10946]DEBUG:launcher.core.stub: [stub (3333)] Nc: Connecting to probe 1 core 0 (using server started externally) reports:
    'Ee(42). Could not connect to core.'
Nc: Retrying...
[12692]DEBUG:launcher.core.stub: [stub (3333)] Nc: Reconnected to existing LinkServer process.
[12824]DEBUG:launcher.core.stub: GDB (3333) -&amp;gt; stub (13333): b'$qSupported:multiprocess+;swbreak+;hwbreak+;qRelocInsn+;fork-events+;vfork-events+;exec-events+;vContSupported+;QThreadEvents+;no-resumed+#df'
[13316]DEBUG:launcher.core.stub: [stub (3333)] Nc: Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
[13558]DEBUG:launcher.core.stub: [stub (3333)] Wc: ============= SCRIPT: RT1170_connect_M7_wake_M4.scp =============
Wc: RT1170 Connect M7 and Wake M4 Script
Wc: Error: Wire Ack Fault - target connected?
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Setting M4 spin code
[13558]DEBUG:launcher.core.stub: [stub (3333)] Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Setting M4 clock
Wc: Error: Wire not connected
Wc: Resetting M4 core
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: View cores on the DAP AP
Wc: Error: Wire Ack Fault - target connected?
Wc: Error: Wire Ack Fault - target connected?
Wc: Error: Wire not connected
Wc: Error: Wire not connected
Wc: ============= END SCRIPT ========================================
[13682]DEBUG:launcher.core.stub: [stub (3333)] Ed:02: Failed on connect: Ee(42). Could not connect to core.
Et:31: No connection to chip's debug port
Pc: (100) Target Operation Failed
[13682]DEBUG:launcher.core.stub: Stub stdout socket closed (15555)
[13683]DEBUG:launcher.core.stub: Stub socket closed (13333). Closing GDB socket (3333)
[13683]DEBUG:launcher.core.stub: GDB socket closed (3333). Closing stub socket (13333)
Gdbserver on port 3333 has closed
[13684]INFO:launcher.cli.cmd.gdbserver: Disconnected from core cm7
[13685]DEBUG:launcher.core.redlinkserv: [write] exit
[13685]DEBUG:launcher.core.redlinkserv: Waiting for redlinkserv to close
[13784]DEBUG:launcher.core.redlinkserv: Redlinkserv has closed&lt;/LI-CODE&gt;</description>
      <pubDate>Tue, 12 Nov 2024 14:10:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1992891#M32550</guid>
      <dc:creator>raddeh</dc:creator>
      <dc:date>2024-11-12T14:10:37Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1992896#M32551</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234959"&gt;@Littell&lt;/a&gt;I'm unable to post direct schematics as per company policy. But multiple people verified the pin connections &lt;EM&gt;it works when using a JLink&lt;/EM&gt; &lt;EM&gt;debugger. &lt;/EM&gt;Th&lt;EM&gt;is&lt;/EM&gt; points me to it being a configuration error on the LinkServer tool side...&lt;/P&gt;&lt;P&gt;I don't want a flash erase, I just want connection to the stopped uC and then upload code to internal RAM. The external flash is anyways another than on the EVK/EVKB board, so I don't expect a driver for it to be part of the LinkServer. That's the same we do as when we use the JLink: connect to the core and upload to the internal RAM and then start execution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe I need a custom script for the LinkServer tool? But I can't find documentation about it anywhere. &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196430"&gt;@Pavel_Hernandez&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 14:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1992896#M32551</guid>
      <dc:creator>raddeh</dc:creator>
      <dc:date>2024-11-12T14:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1992906#M32552</link>
      <description>&lt;P&gt;Bummer.&amp;nbsp; Sorry, I thought the EVK/EVKB distinction would make a difference as the EVKB uses an MCU-Link equivalent.&amp;nbsp; Good luck.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 14:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1992906#M32552</guid>
      <dc:creator>Littell</dc:creator>
      <dc:date>2024-11-12T14:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1993006#M32553</link>
      <description>&lt;P&gt;Could it be a cable problem from the MCU-Link to your board?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 18:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/1993006#M32553</guid>
      <dc:creator>Littell</dc:creator>
      <dc:date>2024-11-12T18:03:36Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging RT1176 with MCU-Link and GDB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/2011387#M32889</link>
      <description>&lt;P&gt;Hi raddeh,&lt;/P&gt;
&lt;P&gt;Looks like you werent able to resolve this problem? If that's the case and you still want to troubleshoot, could you:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Confirm what supply voltage you are using&lt;/LI&gt;
&lt;LI&gt;Let us know what pull ups/downs you have on the SWD connections (if any)&lt;/LI&gt;
&lt;LI&gt;Let us know what is connected to pins 7, 8, 9 and 10 on your board&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 00:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugging-RT1176-with-MCU-Link-and-GDB/m-p/2011387#M32889</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2024-12-11T00:10:35Z</dc:date>
    </item>
  </channel>
</rss>