<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to enter SEMC SDRAM into low power in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-enter-SEMC-SDRAM-into-low-power/m-p/1963795#M31995</link>
    <description>&lt;P&gt;We are using a imxrt106F, with VDD_HIGH_IN, SNVS_IN, and DCDC_IN tied together. However the issue we see is entering into SNVS does not automatically put the SDRAM into low power mode as our SDRAM is constantly powered. We are seeing very high power consumption. How can we put the SDRAM into low power mode?&lt;/P&gt;</description>
    <pubDate>Sat, 28 Sep 2024 01:06:41 GMT</pubDate>
    <dc:creator>rjengr</dc:creator>
    <dc:date>2024-09-28T01:06:41Z</dc:date>
    <item>
      <title>How to enter SEMC SDRAM into low power</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-enter-SEMC-SDRAM-into-low-power/m-p/1963795#M31995</link>
      <description>&lt;P&gt;We are using a imxrt106F, with VDD_HIGH_IN, SNVS_IN, and DCDC_IN tied together. However the issue we see is entering into SNVS does not automatically put the SDRAM into low power mode as our SDRAM is constantly powered. We are seeing very high power consumption. How can we put the SDRAM into low power mode?&lt;/P&gt;</description>
      <pubDate>Sat, 28 Sep 2024 01:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-enter-SEMC-SDRAM-into-low-power/m-p/1963795#M31995</guid>
      <dc:creator>rjengr</dc:creator>
      <dc:date>2024-09-28T01:06:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to enter SEMC SDRAM into low power</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-enter-SEMC-SDRAM-into-low-power/m-p/1965887#M32045</link>
      <description>&lt;P&gt;If the SDRAM has a low power mode then you need to enter the command to send it to low power before setting the mcu at SNVS mode.&lt;/P&gt;
&lt;P&gt;Ideally, SDRAM is powered-off on SNVS mode since external DC/DC(which powers SDRAM) is turned off.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_0-1727894242690.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/302394i15846C7271422CB7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_0-1727894242690.png" alt="Omar_Anguiano_0-1727894242690.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 02 Oct 2024 18:37:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-enter-SEMC-SDRAM-into-low-power/m-p/1965887#M32045</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2024-10-02T18:37:37Z</dc:date>
    </item>
  </channel>
</rss>