<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with iMXRT1064 EVK + RIVERDI RVT70HSTNWC00-B 7inch display + GUIX in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-iMXRT1064-EVK-RIVERDI-RVT70HSTNWC00-B-7inch-display/m-p/1961778#M31954</link>
    <description>Hi,&lt;BR /&gt;Did you get above issue resolved in using a Riverdi Display and NXP code?&lt;BR /&gt;Did you also get the touchpanel from Riverdi working on that?&lt;BR /&gt;Could you make this touchpanel operating using a default fsl_ft5406 or fsl_gt911 touchpanel drivers? Or did you use Riverdi specific drivers for that? Any assistance is mostly appreciated.&lt;BR /&gt;</description>
    <pubDate>Wed, 25 Sep 2024 12:21:11 GMT</pubDate>
    <dc:creator>sven61508</dc:creator>
    <dc:date>2024-09-25T12:21:11Z</dc:date>
    <item>
      <title>Problem with iMXRT1064 EVK + RIVERDI RVT70HSTNWC00-B 7inch display + GUIX</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-iMXRT1064-EVK-RIVERDI-RVT70HSTNWC00-B-7inch-display/m-p/1639158#M24783</link>
      <description>&lt;P&gt;We are facing similar issue like this thread -&amp;gt;&amp;nbsp; &lt;A href="https://community.nxp.com/t5/i-MX-RT/i-MX-RT-eLCDIF-RGB-Mode-Use-Case/mp/981839" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/i-MX-RT-eLCDIF-RGB-Mode-Use-Case/mp/981839&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Configuration:&lt;/P&gt;&lt;P&gt;- 1024*600 display(RGB 565) - will convert it to RGB 888 later&lt;/P&gt;&lt;P&gt;- Using HS/VS mode instead of DE mode - As per RIVERDI display datasheet(attached)&lt;/P&gt;&lt;P&gt;- Started with sample example of&amp;nbsp;RK043FN02H-CT display panel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question -1: Are below setting correct?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="godcks91_0-1682364951029.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220617iE013D45FC08CC0B5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="godcks91_0-1682364951029.png" alt="godcks91_0-1682364951029.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;godcks91_0-1682364951029.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;#define APP_HSW 1&lt;BR /&gt;#define APP_HFP 16&lt;BR /&gt;#define APP_HBP 160&lt;BR /&gt;#define APP_VSW 1&lt;BR /&gt;#define APP_VFP 1&lt;BR /&gt;#define APP_VBP 23&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question-2:&lt;/P&gt;&lt;P&gt;Below postDivider cannot be changed to 16 - We need Clock between 44.3 to 63.&amp;nbsp; postDivider = 16 does not make any change in the clock. Is there any limitation to below equation? When I use loopDivider = 27 and postDivider = 8 - screen glows to white.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="godcks91_1-1682365034838.png" style="width: 471px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220618iADE79FF36D690A36/image-dimensions/471x106?v=v2" width="471" height="106" role="button" title="godcks91_1-1682365034838.png" alt="godcks91_1-1682365034838.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;godcks91_1-1682365034838.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I do additional changes for clock - as per below snip - screen stopped glowing white but show few random lines. My frame buffer was not fully set as I did not use SDRAM for frame buffer.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="godcks91_4-1682365640482.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220621i91A9C951AD500456/image-size/medium?v=v2&amp;amp;px=400" role="button" title="godcks91_4-1682365640482.png" alt="godcks91_4-1682365640482.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;godcks91_4-1682365640482.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Question-3:&lt;/P&gt;&lt;P&gt;I have tried to use SDRAM(32MB) area for Non-Cachable region to store Frame buffer. Configured SDRAM to 27MB and allocate 5MB to Non-Cachable region. Is there any issue with this configuration? When I used SDRAM region like this - screen stopped glowing white - nothing on the screen - even some debug print stopped coming.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="godcks91_2-1682365403890.png" style="width: 596px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220619i747AB5E7FC75154A/image-dimensions/596x121?v=v2" width="596" height="121" role="button" title="godcks91_2-1682365403890.png" alt="godcks91_2-1682365403890.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;godcks91_2-1682365403890.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="godcks91_3-1682365446119.png" style="width: 612px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220620iA42AD57A8407D070/image-dimensions/612x222?v=v2" width="612" height="222" role="button" title="godcks91_3-1682365446119.png" alt="godcks91_3-1682365446119.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;godcks91_3-1682365446119.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I even tried with above setting and stopping I &amp;amp; D cache like below&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="godcks91_5-1682365728745.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220622i934FEA6B0FBB819D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="godcks91_5-1682365728745.png" alt="godcks91_5-1682365728745.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;godcks91_5-1682365728745.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question - 4:&lt;/P&gt;&lt;P&gt;Is it okay to use -&amp;gt; #define FRAME_BUFFER_ALIGN 32 ? In example provided with imxrt1064 evk - it is 64.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone please help us? We are trying to solve above issues for many days without any luck.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;- CS&lt;/P&gt;</description>
      <pubDate>Mon, 24 Apr 2023 19:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-iMXRT1064-EVK-RIVERDI-RVT70HSTNWC00-B-7inch-display/m-p/1639158#M24783</guid>
      <dc:creator>godcks91</dc:creator>
      <dc:date>2023-04-24T19:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with iMXRT1064 EVK + RIVERDI RVT70HSTNWC00-B 7inch display + GUIX</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-iMXRT1064-EVK-RIVERDI-RVT70HSTNWC00-B-7inch-display/m-p/1961778#M31954</link>
      <description>Hi,&lt;BR /&gt;Did you get above issue resolved in using a Riverdi Display and NXP code?&lt;BR /&gt;Did you also get the touchpanel from Riverdi working on that?&lt;BR /&gt;Could you make this touchpanel operating using a default fsl_ft5406 or fsl_gt911 touchpanel drivers? Or did you use Riverdi specific drivers for that? Any assistance is mostly appreciated.&lt;BR /&gt;</description>
      <pubDate>Wed, 25 Sep 2024 12:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-iMXRT1064-EVK-RIVERDI-RVT70HSTNWC00-B-7inch-display/m-p/1961778#M31954</guid>
      <dc:creator>sven61508</dc:creator>
      <dc:date>2024-09-25T12:21:11Z</dc:date>
    </item>
  </channel>
</rss>