<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: MCUXpresso Secure Provisioning error while configuring flash boot memory</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-Secure-Provisioning-error-while-configuring-flash/m-p/1959186#M31896</link>
    <description>&lt;P&gt;After a little digging, I've come up with an idea, that the provisioning software is using another version of the library, probably being distributed alongside it.&lt;/P&gt;&lt;P&gt;So, after searching in my file system, I found a libreadline.so.8 binary under&amp;nbsp;/opt/nxp/MCUX_Provi_v8/bin/_internal/. After removing it, the tool could load the system installed&amp;nbsp;libreadline.so.8.2 and the ext_memory_setup.sh script worked as intended.&lt;/P&gt;&lt;P&gt;Seens that a litte version bump in the provisiong tool libreadline to 8.2 would resolve the problem for linux users.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 22 Sep 2024 00:39:33 GMT</pubDate>
    <dc:creator>piOverThree</dc:creator>
    <dc:date>2024-09-22T00:39:33Z</dc:date>
    <item>
      <title>MCUXpresso Secure Provisioning error while configuring flash boot memory</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-Secure-Provisioning-error-while-configuring-flash/m-p/1959185#M31895</link>
      <description>&lt;P&gt;Hello people. So, while using the secure provisioning software to flash a image to my EVKBIMXRT105 dev board I encountered this error in the Boot config menu:&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Status of the operation: SUCCESS: Settings loaded successfully; workspace: `/home/user/source/imxExamples/usb_device_video_virtual_camera/bm/provisioning`
Executing script /home/user/source/imxExamples/usb_device_video_virtual_camera/bm/provisioning/ext_memory_setup.sh
ERROR: Script failed with return code: [2]ERROR
### SCRIPT: Initialize external memory: /home/user/source/imxExamples/usb_device_video_virtual_camera/bm/provisioning/ext_memory_setup.sh
/bin/bash: symbol lookup error: /bin/bash: undefined symbol: rl_trim_arg_from_keyseq

### RESULT of the script `Initialize external memory`: FAILURE (return code = [2]ERROR)
Status of the operation: FAILURE: Initialize external memory&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems like there is an error related to the libreadline. Any help diagnosing this problem would be nice!&lt;/P&gt;&lt;P&gt;My setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;OS: Archlinux, Kernel 6.10&lt;/LI&gt;&lt;LI&gt;librealine: readline 8.2&lt;/LI&gt;&lt;LI&gt;MCUXpresso Secure Provisioning: v8.0&lt;/LI&gt;&lt;LI&gt;Board:&amp;nbsp; EVKBIMXRT105&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Sun, 22 Sep 2024 00:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-Secure-Provisioning-error-while-configuring-flash/m-p/1959185#M31895</guid>
      <dc:creator>piOverThree</dc:creator>
      <dc:date>2024-09-22T00:34:51Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Secure Provisioning error while configuring flash boot memory</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-Secure-Provisioning-error-while-configuring-flash/m-p/1959186#M31896</link>
      <description>&lt;P&gt;After a little digging, I've come up with an idea, that the provisioning software is using another version of the library, probably being distributed alongside it.&lt;/P&gt;&lt;P&gt;So, after searching in my file system, I found a libreadline.so.8 binary under&amp;nbsp;/opt/nxp/MCUX_Provi_v8/bin/_internal/. After removing it, the tool could load the system installed&amp;nbsp;libreadline.so.8.2 and the ext_memory_setup.sh script worked as intended.&lt;/P&gt;&lt;P&gt;Seens that a litte version bump in the provisiong tool libreadline to 8.2 would resolve the problem for linux users.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 22 Sep 2024 00:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-Secure-Provisioning-error-while-configuring-flash/m-p/1959186#M31896</guid>
      <dc:creator>piOverThree</dc:creator>
      <dc:date>2024-09-22T00:39:33Z</dc:date>
    </item>
  </channel>
</rss>