<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Custom bootloader imxrt1170 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Custom-bootloader-imxrt1170/m-p/1956994#M31851</link>
    <description>&lt;P&gt;As they say, "Good luck with that."&amp;nbsp; Hopefully this will help some: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12564.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12564.pdf&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 18 Sep 2024 22:47:00 GMT</pubDate>
    <dc:creator>Littell</dc:creator>
    <dc:date>2024-09-18T22:47:00Z</dc:date>
    <item>
      <title>Custom bootloader imxrt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Custom-bootloader-imxrt1170/m-p/1956331#M31841</link>
      <description>&lt;P&gt;I am trying to port already existing boot firmware from STM platform to IMXRT platform.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have 2 QSPI Flashes. First one is executing the code only and the second is for storing some data.&lt;/P&gt;&lt;P&gt;I am also trying to add boot firmware to the second one. Every boot time, I will start to run from the second QSPI flash. If no new firmware is upgraded/loaded within a pre-defined time interval, I will start to execute main app program in&amp;nbsp;first QSPI. At that time I am also trying to force second QSPI flash to "read/write" mode thereafter. However I could not find a way how to do that. Can you give me any example or show me a way of doing it?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 07:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Custom-bootloader-imxrt1170/m-p/1956331#M31841</guid>
      <dc:creator>burhanhagi</dc:creator>
      <dc:date>2024-09-18T07:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: Custom bootloader imxrt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Custom-bootloader-imxrt1170/m-p/1956994#M31851</link>
      <description>&lt;P&gt;As they say, "Good luck with that."&amp;nbsp; Hopefully this will help some: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12564.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12564.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 22:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Custom-bootloader-imxrt1170/m-p/1956994#M31851</guid>
      <dc:creator>Littell</dc:creator>
      <dc:date>2024-09-18T22:47:00Z</dc:date>
    </item>
  </channel>
</rss>