<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： MIMXRT1170 EVK JLink Verification failed in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-JLink-Verification-failed/m-p/1956367#M31842</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240565"&gt;@spencermacdonald&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well!&lt;/P&gt;
&lt;P&gt;I'm not sure if your jumper cap configuration has changed, so the first thing we recommend is that you follow this document for testing:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/Using-J-Link-with-MIMXRT1170-EVKB/ta-p/1715138" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/Using-J-Link-with-MIMXRT1170-EVKB/ta-p/1715138&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, you are using the JLink firmware for the on-board debugger, so I'm sure you are already familiar with how to update/replace the firmware for the on-board debugger. It is recommended to update to the latest version first. If you still have problems, please feel free to continue to discuss.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;(The new version of the script for replacing the debugger firmware moved here : &lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/linkserver-for-microcontrollers:LINKERSERVER)" target="_blank"&gt;https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/linkserver-for-microcontrollers:LINKERSERVER)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Gavin_Jia_0-1726645528623.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/299633i6BAFE71C7E6E4042/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Gavin_Jia_0-1726645528623.png" alt="Gavin_Jia_0-1726645528623.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 18 Sep 2024 07:45:46 GMT</pubDate>
    <dc:creator>Gavin_Jia</dc:creator>
    <dc:date>2024-09-18T07:45:46Z</dc:date>
    <item>
      <title>MIMXRT1170 EVK JLink Verification failed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-JLink-Verification-failed/m-p/1955204#M31825</link>
      <description>&lt;P&gt;When trying to flash the&amp;nbsp;MIMXRT1170 EVK&amp;nbsp; using the onboard JLink.&amp;nbsp; USB cable is connected to J11. I'm getting the following error.&amp;nbsp; Sometimes the board is successfully fleshed and runs the updated application other times it fails and doesn't boot.&amp;nbsp; I've tried different host PC's boards and USB cables.&amp;nbsp; Any ideas would be appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;$ west -v flash --build-dir ../test_blinky&lt;BR /&gt;-- west flash: rebuilding&lt;BR /&gt;cmake version 3.30.1 is OK; minimum version is 3.13.1&lt;BR /&gt;Running CMake: 'C:\Program Files\CMake\bin\cmake.EXE' --build ../test_blinky&lt;BR /&gt;ninja: no work to do.&lt;BR /&gt;[0/3] Performing build step for 'blinky'&lt;BR /&gt;[2/3] No install step for 'blinky'&lt;BR /&gt;[3/3] Completed 'blinky'&lt;BR /&gt;-- west flash: using runner jlink&lt;BR /&gt;-- runners.jlink: reset after flashing requested&lt;BR /&gt;runners.jlink: JLINKARM_GetDLLVersion()=79402&lt;BR /&gt;-- runners.jlink: JLink version: 7.94b&lt;BR /&gt;runners.jlink: JLink commander script:&lt;BR /&gt;ExitOnError 1&lt;BR /&gt;r&lt;BR /&gt;LE&lt;BR /&gt;loadfile "C:\Dev\VSCode\Phoenix\mani-test\test_blinky\blinky\zephyr\zephyr.bin" 0x30000000&lt;BR /&gt;r&lt;BR /&gt;g&lt;BR /&gt;writeDP 1 0&lt;BR /&gt;readDP 1&lt;BR /&gt;q&lt;BR /&gt;-- runners.jlink: Flashing file: C:\Dev\VSCode\mani-test\test_blinky\blinky\zephyr\zephyr.bin&lt;BR /&gt;runners.jlink: 'C:\Program Files\SEGGER\JLink\JLink.exe' -nogui 1 -if swd -speed auto -device MIMXRT1176xxxA_M7 -CommanderScript 'C:\Users\MacDonaS\AppData\Local\Temp\tmpcgv8kpyejlink\runner.jlink' -nogui 1&lt;BR /&gt;SEGGER J-Link Commander V7.94b (Compiled Dec 13 2023 17:07:41)&lt;BR /&gt;DLL version V7.94b, compiled Dec 13 2023 17:05:52&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;J-Link Command File read successfully.&lt;BR /&gt;Processing script file...&lt;BR /&gt;J-Link&amp;gt;ExitOnError 1&lt;BR /&gt;J-Link Commander will now exit on Error&lt;BR /&gt;J-Link&amp;gt;r&lt;BR /&gt;J-Link connection not established yet but required for command.&lt;BR /&gt;Connecting to J-Link via USB...O.K.&lt;BR /&gt;Firmware: J-Link LPCXpresso V2 compiled Apr 4 2019 16:54:03&lt;BR /&gt;Hardware version: V1.00&lt;BR /&gt;J-Link uptime (since boot): N/A (Not supported by this model)&lt;BR /&gt;S/N: 721381573&lt;BR /&gt;VTref=3.300V&lt;BR /&gt;Target connection not established yet but required for command.&lt;BR /&gt;Device "MIMXRT1176XXXA_M7" selected.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Connecting to target via SWD&lt;BR /&gt;Found SW-DP with ID 0x6BA02477&lt;BR /&gt;DPv0 detected&lt;BR /&gt;CoreSight SoC-400 or earlier&lt;BR /&gt;Scanning AP map to find all available APs&lt;BR /&gt;AP[3]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;AP[0]: AHB-AP (IDR: 0x84770001)&lt;BR /&gt;AP[1]: AHB-AP (IDR: 0x24770011)&lt;BR /&gt;AP[2]: APB-AP (IDR: 0x54770002)&lt;BR /&gt;Iterating through AP map to find AHB-AP to use&lt;BR /&gt;AP[0]: Core found&lt;BR /&gt;AP[0]: AHB-AP ROM base: 0xE00FD000&lt;BR /&gt;CPUID register: 0x411FC272. Implementer code: 0x41 (ARM)&lt;BR /&gt;Cache: L1 I/D-cache present&lt;BR /&gt;Found Cortex-M7 r1p2, Little endian.&lt;BR /&gt;FPUnit: 8 code (BP) slots and 0 literal slots&lt;BR /&gt;CoreSight components:&lt;BR /&gt;ROMTbl[0] @ E00FD000&lt;BR /&gt;[0][0]: E00FE000 CID B105100D PID 000BB4C8 ROM Table&lt;BR /&gt;ROMTbl[1] @ E00FE000&lt;BR /&gt;[1][0]: E00FF000 CID B105100D PID 000BB4C7 ROM Table&lt;BR /&gt;ROMTbl[2] @ E00FF000&lt;BR /&gt;[2][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7&lt;BR /&gt;[2][1]: E0001000 CID B105E00D PID 000BB002 DWT&lt;BR /&gt;[2][2]: E0002000 CID B105E00D PID 000BB00E FPB-M7&lt;BR /&gt;[2][3]: E0000000 CID B105E00D PID 000BB001 ITM&lt;BR /&gt;[1][1]: E0041000 CID B105900D PID 001BB975 ETM-M7&lt;BR /&gt;[1][2]: E0042000 CID B105900D PID 004BB906 CTI&lt;BR /&gt;[0][1]: E0043000 CID B105900D PID 001BB908 CSTF&lt;BR /&gt;I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way&lt;BR /&gt;D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way&lt;BR /&gt;Memory zones:&lt;BR /&gt;Zone: "Default" Description: Default access mode&lt;BR /&gt;Cortex-M7 identified.&lt;BR /&gt;Reset delay: 0 ms&lt;BR /&gt;Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.&lt;BR /&gt;Reset: Halt core after reset via DEMCR.VC_CORERESET.&lt;BR /&gt;Reset: Reset device via AIRCR.SYSRESETREQ.&lt;BR /&gt;Core did not halt after reset, halting it manually.&lt;BR /&gt;AfterResetTarget() start&lt;BR /&gt;Valid application detected. Setting PC / SP manually.&lt;BR /&gt;Booting from FlexSPI1.&lt;BR /&gt;PC = 0x30003539&lt;BR /&gt;SP = 0x80001100&lt;BR /&gt;Clean &amp;amp; invalidate cached CPU registers&lt;BR /&gt;AfterResetTarget() end - Took 61.8ms&lt;BR /&gt;J-Link&amp;gt;LE&lt;BR /&gt;J-Link&amp;gt;loadfile "C:\Dev\VSCode\mani-test\test_blinky\blinky\zephyr\zephyr.bin" 0x30000000&lt;BR /&gt;'loadfile': Performing implicit reset &amp;amp; halt of MCU.&lt;BR /&gt;Reset: Halt core after reset via DEMCR.VC_CORERESET.&lt;BR /&gt;Reset: Reset device via AIRCR.SYSRESETREQ.&lt;BR /&gt;Reset: Core did not halt after reset, trying to disable WDT.&lt;BR /&gt;Reset: Halt core after reset via DEMCR.VC_CORERESET.&lt;BR /&gt;Reset: Reset device via AIRCR.SYSRESETREQ.&lt;BR /&gt;Core did not halt after reset, halting it manually.&lt;BR /&gt;AfterResetTarget() start&lt;BR /&gt;Valid application detected. Setting PC / SP manually.&lt;BR /&gt;Booting from FlexSPI1.&lt;BR /&gt;PC = 0x30003539&lt;BR /&gt;SP = 0x80001100&lt;BR /&gt;Clean &amp;amp; invalidate cached CPU registers&lt;BR /&gt;AfterResetTarget() end - Took 62.2ms&lt;BR /&gt;Downloading file [C:\Dev\VSCode\mani-test\test_blinky\blinky\zephyr\zephyr.bin]...&lt;BR /&gt;Comparing flash [100%] Done.&lt;BR /&gt;Erasing flash [100%] Done.&lt;BR /&gt;Programming flash [100%] Done.&lt;BR /&gt;Verifying flash [100%] Done.&lt;BR /&gt;J-Link: Flash download: Bank 0 @ 0x30000000: 1 range affected (65536 bytes)&lt;BR /&gt;J-Link: Flash download: Total: 1.216s (Prepare: 0.260s, Compare: 0.203s, Erase: 0.123s, Program: 0.287s, Verify: 0.202s, Restore: 0.138s)&lt;BR /&gt;J-Link: Flash download: Program speed: 223 KB/s&lt;/P&gt;&lt;P&gt;****** Error: Verification failed @ address 0x30000000&lt;BR /&gt;Error while programming flash: Verify failed.&lt;/P&gt;&lt;P&gt;Script processing completed.&lt;/P&gt;&lt;P&gt;FATAL ERROR: command exited with status 1: 'C:\Program Files\SEGGER\JLink\JLink.exe' -nogui 1 -if swd -speed auto -device MIMXRT1176xxxA_M7 -CommanderScript 'C:\Users\MacDonaS\AppData\Local\Temp\tmpcgv8kpyejlink\runner.jlink' -nogui 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Sep 2024 12:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-JLink-Verification-failed/m-p/1955204#M31825</guid>
      <dc:creator>spencermacdonald</dc:creator>
      <dc:date>2024-09-16T12:57:55Z</dc:date>
    </item>
    <item>
      <title>回复： MIMXRT1170 EVK JLink Verification failed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-JLink-Verification-failed/m-p/1956367#M31842</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240565"&gt;@spencermacdonald&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well!&lt;/P&gt;
&lt;P&gt;I'm not sure if your jumper cap configuration has changed, so the first thing we recommend is that you follow this document for testing:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/Using-J-Link-with-MIMXRT1170-EVKB/ta-p/1715138" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/Using-J-Link-with-MIMXRT1170-EVKB/ta-p/1715138&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, you are using the JLink firmware for the on-board debugger, so I'm sure you are already familiar with how to update/replace the firmware for the on-board debugger. It is recommended to update to the latest version first. If you still have problems, please feel free to continue to discuss.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;(The new version of the script for replacing the debugger firmware moved here : &lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/linkserver-for-microcontrollers:LINKERSERVER)" target="_blank"&gt;https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/linkserver-for-microcontrollers:LINKERSERVER)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Gavin_Jia_0-1726645528623.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/299633i6BAFE71C7E6E4042/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Gavin_Jia_0-1726645528623.png" alt="Gavin_Jia_0-1726645528623.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 07:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-JLink-Verification-failed/m-p/1956367#M31842</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-09-18T07:45:46Z</dc:date>
    </item>
  </channel>
</rss>