<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: RT1170 usb dev hid detection problem</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-usb-dev-hid-detection-problem/m-p/1952739#M31789</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209213"&gt;@dskim2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Due to the complexity and dependencies of the FlexSPI example code, I would recommend you port the USB capabilities to the FlexSPI example, rather than the FlexSPI capabilities to the USB example. On the&amp;nbsp;&lt;SPAN&gt;evkbmimxrt1170_flexspi_nor_polling_transfer_cm7, add the USB component using the&amp;nbsp;"Manage SDK components" window, and then copy and paste the code from&amp;nbsp;evkbmimxrt1170_dev_hid_generic_bm_cm7 that you wish to incorporate into the project.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR,&lt;BR /&gt;Edwin.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Sep 2024 22:49:47 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2024-09-11T22:49:47Z</dc:date>
    <item>
      <title>RT1170 usb dev hid detection problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-usb-dev-hid-detection-problem/m-p/1949740#M31755</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I tested&amp;nbsp;evkbmimxrt1170_dev_hid_generic_bm_cm7 example with MiMXRT1170-EVKB.&lt;/P&gt;&lt;P&gt;It is work well.&lt;/P&gt;&lt;P&gt;I want to use&amp;nbsp;flexspi nor flash and dev hid usb in the same project.&lt;/P&gt;&lt;P&gt;I added the linkscript from evkbmimxrt1170_flexspi_nor_polling_transfer_cm7 to evkbmimxrt1170_dev_hid_generic_bm_cm7.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dskim2_3-1725861428797.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/297803iAC6F1F231B53B5FF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dskim2_3-1725861428797.png" alt="dskim2_3-1725861428797.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the EVK was not detected.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dskim2_1-1725861365712.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/297801i7AB90C81A7A1A127/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dskim2_1-1725861365712.png" alt="dskim2_1-1725861365712.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If linkscript is not added to the project, the USB is recognized, but flash related functions do not work.&lt;/P&gt;&lt;P&gt;How can I solve this?&lt;/P&gt;&lt;P&gt;Please see attatched source zip file.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 06:03:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-usb-dev-hid-detection-problem/m-p/1949740#M31755</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2024-09-09T06:03:05Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 usb dev hid detection problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-usb-dev-hid-detection-problem/m-p/1952739#M31789</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209213"&gt;@dskim2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Due to the complexity and dependencies of the FlexSPI example code, I would recommend you port the USB capabilities to the FlexSPI example, rather than the FlexSPI capabilities to the USB example. On the&amp;nbsp;&lt;SPAN&gt;evkbmimxrt1170_flexspi_nor_polling_transfer_cm7, add the USB component using the&amp;nbsp;"Manage SDK components" window, and then copy and paste the code from&amp;nbsp;evkbmimxrt1170_dev_hid_generic_bm_cm7 that you wish to incorporate into the project.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR,&lt;BR /&gt;Edwin.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 22:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-usb-dev-hid-detection-problem/m-p/1952739#M31789</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-09-11T22:49:47Z</dc:date>
    </item>
  </channel>
</rss>