<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: problem USB HID Generic interrupt</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1948817#M31741</link>
    <description>&lt;P&gt;Is there any solution?&lt;/P&gt;&lt;P&gt;I can't solve this issue&lt;/P&gt;</description>
    <pubDate>Fri, 06 Sep 2024 06:59:35 GMT</pubDate>
    <dc:creator>dskim2</dc:creator>
    <dc:date>2024-09-06T06:59:35Z</dc:date>
    <item>
      <title>problem USB HID Generic interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1810622#M28941</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;When I built and ran the usb dev_hid_generic_bm_cm7 sample source on the RT1170 EVK board, it worked without problem.&lt;/P&gt;&lt;P&gt;However, when I added and activated linkscrip to delete and record data in QSPIFlash, a phenomenon occurred in which the board was not recognized when connected to the PC USB port.&lt;/P&gt;&lt;P&gt;As a result of debugging the USB_OTG1_IRQHandler interrupt function, a phenomenon occurred in which kUSB_DeviceEventGetStringDescriptor was not received after receiving the kUSB_DeviceEventBusReset response.&lt;/P&gt;&lt;P&gt;Upload the linkscript file in the attachment.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 06:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1810622#M28941</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2024-02-19T06:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: problem USB HID Generic interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1816898#M29067</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209213"&gt;@dskim2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I believe the following blog post will prove very useful for your inquiry.&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2021/05/26/placing-code-in-sections-with-managed-gnu-linker-scripts/" target="_blank"&gt;Placing Code in Sections with managed GNU Linker Scripts | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It goes into the details on how to adequately manage linker scripts with MCUXpresso. Let me know if it helps.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 23:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1816898#M29067</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-02-27T23:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: problem USB HID Generic interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1816954#M29071</link>
      <description>&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;I modified the script and moved the execution parts of *flexspi_nor_flash_ops.o(.text*) and *fsl_flexspi.o(.text*) to another SDRAM, but it did not solve the problem.&lt;/P&gt;&lt;P&gt;My requirement is to use QSPI Flash and USB HID communication function simultaneously.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Upload the the source file in the attachment.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 02:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1816954#M29071</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2024-02-28T02:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: problem USB HID Generic interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1948817#M31741</link>
      <description>&lt;P&gt;Is there any solution?&lt;/P&gt;&lt;P&gt;I can't solve this issue&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 06:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/problem-USB-HID-Generic-interrupt/m-p/1948817#M31741</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2024-09-06T06:59:35Z</dc:date>
    </item>
  </channel>
</rss>