<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: i.mx RT 1175 SDRAM J-Link Boot Scripts</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT-1175-SDRAM-J-Link-Boot-Scripts/m-p/1917632#M31330</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Please refer to this post to enable debugging on SDRAM:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-debugging-when-application-is-built-for-SDRAM/td-p/1373296" target="_blank"&gt;Solved: RT1170 debugging when application is built for SDRAM - NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Thu, 25 Jul 2024 23:53:15 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2024-07-25T23:53:15Z</dc:date>
    <item>
      <title>i.mx RT 1175 SDRAM J-Link Boot Scripts</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT-1175-SDRAM-J-Link-Boot-Scripts/m-p/1912425#M31276</link>
      <description>&lt;P&gt;Having issue with connecting/interfacing J-Link to i.MX RT 1175 M7 core using SDRAM. Seen a post with M4 code but not M7. From everything seen on NXP's documentation, M7 boots first. R&lt;SPAN&gt;unning an SDK example on SDRAM will fail on the eval board when using a J-link or PE Micro programmer.&amp;nbsp; However, the same program runs fine on the eval board when using the built in LS programmer.&amp;nbsp; If it is an SDK example that runs off internal memory, then all three programmers work fine.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jul 2024 16:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT-1175-SDRAM-J-Link-Boot-Scripts/m-p/1912425#M31276</guid>
      <dc:creator>MichaelC_Future</dc:creator>
      <dc:date>2024-07-19T16:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx RT 1175 SDRAM J-Link Boot Scripts</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT-1175-SDRAM-J-Link-Boot-Scripts/m-p/1917632#M31330</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Please refer to this post to enable debugging on SDRAM:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-debugging-when-application-is-built-for-SDRAM/td-p/1373296" target="_blank"&gt;Solved: RT1170 debugging when application is built for SDRAM - NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 23:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-mx-RT-1175-SDRAM-J-Link-Boot-Scripts/m-p/1917632#M31330</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2024-07-25T23:53:15Z</dc:date>
    </item>
  </channel>
</rss>