<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Communication protocol between IMX8 and RT1052 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Communication-protocol-between-IMX8-and-RT1052/m-p/1899817#M31121</link>
    <description>&lt;P&gt;The bandwidth will depend on the protocol used for communication.&lt;BR /&gt;You can opt to use LPSPI or ethernet for the communication between devices.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jul 2024 00:34:35 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2024-07-05T00:34:35Z</dc:date>
    <item>
      <title>Communication protocol between IMX8 and RT1052</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Communication-protocol-between-IMX8-and-RT1052/m-p/1895813#M31043</link>
      <description>&lt;P&gt;Hi,sir&lt;/P&gt;&lt;P&gt;Requirements:&lt;BR /&gt;The system requires data interaction between RT1052 and IMX8, and the wider the rate, the better&lt;/P&gt;&lt;P&gt;What is the maximum bandwidth communication mode between imx8 and RT1052?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 09:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Communication-protocol-between-IMX8-and-RT1052/m-p/1895813#M31043</guid>
      <dc:creator>jiaxin</dc:creator>
      <dc:date>2024-06-28T09:18:14Z</dc:date>
    </item>
    <item>
      <title>回复： Communication protocol between IMX8 and RT1052</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Communication-protocol-between-IMX8-and-RT1052/m-p/1896249#M31059</link>
      <description>&lt;P&gt;The amount of data each interaction between the two chips is 512 bytes, and the less time spent, the better&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 01:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Communication-protocol-between-IMX8-and-RT1052/m-p/1896249#M31059</guid>
      <dc:creator>jiaxin</dc:creator>
      <dc:date>2024-07-01T01:24:11Z</dc:date>
    </item>
    <item>
      <title>Re: Communication protocol between IMX8 and RT1052</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Communication-protocol-between-IMX8-and-RT1052/m-p/1899817#M31121</link>
      <description>&lt;P&gt;The bandwidth will depend on the protocol used for communication.&lt;BR /&gt;You can opt to use LPSPI or ethernet for the communication between devices.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jul 2024 00:34:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Communication-protocol-between-IMX8-and-RT1052/m-p/1899817#M31121</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2024-07-05T00:34:35Z</dc:date>
    </item>
  </channel>
</rss>