<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic can i use jtag_mod as gpio,and use swd debug in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/can-i-use-jtag-mod-as-gpio-and-use-swd-debug/m-p/1885853#M30845</link>
    <description>&lt;P&gt;current,the&amp;nbsp;jtag_mod&amp;nbsp; pin is only pull down to gnd, and no other function.But i want to use this pin as gpio,because no any more pin can use.I do not know the jtag_mod function is check at power on or at debug and download.Is this pin can used as gpio,and use swd debug.&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jun 2024 07:06:08 GMT</pubDate>
    <dc:creator>ccc_clive</dc:creator>
    <dc:date>2024-06-12T07:06:08Z</dc:date>
    <item>
      <title>can i use jtag_mod as gpio,and use swd debug</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/can-i-use-jtag-mod-as-gpio-and-use-swd-debug/m-p/1885853#M30845</link>
      <description>&lt;P&gt;current,the&amp;nbsp;jtag_mod&amp;nbsp; pin is only pull down to gnd, and no other function.But i want to use this pin as gpio,because no any more pin can use.I do not know the jtag_mod function is check at power on or at debug and download.Is this pin can used as gpio,and use swd debug.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 07:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/can-i-use-jtag-mod-as-gpio-and-use-swd-debug/m-p/1885853#M30845</guid>
      <dc:creator>ccc_clive</dc:creator>
      <dc:date>2024-06-12T07:06:08Z</dc:date>
    </item>
    <item>
      <title>回复： can i use jtag_mod as gpio,and use swd debug</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/can-i-use-jtag-mod-as-gpio-and-use-swd-debug/m-p/1886047#M30855</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216319"&gt;@ccc_clive&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;Unfortunately, that's not allowed.&amp;nbsp;&lt;SPAN&gt;While we call the signal JTAG_MOD, it will still affect SWD function. So if you want any debugging capability (JTAG or SWD), then we should tie that signal to ground and not try to use it as a GPIO.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Gavin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 10:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/can-i-use-jtag-mod-as-gpio-and-use-swd-debug/m-p/1886047#M30855</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-06-12T10:09:30Z</dc:date>
    </item>
  </channel>
</rss>