<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 iMX RT1050 24MHz clock signal</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1050-24MHz-clock-signal/m-p/904958#M3048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On a project, I need to generate the 24MHz XTALi signal from an external oscillator which outputs 1.8V signals.&lt;/P&gt;&lt;P&gt;To meet the requirement of the iMXRT1052, I use a capacitive voltage divider but the signal out of the divider is below 0V (see attached picture) specified in the IMXRT1050IEC document, page 31.&lt;/P&gt;&lt;P&gt;The High level is also to close to Vihmin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;A resistive voltage divider modifies the signal too much.&lt;/P&gt;&lt;P&gt;What is the best way to do this voltage division in order to meet the NXP requirements?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 May 2019 13:52:35 GMT</pubDate>
    <dc:creator>davidouatt08</dc:creator>
    <dc:date>2019-05-22T13:52:35Z</dc:date>
    <item>
      <title>iMX RT1050 24MHz clock signal</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1050-24MHz-clock-signal/m-p/904958#M3048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On a project, I need to generate the 24MHz XTALi signal from an external oscillator which outputs 1.8V signals.&lt;/P&gt;&lt;P&gt;To meet the requirement of the iMXRT1052, I use a capacitive voltage divider but the signal out of the divider is below 0V (see attached picture) specified in the IMXRT1050IEC document, page 31.&lt;/P&gt;&lt;P&gt;The High level is also to close to Vihmin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;A resistive voltage divider modifies the signal too much.&lt;/P&gt;&lt;P&gt;What is the best way to do this voltage division in order to meet the NXP requirements?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 13:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1050-24MHz-clock-signal/m-p/904958#M3048</guid>
      <dc:creator>davidouatt08</dc:creator>
      <dc:date>2019-05-22T13:52:35Z</dc:date>
    </item>
    <item>
      <title>Re: iMX RT1050 24MHz clock signal</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1050-24MHz-clock-signal/m-p/904959#M3049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="335743" data-username="davidouatt08@hotmail.com" href="https://community.nxp.com/people/davidouatt08@hotmail.com"&gt;David OUATTARA&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;Please refer to the below figure to optimize the voltage divider, and note that: don't use the large resistors (&amp;gt; 300Ω) in the voltage divider.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83939i65BB002C645434A8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 03:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT1050-24MHz-clock-signal/m-p/904959#M3049</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-05-28T03:15:59Z</dc:date>
    </item>
  </channel>
</rss>