<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: How to connect two codecs to a IMXRT processor</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-connect-two-codecs-to-a-IMXRT-processor/m-p/1867528#M30418</link>
    <description>&lt;P&gt;Please refer to this example to use the multichannel feature of the SAI module: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12090.pdf" target="_blank"&gt;Using Multi-Channel Feature of SAI (nxp.com)&lt;/A&gt;&lt;BR /&gt;From RT1020 SAI1 supports up to 8 channels.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Thu, 16 May 2024 23:33:45 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2024-05-16T23:33:45Z</dc:date>
    <item>
      <title>How to connect two codecs to a IMXRT processor</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-connect-two-codecs-to-a-IMXRT-processor/m-p/1865311#M30326</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have to connect a four channels codec (AK4619) to a IMXRT processor, for example the IMXrt1011 (I have the evaluation board) or the IMXrt1021...IMXrt1062..., or two codecs to a IMXRT processor.&lt;/P&gt;&lt;P&gt;May you help me how to do it and if does exist a code example ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Luigi&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 10:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-connect-two-codecs-to-a-IMXRT-processor/m-p/1865311#M30326</guid>
      <dc:creator>LuigiV</dc:creator>
      <dc:date>2024-05-14T10:03:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to connect two codecs to a IMXRT processor</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-connect-two-codecs-to-a-IMXRT-processor/m-p/1867528#M30418</link>
      <description>&lt;P&gt;Please refer to this example to use the multichannel feature of the SAI module: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12090.pdf" target="_blank"&gt;Using Multi-Channel Feature of SAI (nxp.com)&lt;/A&gt;&lt;BR /&gt;From RT1020 SAI1 supports up to 8 channels.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 16 May 2024 23:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-connect-two-codecs-to-a-IMXRT-processor/m-p/1867528#M30418</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2024-05-16T23:33:45Z</dc:date>
    </item>
  </channel>
</rss>