<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MXRT1051DVL6A (A0 silicon): can 3V3 on DCDC_In damage part? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1051DVL6A-A0-silicon-can-3V3-on-DCDC-In-damage-part/m-p/750678#M298</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm coming on-board to a new design using the i.MXRT1051DVL6A where the A0 silicon was specified in the BoM and the board was designed with 3V3 on the DCDC-In rail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking in the datasheet, this rail appears to still have an Absolute Maximum rating that seems like it should withstand &amp;gt; 3V0 volts on DCDC-IN, but two boards that I'm working with draw so much current when 3V3 is put on the NVCC-* rails that the LDOs end-up current limiting and shunt the 3V3 rail to about 0.7V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've made a small mod where I put a diode in series to the DCDC-IN rail to try and limit it to ~3V but as soon as NVCC is connected the 3V3 rail tanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can't wait for a board spin and are thinking of replacing the BGA MCU using a turnkey but wanted an opinion if 3V3 on A0 silicon will damage the MCU or if we should ensure that hardware mods are performed before powering-up the MCU after replacement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've isolated the SDRAM supply and the flash supply is connected to 3V3 directly; all told, it comes down to connecting the NVCC lines to the MCU where the overcurrent happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Scott Thompson, TC Helicon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jun 2018 23:52:58 GMT</pubDate>
    <dc:creator>scott_thompson</dc:creator>
    <dc:date>2018-06-04T23:52:58Z</dc:date>
    <item>
      <title>i.MXRT1051DVL6A (A0 silicon): can 3V3 on DCDC_In damage part?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1051DVL6A-A0-silicon-can-3V3-on-DCDC-In-damage-part/m-p/750678#M298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm coming on-board to a new design using the i.MXRT1051DVL6A where the A0 silicon was specified in the BoM and the board was designed with 3V3 on the DCDC-In rail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking in the datasheet, this rail appears to still have an Absolute Maximum rating that seems like it should withstand &amp;gt; 3V0 volts on DCDC-IN, but two boards that I'm working with draw so much current when 3V3 is put on the NVCC-* rails that the LDOs end-up current limiting and shunt the 3V3 rail to about 0.7V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've made a small mod where I put a diode in series to the DCDC-IN rail to try and limit it to ~3V but as soon as NVCC is connected the 3V3 rail tanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can't wait for a board spin and are thinking of replacing the BGA MCU using a turnkey but wanted an opinion if 3V3 on A0 silicon will damage the MCU or if we should ensure that hardware mods are performed before powering-up the MCU after replacement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've isolated the SDRAM supply and the flash supply is connected to 3V3 directly; all told, it comes down to connecting the NVCC lines to the MCU where the overcurrent happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Scott Thompson, TC Helicon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jun 2018 23:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1051DVL6A-A0-silicon-can-3V3-on-DCDC-In-damage-part/m-p/750678#M298</guid>
      <dc:creator>scott_thompson</dc:creator>
      <dc:date>2018-06-04T23:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1051DVL6A (A0 silicon): can 3V3 on DCDC_In damage part?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1051DVL6A-A0-silicon-can-3V3-on-DCDC-In-damage-part/m-p/750679#M299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A0 erratum and datasheet (below) limited voltage to 3.0V, so 3V3 may damage chip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17013i8E12E3C149E5B33E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17051iACBF8C7113337948/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.jpg" alt="pastedImage_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 23:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1051DVL6A-A0-silicon-can-3V3-on-DCDC-In-damage-part/m-p/750679#M299</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-05T23:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: i.MXRT1051DVL6A (A0 silicon): can 3V3 on DCDC_In damage part?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1051DVL6A-A0-silicon-can-3V3-on-DCDC-In-damage-part/m-p/750680#M300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&amp;nbsp; I was just coming in to check on the Errata for that mask.&amp;nbsp; Now I have something to hand-wave to.&amp;nbsp; Already have some A1 silicon on order to replace these guys.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for taking the time to answer my question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Scott Thompson, TC Helicon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 16:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MXRT1051DVL6A-A0-silicon-can-3V3-on-DCDC-In-damage-part/m-p/750680#M300</guid>
      <dc:creator>scott_thompson</dc:creator>
      <dc:date>2018-06-06T16:18:48Z</dc:date>
    </item>
  </channel>
</rss>