<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Parallel LCD Interface with RT1176</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1836691#M29570</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231235"&gt;@Stargazer1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The necessary clock formulas for proper operation are described as comments on the "display_support.c" file, under the "board" folder.&lt;/P&gt;
&lt;P&gt;For pixel clock:&lt;/P&gt;
&lt;PRE&gt;The pixel clock is (height + VSW + VFP + VBP) * (width + HSW + HFP + HBP) * frame rate.&lt;/PRE&gt;
&lt;P&gt;and for PHY clock:&lt;/P&gt;
&lt;PRE&gt;DPHY bit clock must be larger than:&lt;BR /&gt;(Pixel clock * bit per output pixel) / number of MIPI data lane&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Mar 2024 19:24:28 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2024-03-27T19:24:28Z</dc:date>
    <item>
      <title>Parallel LCD Interface with RT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1832579#M29455</link>
      <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I'm currently using the rt1176 board and interfacing it with the 800*480 resolution parallel lcd panel. I changed the pin configuration and hsync vsync values. I set the pixel clock value as 25MHz and changed the video mux to parallel. But the display is not showing. I'm using the elcdif rgb example in the SDK examples file. Can you help me to rectify this issue&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 04:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1832579#M29455</guid>
      <dc:creator>Stargazer1</dc:creator>
      <dc:date>2024-03-21T04:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel LCD Interface with RT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1833163#M29472</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231235"&gt;@Stargazer1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please look into the following application note, which describes the inner workings of the MIPI and LCDIF controllers of the RT1170, as well as how to adequately interface them with an LCD:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12940.pdf" target="_blank"&gt;AN12940: Use Case of RT1170 LCD Display System based on MIPI DSI – Application Note (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I believe this application note will prove very useful for your inquiry. If you have further questions about this topic, do let me know.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 18:58:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1833163#M29472</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-03-21T18:58:26Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel LCD Interface with RT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1835124#M29524</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am now getting colours in elcdif rgb program clearly. But for in sdcrad_jpeg, image was not showing. I changed all the things i done in elcdif rgb but image was not showing.&lt;/P&gt;&lt;P&gt;For video pll clock configurations, at what MHz it needs to be set. What is the formula for that?&lt;/P&gt;</description>
      <pubDate>Tue, 26 Mar 2024 05:47:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1835124#M29524</guid>
      <dc:creator>Stargazer1</dc:creator>
      <dc:date>2024-03-26T05:47:21Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel LCD Interface with RT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1836691#M29570</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231235"&gt;@Stargazer1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The necessary clock formulas for proper operation are described as comments on the "display_support.c" file, under the "board" folder.&lt;/P&gt;
&lt;P&gt;For pixel clock:&lt;/P&gt;
&lt;PRE&gt;The pixel clock is (height + VSW + VFP + VBP) * (width + HSW + HFP + HBP) * frame rate.&lt;/PRE&gt;
&lt;P&gt;and for PHY clock:&lt;/P&gt;
&lt;PRE&gt;DPHY bit clock must be larger than:&lt;BR /&gt;(Pixel clock * bit per output pixel) / number of MIPI data lane&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 19:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Parallel-LCD-Interface-with-RT1176/m-p/1836691#M29570</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-03-27T19:24:28Z</dc:date>
    </item>
  </channel>
</rss>