<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Not recieving frames with demo PTP program. in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1828488#M29361</link>
    <description>&lt;P&gt;Gavin,&lt;/P&gt;&lt;P&gt;Thank you for your assistance. I have resolved the issue. Previously, I had run the evkmimxrt1024_lpspi_loopback demo, and I had left in the SIN to SOUT jumber. Once the jumper was removed the PTP demo started receiving data. I don't know why the SPI jumper would prevent the ethernet from receiving data, but that was the issue.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Mar 2024 12:38:57 GMT</pubDate>
    <dc:creator>wlevans</dc:creator>
    <dc:date>2024-03-14T12:38:57Z</dc:date>
    <item>
      <title>Not recieving frames with demo PTP program.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1826584#M29319</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an i.MX RT1024 evaluation kit, and I am working on the evkmimxrt1024_enet_txrx_ptp1588_transfer demo program from the SDK with a loopback network cable. I can compile and download the program to the board. When I run the program it shows that the frames are transmitted successfully. However, it does not show that the frames are received.&lt;/P&gt;&lt;P&gt;I've checked the return value from the call to "&lt;SPAN&gt;ENET_GetRxFrameSize", and it returns "error&lt;/SPAN&gt;&lt;SPAN&gt;kStatus_ENET_RxFrameError" for each transmitted frame.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I've attached a copy of my serial output.&lt;/P&gt;&lt;P&gt;Any help I can get to get this working would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 21:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1826584#M29319</guid>
      <dc:creator>wlevans</dc:creator>
      <dc:date>2024-03-12T21:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: Not recieving frames with demo PTP program.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1826589#M29320</link>
      <description>&lt;P&gt;I should have stated that I am using MCUXpresso IDE v11.9.0_2144.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 22:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1826589#M29320</guid>
      <dc:creator>wlevans</dc:creator>
      <dc:date>2024-03-12T22:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: Not recieving frames with demo PTP program.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1826888#M29325</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230863"&gt;@wlevans&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;The demo evkmimxrt1024_enet_txrx_ptp1588_transfer needs a loopback network cable installed.&amp;nbsp; As described in the ReadMe.md file:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Gavin_Jia_0-1710313843821.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268045i89ABC8CD95BC3051/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Gavin_Jia_0-1710313843821.png" alt="Gavin_Jia_0-1710313843821.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Gavin_Jia_0-1710313843821.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps!&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Gavin&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 07:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1826888#M29325</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-03-13T07:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: Not recieving frames with demo PTP program.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1827173#M29332</link>
      <description>Thanks for your reply, but as I stated in my original post I am using a loopback network cable.</description>
      <pubDate>Wed, 13 Mar 2024 12:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1827173#M29332</guid>
      <dc:creator>wlevans</dc:creator>
      <dc:date>2024-03-13T12:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: Not recieving frames with demo PTP program.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1827948#M29351</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230863"&gt;@wlevans&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thank you for your feedback. &lt;BR /&gt;However, this demo should run well if you follow the instructions in the README guide. Our colleague has tested it before, so we doubt that there is a fault with the network cable connection. If it still does not work properly, I can test it on my side for you again. It may take some time next week due to my upcoming holiday. &lt;BR /&gt;&lt;BR /&gt;I suggest you check if the loopback network cable is correctly connected. If you don't want to modify it, you can try another demo instead (lwip demos in SDK:&amp;nbsp;&lt;U&gt;&lt;EM&gt;SDK_2_15_000_MIMXRT1024-EVK\boards\evkmimxrt1024\lwip_examples&lt;/EM&gt;&lt;/U&gt; ). It will connect to an external device, and only a regular network cable is needed.&lt;BR /&gt;Thank you in advance for your kind patience!&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Gavin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 03:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1827948#M29351</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-03-14T03:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: Not recieving frames with demo PTP program.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1828488#M29361</link>
      <description>&lt;P&gt;Gavin,&lt;/P&gt;&lt;P&gt;Thank you for your assistance. I have resolved the issue. Previously, I had run the evkmimxrt1024_lpspi_loopback demo, and I had left in the SIN to SOUT jumber. Once the jumper was removed the PTP demo started receiving data. I don't know why the SPI jumper would prevent the ethernet from receiving data, but that was the issue.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 12:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Not-recieving-frames-with-demo-PTP-program/m-p/1828488#M29361</guid>
      <dc:creator>wlevans</dc:creator>
      <dc:date>2024-03-14T12:38:57Z</dc:date>
    </item>
  </channel>
</rss>