<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX RT1176 First time program installation in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1824933#M29252</link>
    <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;,&lt;BR /&gt;We have no problem writing to Flash and reading it. We get a flash error when we want to load a program that runs as xip during the first program loading on the cards coming from production. After loading and running a program that runs on ocram, after turning off the power and turning it on, the program can be loaded into the flash normally. Why can't we assign code to the flash during the first program loading? (Flash on the custom board is different from the flash on the development board).&lt;BR /&gt;&lt;BR /&gt;thanks.</description>
    <pubDate>Mon, 11 Mar 2024 08:41:55 GMT</pubDate>
    <dc:creator>tbayram</dc:creator>
    <dc:date>2024-03-11T08:41:55Z</dc:date>
    <item>
      <title>IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1822064#M29177</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;We are working on a custom board with IMX rt1176 processor. External QSPI flash is different from the flash on the development board. The programs loaded in the flash do not work when I first code to the processor. First we can run a program in OCRam and then we can load the code into the flash. What is the reason for this? Is this a problem?&lt;BR /&gt;Good day to everyone.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 05:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1822064#M29177</guid>
      <dc:creator>tbayram</dc:creator>
      <dc:date>2024-03-06T05:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1822879#M29201</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225235"&gt;@tbayram&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; It's easy to check the issues, please follow me:&lt;/P&gt;
&lt;P&gt;1. open the SDK flexspi_nr_polling_transfer_cm7 code .&lt;/P&gt;
&lt;P&gt;2. check :&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {&lt;/P&gt;
&lt;P&gt;make sure the LUT read, erase, quad, etc commander matches you used flash.&lt;/P&gt;
&lt;P&gt;3. Run the project in the internal RAM:&lt;/P&gt;
&lt;P&gt;Whether it can pass all the testing?&lt;/P&gt;
&lt;P&gt;I mean, the log should like this:&lt;/P&gt;
&lt;P&gt;~~~~~~~~~~~~~~~~~~~~~~~~~~~~&lt;/P&gt;
&lt;P&gt;FLEXSPI example started!&lt;BR /&gt;Vendor ID: 0x9d&lt;BR /&gt;Erasing Serial NOR over FlexSPI...&lt;BR /&gt;Erase data - successfully.&lt;BR /&gt;Program data - successfully.&lt;BR /&gt;~~~~~~~~~~~~~~~~~~~~~~~~~~~~&lt;/P&gt;
&lt;P&gt;This will help you to check your external flash situation, and also help you enable the quad mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please try it on your side.&lt;/P&gt;
&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 03:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1822879#M29201</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2024-03-07T03:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1824933#M29252</link>
      <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;,&lt;BR /&gt;We have no problem writing to Flash and reading it. We get a flash error when we want to load a program that runs as xip during the first program loading on the cards coming from production. After loading and running a program that runs on ocram, after turning off the power and turning it on, the program can be loaded into the flash normally. Why can't we assign code to the flash during the first program loading? (Flash on the custom board is different from the flash on the development board).&lt;BR /&gt;&lt;BR /&gt;thanks.</description>
      <pubDate>Mon, 11 Mar 2024 08:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1824933#M29252</guid>
      <dc:creator>tbayram</dc:creator>
      <dc:date>2024-03-11T08:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1825056#M29255</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225235"&gt;@tbayram&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Which QSPI fash partnumber you are using?&lt;/P&gt;
&lt;P&gt;You mentioned:&amp;nbsp;&lt;SPAN&gt;We get a flash error when we want to load a program that runs as xip during the first program loading on the cards coming from production,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You want the XIP and to do the flash operation, right? In this situation, you need to copy the flash driver to the internal RAM, otherwise, it will have issues, you can refer to the SDK flexspi_nr_polling_transfer_cm7 code.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you！&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 10:26:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1825056#M29255</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2024-03-11T10:26:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1825073#M29257</link>
      <description>hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;,&lt;BR /&gt;we are using qspi flash partnumber is MX25L6433FM2Q-09G.&lt;BR /&gt;I will refer flexspi_nr_polling_transfer_cm7 example.&lt;BR /&gt;&lt;BR /&gt;Thank you so much.</description>
      <pubDate>Mon, 11 Mar 2024 10:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1825073#M29257</guid>
      <dc:creator>tbayram</dc:creator>
      <dc:date>2024-03-11T10:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1825729#M29291</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225235"&gt;@tbayram&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Please run this&amp;nbsp;&lt;SPAN&gt;flexspi_nr_polling_transfer_cm7&amp;nbsp;demo in the internal RAM at first, then share the result to me, you also need to check the LUT commander to match your used flash datasheet, thanks.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Linker to RAM is like this configuration in the MCUXpresso project:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1710218518227.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267696iD2C6BFEBCFFD9ABC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1710218518227.png" alt="kerryzhou_0-1710218518227.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Any updated information, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 04:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1825729#M29291</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2024-03-12T04:42:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1827080#M29329</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tbayram_0-1710325208617.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268079i50F8A476CE2724FB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tbayram_0-1710325208617.png" alt="tbayram_0-1710325208617.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Our result is same with yours. Is it meaning there is no problem?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 10:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1827080#M29329</guid>
      <dc:creator>tbayram</dc:creator>
      <dc:date>2024-03-13T10:21:08Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1176 First time program installation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1827914#M29347</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225235"&gt;@tbayram&lt;/a&gt;&amp;nbsp;，&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Yes, this test result means your external flash works OK.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Now, you can download the app image to your external flash, and boot it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Do you still have issues about it?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You need to check the BOOT_MODE, and BOOT_CFG, make sure it is internal boot mode, and the CFG for the QSPI flash, to the BOOT_CFG related pins, just keep 0 is OK, to the BOOT_MODE[1:0]=10, this is the internal boot mode.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 02:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1176-First-time-program-installation/m-p/1827914#M29347</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2024-03-14T02:37:27Z</dc:date>
    </item>
  </channel>
</rss>