<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: i.MX RT1060 EVKB display interface using segger_emWin_GUIDRV_Lin driver</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-EVKB-display-interface-using-segger-emWin-GUIDRV-Lin/m-p/1822778#M29199</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226828"&gt;@abilashjoseph&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;By the description you mention it seems like the SYNC timings are probably the main cause of your issues. Are you certain that you set them up according to your display's datasheet? The following application note, specifically section "2.2. LCD RGB bus timing parameters" describes the configuration changes required for the timing parameters, please take a look into it:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12302.pdf" target="_blank"&gt;i.MX RT eLCDIF RGB Mode Use Case (nxp.com)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Thu, 07 Mar 2024 00:04:23 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2024-03-07T00:04:23Z</dc:date>
    <item>
      <title>i.MX RT1060 EVKB display interface using segger_emWin_GUIDRV_Lin driver</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-EVKB-display-interface-using-segger-emWin-GUIDRV-Lin/m-p/1822098#M29178</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to interface the display&amp;nbsp;LQ035Q3DY01 with i.MX RT 1060 EVKB using MCUXpresso IDE and its example codes. The library using in the example code is segger emWin&amp;nbsp;GUIDRV_Lin. I am able to do initialize, set the background color, add shapes etc.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I made the following changes in the code to meet the timing requirement of display.&lt;/P&gt;&lt;P&gt;1. Frequency&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Horizontal and Vertical SYNC timings&lt;/P&gt;&lt;P&gt;3. Resolution to 320x240&lt;/P&gt;&lt;P&gt;But I am facing few issues that are given below.&lt;/P&gt;&lt;P&gt;1. Unable to set the location (0,0) on the display corner. its starts somewhere in the display.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Unable to use the entire display area. some portions of the display only working.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. duplication of the data in the display area.&amp;nbsp;&lt;/P&gt;&lt;P&gt;4. Display goes freeze within seconds and unable to update the display. and gradually display changes uneven.&amp;nbsp;&lt;/P&gt;&lt;P&gt;the reference of the issues is attached.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abilash Joseph&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 06:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-EVKB-display-interface-using-segger-emWin-GUIDRV-Lin/m-p/1822098#M29178</guid>
      <dc:creator>abilashjoseph</dc:creator>
      <dc:date>2024-03-06T06:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT1060 EVKB display interface using segger_emWin_GUIDRV_Lin driver</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-EVKB-display-interface-using-segger-emWin-GUIDRV-Lin/m-p/1822778#M29199</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226828"&gt;@abilashjoseph&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;By the description you mention it seems like the SYNC timings are probably the main cause of your issues. Are you certain that you set them up according to your display's datasheet? The following application note, specifically section "2.2. LCD RGB bus timing parameters" describes the configuration changes required for the timing parameters, please take a look into it:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12302.pdf" target="_blank"&gt;i.MX RT eLCDIF RGB Mode Use Case (nxp.com)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 00:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-EVKB-display-interface-using-segger-emWin-GUIDRV-Lin/m-p/1822778#M29199</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-03-07T00:04:23Z</dc:date>
    </item>
  </channel>
</rss>