<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMXRT1062 Flexcan-FD FIFO Example in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1062-Flexcan-FD-FIFO-Example/m-p/898643#M2913</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Been looking in the SDKs for an example using FIFO for RX and TX but do not see any in the CAN or CANFD driver examples.&amp;nbsp; Can you all provide a sample program using FIFO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&amp;nbsp; One of the things that this would be helpful with is setting up the id filter table and the appropriate structure.&amp;nbsp; I really would like to be able to receive on any mailbox a series of message ides as well as setting up a CANFD fifo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT2:&amp;nbsp; BTW the docs for the FD example in the 1060evk sdk state&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Board settings&lt;BR /&gt;==============&lt;BR /&gt;The example requires 2 sets of boards, each of them are mounted with the base board. Using a male to male CAN&lt;BR /&gt;cable to connect the CAN2 instance (J11) between the 2 base boards.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In looking at the schematic and the pins it looks like the CAN3 tx/rx pins go to the Arduino header.&amp;nbsp; So how can you test CANFD if you don't have a receiver?&amp;nbsp; CAN2 is not CANFD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 May 2019 14:26:16 GMT</pubDate>
    <dc:creator>michaelsmorto</dc:creator>
    <dc:date>2019-05-01T14:26:16Z</dc:date>
    <item>
      <title>IMXRT1062 Flexcan-FD FIFO Example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1062-Flexcan-FD-FIFO-Example/m-p/898643#M2913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Been looking in the SDKs for an example using FIFO for RX and TX but do not see any in the CAN or CANFD driver examples.&amp;nbsp; Can you all provide a sample program using FIFO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&amp;nbsp; One of the things that this would be helpful with is setting up the id filter table and the appropriate structure.&amp;nbsp; I really would like to be able to receive on any mailbox a series of message ides as well as setting up a CANFD fifo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT2:&amp;nbsp; BTW the docs for the FD example in the 1060evk sdk state&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Board settings&lt;BR /&gt;==============&lt;BR /&gt;The example requires 2 sets of boards, each of them are mounted with the base board. Using a male to male CAN&lt;BR /&gt;cable to connect the CAN2 instance (J11) between the 2 base boards.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In looking at the schematic and the pins it looks like the CAN3 tx/rx pins go to the Arduino header.&amp;nbsp; So how can you test CANFD if you don't have a receiver?&amp;nbsp; CAN2 is not CANFD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2019 14:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1062-Flexcan-FD-FIFO-Example/m-p/898643#M2913</guid>
      <dc:creator>michaelsmorto</dc:creator>
      <dc:date>2019-05-01T14:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1062 Flexcan-FD FIFO Example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1062-Flexcan-FD-FIFO-Example/m-p/898644#M2914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael Smorto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, there isn't any example code of flexcan using the RXFIFO buffer provided along with the SDK. You can check the following post:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/484816" rel="nofollow noopener noreferrer" target="_blank"&gt;K10 FlexCan RX FIFO Filter&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/475008" rel="nofollow noopener noreferrer" target="_blank"&gt;FlexCAN Fifo SDK 2.0 example&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even if they are for different chips, you could use them as reference for your implementation. I have implement a simple example using the FIFO:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;flexcan_rx_fifo_config_t fifoConfig&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
     uint32_t tableID&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;10&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;3&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
              &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;6&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;7&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
            &lt;SPAN class="token function"&gt;FLEXCAN_RX_FIFO_STD_MASK_TYPE_A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rxIdentifier&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;9&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;


     fifoConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;idFilterType &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kFLEXCAN_RxFifoFilterTypeA&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  fifoConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;idFilterNum &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;tableID&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;tableID&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;//2;&lt;/SPAN&gt;
  fifoConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;idFilterTable &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; tableID&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  fifoConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;priority &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kFLEXCAN_RxFifoPrioHigh&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

     &lt;SPAN class="token function"&gt;FLEXCAN_SetRxFifoConfig&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;EXAMPLE_CAN&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;fifoConfig&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; true&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;

&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/* When you want to receive some data */&lt;/SPAN&gt;

rxXferfifo&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;frame &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;frame&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

   &lt;SPAN class="token function"&gt;FLEXCAN_TransferReceiveFifoNonBlocking&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;EXAMPLE_CAN&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;flexcanHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;rxXferfifo&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;EDIT2:&amp;nbsp; BTW the docs for the FD example in the 1060evk sdk state&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Thanks for pointing out the mistake, this is a error in the read me file, it should actually say CAN3, those pins have also the functionality of the CAN3_Tx/Rx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this could helps you&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note: - If this post answers your question, please click the "Mark Correct" button. Thank you&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 21:56:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1062-Flexcan-FD-FIFO-Example/m-p/898644#M2914</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-05-10T21:56:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1062 Flexcan-FD FIFO Example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1062-Flexcan-FD-FIFO-Example/m-p/898645#M2915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="280170" data-username="jorge_a_vazquez" href="https://community.nxp.com/people/jorge_a_vazquez" style="border-image-outset: 0; border-image-repeat: stretch; border-image-slice: 100%; border-image-source: none; border-image-width: 1; color: #3d9ce7; fill: #3d9ce7; font-family: inherit; font-size: 1.28rem; font-style: inherit; font-variant: normal; font-weight: 200; letter-spacing: normal; line-height: 1.28rem; orphans: 2; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; transition-delay: 0s; transition-duration: 0.1s; transition-property: color; transition-timing-function: linear; vertical-align: baseline; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px; padding: 0px; margin: 0px; border: 0px none currentColor;"&gt;Jorge Antonio Alcala Vazquez&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I really appreciate your reply. Thank you for the links - they really help in understanding how to set up the FIFO which was what I was looking. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now for the fun - start implementation of the FIFO in the application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 May 2019 11:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1062-Flexcan-FD-FIFO-Example/m-p/898645#M2915</guid>
      <dc:creator>michaelsmorto</dc:creator>
      <dc:date>2019-05-11T11:47:28Z</dc:date>
    </item>
  </channel>
</rss>