<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: reset adc input voltage range from 3.3v to 5v in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/reset-adc-input-voltage-range-from-3-3v-to-5v/m-p/898474#M2912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zhou Zhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to Table 54 of the datasheet.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83495i16BC7A5CF0027A8F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The maximum voltage allowed by Ref Voltage High is 3.6V, although is not recommended to work with the maximum voltage allowed, this is why by default comes with 3.3V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 May 2019 14:37:49 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2019-05-21T14:37:49Z</dc:date>
    <item>
      <title>reset adc input voltage range from 3.3v to 5v</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/reset-adc-input-voltage-range-from-3-3v-to-5v/m-p/898473#M2911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi nxp,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the MIMXRT106x-evk board to read some data in the adc channel. I check the datasheet, the max input voltage can be decided by Vref. The default setting is 3.3v represented of 4096 step. How could I change its max range from 3.3v to 5.0V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 17:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/reset-adc-input-voltage-range-from-3-3v-to-5v/m-p/898473#M2911</guid>
      <dc:creator>z_zhou</dc:creator>
      <dc:date>2019-05-16T17:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: reset adc input voltage range from 3.3v to 5v</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/reset-adc-input-voltage-range-from-3-3v-to-5v/m-p/898474#M2912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zhou Zhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to Table 54 of the datasheet.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83495i16BC7A5CF0027A8F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The maximum voltage allowed by Ref Voltage High is 3.6V, although is not recommended to work with the maximum voltage allowed, this is why by default comes with 3.3V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2019 14:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/reset-adc-input-voltage-range-from-3-3v-to-5v/m-p/898474#M2912</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-05-21T14:37:49Z</dc:date>
    </item>
  </channel>
</rss>