<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT685-AUD-EVK - how to modify pin configuration for DSP project in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT685-AUD-EVK-how-to-modify-pin-configuration-for-DSP/m-p/1805053#M28862</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;, thanks for the reply.&lt;/P&gt;&lt;P&gt;I've looked at dsp_audio_demo_bm_hifi4 project, and it has pin_mux.c and pin_mux.h in the "board" folder. These files that appear to be generated by MCUXpresso config tools (although they are part of the dsp HiFi4 project) - see the below from pin_mux.c from dsp_audio_demo_bm_hifi4 (see below):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alex_SRL_0-1707694707513.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262776i66F8271B06D4113A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alex_SRL_0-1707694707513.png" alt="Alex_SRL_0-1707694707513.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So is the correct way to configure pins for HiFi4 is to use MCUXpresso Config tools to generate/update pin_mux.c and pin_mux.h files for HiFi4 source and then add that file to the HiFi4 project folder?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 11 Feb 2024 23:39:05 GMT</pubDate>
    <dc:creator>Alex_SRL</dc:creator>
    <dc:date>2024-02-11T23:39:05Z</dc:date>
    <item>
      <title>MIMXRT685-AUD-EVK - how to modify pin configuration for DSP project</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT685-AUD-EVK-how-to-modify-pin-configuration-for-DSP/m-p/1803845#M28840</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd like to add HW peripherals controlled by HiFi4 dsp code to existing example project but seems that the pin configuration file (*.mex) only exists for the ARM code, but not for the dsp code.&lt;/P&gt;&lt;P&gt;Do I need to modify the pin_mux.c in dsp folder to add a peripheral device or there is a way to do it with MCUxpresso Config Tools like with the arm core?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Feb 2024 03:44:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT685-AUD-EVK-how-to-modify-pin-configuration-for-DSP/m-p/1803845#M28840</guid>
      <dc:creator>Alex_SRL</dc:creator>
      <dc:date>2024-02-08T03:44:07Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT685-AUD-EVK - how to modify pin configuration for DSP project</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT685-AUD-EVK-how-to-modify-pin-configuration-for-DSP/m-p/1804941#M28860</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193431"&gt;@Alex_SRL&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm afraid the HiFi4 DSP does not have ConfigTools compatibility. In MCUXpresso IDE, if you click on "ConfigTools" on the top menu bar and then select "Data Manager" a window opens with all of the tool's compatibility with different products. Sadly, the HiFi4 DSP is not listed in this window, so it does not have any compatibility with ConfigTools.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EdwinHz_0-1707514532691.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262745i04BA3FADDD26AAE3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EdwinHz_0-1707514532691.png" alt="EdwinHz_0-1707514532691.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Feb 2024 21:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT685-AUD-EVK-how-to-modify-pin-configuration-for-DSP/m-p/1804941#M28860</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-02-09T21:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT685-AUD-EVK - how to modify pin configuration for DSP project</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT685-AUD-EVK-how-to-modify-pin-configuration-for-DSP/m-p/1805053#M28862</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;, thanks for the reply.&lt;/P&gt;&lt;P&gt;I've looked at dsp_audio_demo_bm_hifi4 project, and it has pin_mux.c and pin_mux.h in the "board" folder. These files that appear to be generated by MCUXpresso config tools (although they are part of the dsp HiFi4 project) - see the below from pin_mux.c from dsp_audio_demo_bm_hifi4 (see below):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alex_SRL_0-1707694707513.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262776i66F8271B06D4113A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alex_SRL_0-1707694707513.png" alt="Alex_SRL_0-1707694707513.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So is the correct way to configure pins for HiFi4 is to use MCUXpresso Config tools to generate/update pin_mux.c and pin_mux.h files for HiFi4 source and then add that file to the HiFi4 project folder?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 11 Feb 2024 23:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT685-AUD-EVK-how-to-modify-pin-configuration-for-DSP/m-p/1805053#M28862</guid>
      <dc:creator>Alex_SRL</dc:creator>
      <dc:date>2024-02-11T23:39:05Z</dc:date>
    </item>
  </channel>
</rss>