<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX RT 1062 MCU LCDIF Pigeon Mode Example code. in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT-1062-MCU-LCDIF-Pigeon-Mode-Example-code/m-p/1804451#M28851</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226828"&gt;@abilashjoseph&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm afraid we don't have any example codes for pigeon mode on the eLCDIF module. Perhaps using &lt;A href="https://www.nxp.com/docs/en/application-note/AN12822.pdf" target="_self"&gt;AN12822&lt;/A&gt; as reference could prove useful for this inquiry, although this would be an alternative with the FlexIO module, rather than a baseline for pigeon mode with eLCDIF.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Thu, 08 Feb 2024 23:27:05 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2024-02-08T23:27:05Z</dc:date>
    <item>
      <title>iMX RT 1062 MCU LCDIF Pigeon Mode Example code.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT-1062-MCU-LCDIF-Pigeon-Mode-Example-code/m-p/1803962#M28843</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a display (PN: LQ035Q7DB05) that is working in the old type of LCD interface, from my understanding it works on the pigeon mode. So, I am looking for an example code for the LCDIF in pigeon mode with RGB 565 format. NXP have any example code readily available? with Easly configure the pigeon mode registers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the iMXRT 1060 EVK with me, I planning to take the pigeon mode signals from ethernet signals on the EVK by doing a rework on the EVK.&lt;/P&gt;&lt;P&gt;Kindly suggest me solution.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abilash Joseph&lt;/P&gt;</description>
      <pubDate>Thu, 08 Feb 2024 09:09:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT-1062-MCU-LCDIF-Pigeon-Mode-Example-code/m-p/1803962#M28843</guid>
      <dc:creator>abilashjoseph</dc:creator>
      <dc:date>2024-02-08T09:09:29Z</dc:date>
    </item>
    <item>
      <title>Re: iMX RT 1062 MCU LCDIF Pigeon Mode Example code.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT-1062-MCU-LCDIF-Pigeon-Mode-Example-code/m-p/1804451#M28851</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226828"&gt;@abilashjoseph&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm afraid we don't have any example codes for pigeon mode on the eLCDIF module. Perhaps using &lt;A href="https://www.nxp.com/docs/en/application-note/AN12822.pdf" target="_self"&gt;AN12822&lt;/A&gt; as reference could prove useful for this inquiry, although this would be an alternative with the FlexIO module, rather than a baseline for pigeon mode with eLCDIF.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Feb 2024 23:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMX-RT-1062-MCU-LCDIF-Pigeon-Mode-Example-code/m-p/1804451#M28851</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-02-08T23:27:05Z</dc:date>
    </item>
  </channel>
</rss>