<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Implementation of S-bus in IMXRT1176 controller in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1796769#M28677</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199320"&gt;@_Leo_&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Do you have any idea whether we can implement the same above sensor using normal GPIO pins as you have mentioned its not compatible with I2C pins.?&lt;/P&gt;</description>
    <pubDate>Mon, 29 Jan 2024 09:44:45 GMT</pubDate>
    <dc:creator>Jeevan</dc:creator>
    <dc:date>2024-01-29T09:44:45Z</dc:date>
    <item>
      <title>Implementation of S-bus in IMXRT1176 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1786049#M28408</link>
      <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;We are using IMXRT1176 controller, kindly do let us know how to configure or implement the S-bus protocol in the above-mentioned controller using the MCUxpresso IDE so that it will give us an idea on the feasibility of implementation of S-bus protocol.&lt;/P&gt;&lt;P&gt;Initially we are planning to use an eval board also "IMXRT1170 EVK board". Please do let us know the s-bus implementation in the mentioned eval board also.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 11:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1786049#M28408</guid>
      <dc:creator>Jeevan</dc:creator>
      <dc:date>2024-01-10T11:34:08Z</dc:date>
    </item>
    <item>
      <title>Re: Implementation of S-bus in IMXRT1176 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1789755#M28487</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Do you refer to the System Management Bus (SMBus)? There is no any reference about S-Bus or SBUS in the i.MX RTs.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 21:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1789755#M28487</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-01-16T21:46:28Z</dc:date>
    </item>
    <item>
      <title>Re: Implementation of S-bus in IMXRT1176 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1790167#M28498</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199320"&gt;@_Leo_&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are interfacing one "temperature &amp;amp; humidity sensor" (SHT-15) with the imxrt1176 controller and the data sheet of the sensor is attached below.&lt;/P&gt;&lt;P&gt;Kindly suggest if the mentioned sensor works by interfacing it with the I2C pins of the imxrt1176 controller.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 09:21:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1790167#M28498</guid>
      <dc:creator>Jeevan</dc:creator>
      <dc:date>2024-01-17T09:21:54Z</dc:date>
    </item>
    <item>
      <title>Re: Implementation of S-bus in IMXRT1176 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1792326#M28553</link>
      <description>&lt;P&gt;The datasheet of the sensor you mention states that it is not compatible with I2C interfaces.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="_Leo__0-1705704785287.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/259226i4B6C38F7F62FF4E3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="_Leo__0-1705704785287.png" alt="_Leo__0-1705704785287.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also the&amp;nbsp;&lt;EM&gt;Serial Interface (Bidirectional 2-wire)&lt;/EM&gt; that such part use is no compatible with any of the interfaces of the RT1170.&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;Maybe you can consult our &lt;A href="https://www.nxp.com/products/sensors:SNSHOME" target="_blank" rel="noopener"&gt;Sensor&lt;/A&gt; portfolio to check if any of our devices match with your needs.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 23:04:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1792326#M28553</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-01-19T23:04:33Z</dc:date>
    </item>
    <item>
      <title>Re: Implementation of S-bus in IMXRT1176 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1796769#M28677</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199320"&gt;@_Leo_&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Do you have any idea whether we can implement the same above sensor using normal GPIO pins as you have mentioned its not compatible with I2C pins.?&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 09:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1796769#M28677</guid>
      <dc:creator>Jeevan</dc:creator>
      <dc:date>2024-01-29T09:44:45Z</dc:date>
    </item>
    <item>
      <title>Re: Implementation of S-bus in IMXRT1176 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1798123#M28714</link>
      <description>&lt;P&gt;Hi again,&lt;/P&gt;
&lt;P&gt;The datasheet that you share with us is the one that mentions that it is not compatible with I2C.&lt;/P&gt;
&lt;P&gt;I must admit that your question is difficult to answer because we do not have something similar developed. And you will need to develop your own driver, which will not me a trivial task.&lt;/P&gt;
&lt;P&gt;But for that you can refer to the &lt;EM&gt;4.3.2.1 General purpose I/O (GPIO) AC parameters&lt;/EM&gt; section of the datasheet.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 00:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementation-of-S-bus-in-IMXRT1176-controller/m-p/1798123#M28714</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-01-31T00:26:40Z</dc:date>
    </item>
  </channel>
</rss>