<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Is there a function example for OTFAD encryption?</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-a-function-example-for-OTFAD-encryption/m-p/1791975#M28540</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This is going to be helpful&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/OTFAD-encryption-for-i-MX-RT-1160-EVK-without-fuse/m-p/1493328" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/OTFAD-encryption-for-i-MX-RT-1160-EVK-without-fuse/m-p/1493328&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 19 Jan 2024 14:20:37 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-01-19T14:20:37Z</dc:date>
    <item>
      <title>Is there a function example for OTFAD encryption?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-a-function-example-for-OTFAD-encryption/m-p/1788668#M28457</link>
      <description>&lt;P&gt;&lt;SPAN&gt;if OTFAD is enabled,the firmware was encrypted using image_enc.exe on Windows, but now I want to encrypt some fields in the program.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have seen the source code of image_enc on GitHub, but it takes up a lot of memory if placed the AES-related code in NOR Flash.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any code example that can encrypt plaintext into corresponding ciphertext based on the current OTFAD IEK in the RT1170 chip?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've found relevant functions in&amp;nbsp;&lt;A title="https://mcuxpresso.nxp.com/api_doc/dev/2304/a00047.html" href="https://mcuxpresso.nxp.com/api_doc/dev/2304/a00047.html" target="_self"&gt;https://mcuxpresso.nxp.com/api_doc/dev/2304/a00047.html&lt;/A&gt;,it seems SDK of other RT chips support OTFAD examples.&lt;SPAN&gt;RT1170 doesn't have relevant implementaions in the SDK?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 09:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-a-function-example-for-OTFAD-encryption/m-p/1788668#M28457</guid>
      <dc:creator>Vinos</dc:creator>
      <dc:date>2024-01-15T09:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a function example for OTFAD encryption?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-a-function-example-for-OTFAD-encryption/m-p/1791975#M28540</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This is going to be helpful&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/OTFAD-encryption-for-i-MX-RT-1160-EVK-without-fuse/m-p/1493328" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/OTFAD-encryption-for-i-MX-RT-1160-EVK-without-fuse/m-p/1493328&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 14:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-a-function-example-for-OTFAD-encryption/m-p/1791975#M28540</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-01-19T14:20:37Z</dc:date>
    </item>
  </channel>
</rss>