<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMXRT1010 LPI2C problem using debug mode in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1010-LPI2C-problem-using-debug-mode/m-p/1788244#M28442</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Could you please tell me the SDK version you are using?&lt;BR /&gt;Could you confirm SAI works correctly if it runs independently?&lt;BR /&gt;By debug mode you mean you have a debug session running, am I right? Is this problem still occurs if you don't run it with the debug session? &lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Daniel.&lt;/P&gt;</description>
    <pubDate>Fri, 12 Jan 2024 22:14:22 GMT</pubDate>
    <dc:creator>DanielRuvalcaba</dc:creator>
    <dc:date>2024-01-12T22:14:22Z</dc:date>
    <item>
      <title>IMXRT1010 LPI2C problem using debug mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1010-LPI2C-problem-using-debug-mode/m-p/1785130#M28382</link>
      <description>&lt;P&gt;I use the IMXRT1010 EVK and the MCUXpresso; I configured the LPI2C in transfer mode and the SAI in interrupt mode (word); both units work right but not at the same time.&lt;/P&gt;&lt;P&gt;The LPI2C works correctly only when I don't enable the SAI interrupt, if I enable the SAI interrupt the&lt;/P&gt;&lt;P&gt;"&lt;SPAN&gt;LPI2C_MasterWaitForTxReadyF(LPI2Cbase)" &lt;FONT face="arial,helvetica,sans-serif" color="#333333"&gt;seems to&amp;nbsp;freeze the code....&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT face="arial,helvetica,sans-serif" color="#333333"&gt;Anyone may help me ?&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT face="arial,helvetica,sans-serif" color="#333333"&gt;Thank you, Luigi&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 09:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1010-LPI2C-problem-using-debug-mode/m-p/1785130#M28382</guid>
      <dc:creator>LuigiV</dc:creator>
      <dc:date>2024-01-09T09:31:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1010 LPI2C problem using debug mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1010-LPI2C-problem-using-debug-mode/m-p/1788244#M28442</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Could you please tell me the SDK version you are using?&lt;BR /&gt;Could you confirm SAI works correctly if it runs independently?&lt;BR /&gt;By debug mode you mean you have a debug session running, am I right? Is this problem still occurs if you don't run it with the debug session? &lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jan 2024 22:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1010-LPI2C-problem-using-debug-mode/m-p/1788244#M28442</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-01-12T22:14:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1010 LPI2C problem using debug mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1010-LPI2C-problem-using-debug-mode/m-p/1788665#M28456</link>
      <description>Hi Daniel,&lt;BR /&gt;I apologize I haven't signed the post as "solved"...&lt;BR /&gt;&lt;BR /&gt;Thanks anyway, Luigi</description>
      <pubDate>Mon, 15 Jan 2024 09:09:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1010-LPI2C-problem-using-debug-mode/m-p/1788665#M28456</guid>
      <dc:creator>LuigiV</dc:creator>
      <dc:date>2024-01-15T09:09:00Z</dc:date>
    </item>
  </channel>
</rss>