<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックMCUXpresso and RT1050 download and debug in SDRAM</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896979#M2843</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My application is larger than the on chip SRAM, so I am working on building a debug version that will load and run in SDRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a few useful threads and I may be down to the last issue.&amp;nbsp;RT1050_BriefOverview_v201.pdf was very helpful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To summarize some of the changes I made&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I updated the MCU Settings to add the SDRAM, and added a region for the last 2MB which is said to be uncached.&lt;/P&gt;&lt;P&gt;I made the SDRAM first in the list, I also adjusted the stack not to be at the exact top of SDRAM&lt;/P&gt;&lt;P&gt;I set&amp;nbsp;XIP_EXTERNAL_FLASH=0 and I also added&amp;nbsp;SKIP_SYSCLK_INIT&lt;/P&gt;&lt;P&gt;I added&amp;nbsp;RT1050_SDRAM_Init.scp as a connect script for the debugger to init SDRAM controller&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ISSUE&amp;gt;&amp;nbsp;I can not step over a break point, I can't even remove a BP I have hit without reloading the image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It feels like a cache issue, almost like the Debugger is not updating/flushing Instruction Cache&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load a project with a BP already enabled and before I run it I remove the BP, then it is not hit.&lt;/P&gt;&lt;P&gt;If I hit a BP I can use the debugger to move past it, skipping a statement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would rather not disable cache for the SDRAM, I am hoping there is a way to fix it in the debugger&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 May 2019 20:59:06 GMT</pubDate>
    <dc:creator>w2vy</dc:creator>
    <dc:date>2019-05-01T20:59:06Z</dc:date>
    <item>
      <title>MCUXpresso and RT1050 download and debug in SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896979#M2843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My application is larger than the on chip SRAM, so I am working on building a debug version that will load and run in SDRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a few useful threads and I may be down to the last issue.&amp;nbsp;RT1050_BriefOverview_v201.pdf was very helpful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To summarize some of the changes I made&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I updated the MCU Settings to add the SDRAM, and added a region for the last 2MB which is said to be uncached.&lt;/P&gt;&lt;P&gt;I made the SDRAM first in the list, I also adjusted the stack not to be at the exact top of SDRAM&lt;/P&gt;&lt;P&gt;I set&amp;nbsp;XIP_EXTERNAL_FLASH=0 and I also added&amp;nbsp;SKIP_SYSCLK_INIT&lt;/P&gt;&lt;P&gt;I added&amp;nbsp;RT1050_SDRAM_Init.scp as a connect script for the debugger to init SDRAM controller&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ISSUE&amp;gt;&amp;nbsp;I can not step over a break point, I can't even remove a BP I have hit without reloading the image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It feels like a cache issue, almost like the Debugger is not updating/flushing Instruction Cache&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load a project with a BP already enabled and before I run it I remove the BP, then it is not hit.&lt;/P&gt;&lt;P&gt;If I hit a BP I can use the debugger to move past it, skipping a statement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would rather not disable cache for the SDRAM, I am hoping there is a way to fix it in the debugger&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2019 20:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896979#M2843</guid>
      <dc:creator>w2vy</dc:creator>
      <dc:date>2019-05-01T20:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and RT1050 download and debug in SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896980#M2844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I went into board,c and modified&amp;nbsp;BOARD_ConfigMPU(void)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From:&lt;/P&gt;&lt;P&gt;#if defined(SDRAM_IS_SHAREABLE)&lt;BR /&gt; /* Region 7 setting: Memory with Normal type, is shareable, outer/inner write back */&lt;BR /&gt; MPU-&amp;gt;RBAR = ARM_MPU_RBAR(7, 0x80000000U);&lt;BR /&gt; MPU-&amp;gt;RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 1, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);&lt;BR /&gt;#else&lt;BR /&gt;/* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */&lt;BR /&gt; MPU-&amp;gt;RBAR = ARM_MPU_RBAR(7, 0x80000000U);&lt;BR /&gt; MPU-&amp;gt;RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if defined(SDRAM_IS_SHAREABLE)&lt;BR /&gt;/* Region 7 setting: Memory with Normal type, is shareable, outer/inner write back */&lt;BR /&gt;MPU-&amp;gt;RBAR = ARM_MPU_RBAR(7, 0x80000000U);&lt;BR /&gt;MPU-&amp;gt;RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 1, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);&lt;BR /&gt;#else&lt;BR /&gt;&lt;EM&gt;#if defined(SDRAM_IS_CACHEABLE)&lt;/EM&gt;&lt;BR /&gt;/* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */&lt;BR /&gt;MPU-&amp;gt;RBAR = ARM_MPU_RBAR(7, 0x80000000U);&lt;BR /&gt;MPU-&amp;gt;RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);&lt;BR /&gt;&lt;EM&gt;#endif&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;/* Region 7 setting: Memory with Normal type, not shareable, no cache */&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MPU-&amp;gt;RBAR = ARM_MPU_RBAR(7, 0x80000000U);&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MPU-&amp;gt;RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_32MB);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I matched the settings of the last 2MB which the docs describe as being non cached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I still have the same issue with not being able to step through BPs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So maybe I was wrong about the real issue...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2019 20:31:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896980#M2844</guid>
      <dc:creator>w2vy</dc:creator>
      <dc:date>2019-05-02T20:31:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and RT1050 download and debug in SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896981#M2845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;Tom Moulton&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;This is related to the cache and the access to the SDRAM. If you place the code in the SDRAM section that is noncacheable, you will see that this issue of stepping and breakpoints disappears. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;A Breakpoint by default is a software brkp, which is saved in the default RAM, you alternately could use a hardware breakpoint (right click and add breakpoint-&amp;gt;type: hardware).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;Hope this helps&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2019 23:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896981#M2845</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-05-07T23:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and RT1050 download and debug in SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896982#M2846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am seeing the opposite, Not disappearing BPs but ones I can't get rid of&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can try Hardware BPs. but those are typically limited in number.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you debug in SDRAM with software BPs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 15:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896982#M2846</guid>
      <dc:creator>w2vy</dc:creator>
      <dc:date>2019-05-10T15:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and RT1050 download and debug in SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896983#M2847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Tom Moulton &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Yes, sorry for my mistake, what I mean was the breakpoints DOESN'T disappears and you can't get rid of them.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Yes, I'm seeing the same as you, but the alternately for this is using HW BP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 21:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/896983#M2847</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-05-10T21:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and RT1050 download and debug in SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/1371280#M17135</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a very similar problem to this but using an RT1170, with MCUXpresso v11.4.0.&lt;BR /&gt;My program appears to run but:&lt;BR /&gt;- a) once a breakpoint is hit the program is not debuggable afterwards.&lt;BR /&gt;- b) I notice that my (ethernet) interupt callback function is not longer being called.&lt;/P&gt;&lt;P&gt;Before creating my own forum post, I have a few questions about the above.&lt;BR /&gt;w2vy says:&lt;BR /&gt;- "I updated the MCU Settings to add the SDRAM, and added a region for the last 2MB which is said to be uncached".&lt;BR /&gt;- How do I do this? I can split-off some SDRAM using the IDE's MCU Setting dialog, but how to make it uncached? Is that done via a linker script? Or via a code change?&lt;BR /&gt;- "I added RT1050_SDRAM_Init.scp as a connect script for the debugger to init SDRAM controller"&lt;BR /&gt;- I can't see an example of this for the RT1170, so I presume this is something we need to generate ourselves? Unfortunately that's not something I know how to do.&lt;BR /&gt;- Add "/* Region 7 setting: Memory with Normal type, not shareable, no cache */", etc. to BOARD_ConfigMPU().&lt;BR /&gt;- When I add a similar set of lines of code I get a SIGSTOP in MemManage_Handler().&lt;BR /&gt;- Note: If I replace the existing Region 7 lines (appears to be Region 9 on the RT1170) instead of adding them I don't get the crash.&lt;/P&gt;&lt;P&gt;I would be grateful for any help you can provide.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;</description>
      <pubDate>Mon, 15 Nov 2021 11:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MCUXpresso-and-RT1050-download-and-debug-in-SDRAM/m-p/1371280#M17135</guid>
      <dc:creator>robert_s</dc:creator>
      <dc:date>2021-11-15T11:06:34Z</dc:date>
    </item>
  </channel>
</rss>