<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピック回复： boot problem rt1064</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1783490#M28333</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227757"&gt;@tomerk&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP I.MXRT series.&lt;/P&gt;
&lt;P&gt;Can you help clarify here? What do you mean the CPU won't run when debugger is not used?&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Gavin&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jan 2024 08:16:05 GMT</pubDate>
    <dc:creator>Gavin_Jia</dc:creator>
    <dc:date>2024-01-05T08:16:05Z</dc:date>
    <item>
      <title>boot problem rt1064</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1783001#M28318</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I have a problem with the internal flash&amp;nbsp;&lt;SPAN&gt;boot,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;When i load it with the debugger&lt;SPAN&gt;&amp;nbsp;everything works fine but without it the CPU wont begin running.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The legs are set&lt;/P&gt;&lt;P&gt;boot_mode1= 1,&lt;/P&gt;&lt;P&gt;boot_mode0=0&lt;/P&gt;&lt;P&gt;and all the boot_cfg to 0&amp;nbsp;&lt;/P&gt;&lt;P&gt;what could be the issue?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jan 2024 11:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1783001#M28318</guid>
      <dc:creator>tomerk</dc:creator>
      <dc:date>2024-01-04T11:28:27Z</dc:date>
    </item>
    <item>
      <title>回复： boot problem rt1064</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1783490#M28333</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227757"&gt;@tomerk&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP I.MXRT series.&lt;/P&gt;
&lt;P&gt;Can you help clarify here? What do you mean the CPU won't run when debugger is not used?&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 08:16:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1783490#M28333</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-01-05T08:16:05Z</dc:date>
    </item>
    <item>
      <title>回复： boot problem rt1064</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1783941#M28348</link>
      <description>&lt;P&gt;some of the times when i give power nothing happens. In some cases the circuit turns on but probably goes straight into BOOT (one of the lights on the circuit lights up for me).&amp;nbsp; Only in this mode can I burn it and run the mcuxpresso DEBUGGER and then through the DEBUGGER it runs. As soon as I turn off the power and turn it back on, it returns to the states I wrote down.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 07 Jan 2024 08:39:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1783941#M28348</guid>
      <dc:creator>tomerk</dc:creator>
      <dc:date>2024-01-07T08:39:43Z</dc:date>
    </item>
    <item>
      <title>回复： boot problem rt1064</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1784031#M28350</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227757"&gt;@tomerk&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well!&lt;/P&gt;
&lt;P&gt;In your description it seems that image is flashed into RAM to run? Suggest you try deleting and re-importing one of the simplest demos: e.g. Hello_world. Also, switch to 5V DC_DC power supply.&lt;/P&gt;
&lt;P&gt;1. make sure SW7 is 0-0-1-0;&lt;BR /&gt;2. connect the jumper on J1 to 1-2 pin; (at this time the power supply is the 5V from the J1 port)&lt;BR /&gt;3. adjust SW1 to turn on the power supply switch;&lt;BR /&gt;4. flash IMAGE through J41;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 02:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1784031#M28350</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-01-08T02:48:18Z</dc:date>
    </item>
    <item>
      <title>回复： boot problem rt1064</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1784258#M28354</link>
      <description>&lt;P&gt;Hi, thanks for the response,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the module only and not the evk.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 08:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/boot-problem-rt1064/m-p/1784258#M28354</guid>
      <dc:creator>tomerk</dc:creator>
      <dc:date>2024-01-08T08:50:11Z</dc:date>
    </item>
  </channel>
</rss>