<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 回复： i.MX RT1060 Dual USB CDC Virtual Vcom Example Code</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1774278#M28003</link>
    <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;The uTasker project allows dual CDC device on both of the HSUSBs (as well as CDC device/host mixtures).&lt;/P&gt;&lt;P&gt;The attached binary is a complete project which shows two CDC devices on the MIMXRT1060-EVK - loadable via ISP:&lt;BR /&gt;- HSUSB1 can be connected to a terminal emulator and has a command line interface on it (in the USB menu the command "usb-serial" will also transform it into a USB-LPUART bridge with LPUART speed control via the terminal emulator setting - the LPUART is the one on the MIMXRT1060-EVK VCOM port).&lt;BR /&gt;- HSUSB2 can be connected to and just does a simple echo back of all received input.&lt;BR /&gt;&lt;BR /&gt;The complete solution is included in the project - &lt;A href="https://www.utasker.com/index.html" target="_blank"&gt;https://www.utasker.com/index.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;For our discounted i.MX and Kinetis stock availability see &lt;A href="https://www.utasker.com/Shop/semi.html" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.utasker.com/Shop/semi.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 14 Dec 2023 00:49:42 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2023-12-14T00:49:42Z</dc:date>
    <item>
      <title>i.MX RT1060 Dual USB CDC Virtual Vcom Example Code</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1771241#M27918</link>
      <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;&amp;nbsp; Is there an i.MX RT1060 Dual USB CDC Virtual Vcom example code for reference?Only single USB examples are found in the SDK.&lt;/P&gt;&lt;P&gt;claire&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Dec 2023 03:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1771241#M27918</guid>
      <dc:creator>claire_chen</dc:creator>
      <dc:date>2023-12-08T03:16:10Z</dc:date>
    </item>
    <item>
      <title>回复： i.MX RT1060 Dual USB CDC Virtual Vcom Example Code</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1771349#M27922</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181324"&gt;@claire_chen&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in I.MX RT series. I'd like to provide service for you.&lt;/P&gt;
&lt;P&gt;There is an example in the SDK of our partner EmbeddedArtists that should meet your needs, please refer to it. The path is : &lt;U&gt;&lt;EM&gt;\boards\evkbmimxrt1060\usb_examples\usb_device_composite_cdc_vcom_cdc_vcom&lt;/EM&gt;&lt;/U&gt;&lt;/P&gt;
&lt;P&gt;You can find this SDK here:&amp;nbsp;&lt;A href="http://imx.embeddedartists.com/#imxrt1062" target="_blank"&gt;http://imx.embeddedartists.com/#imxrt1062&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Fri, 08 Dec 2023 06:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1771349#M27922</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2023-12-08T06:42:11Z</dc:date>
    </item>
    <item>
      <title>回复： i.MX RT1060 Dual USB CDC Virtual Vcom Example Code</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1771433#M27925</link>
      <description>&lt;P&gt;&lt;FONT face="terminal,monaco" size="4"&gt;Hi &lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203261" target="_self"&gt;&lt;SPAN class=""&gt;Gavin_Jia&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;，&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="terminal,monaco" size="4"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm very sorry that I shouldn't have expressed myself clearly. &lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="terminal,monaco" size="4"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; What is needed is that both USB1 and USB2 are configured as CDC virtual serial ports, not USB1 CDC virtualized as 2 serial ports. Can you help me with this?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="terminal,monaco" size="4"&gt;&amp;nbsp;Claire&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Dec 2023 08:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1771433#M27925</guid>
      <dc:creator>claire_chen</dc:creator>
      <dc:date>2023-12-08T08:46:25Z</dc:date>
    </item>
    <item>
      <title>回复： i.MX RT1060 Dual USB CDC Virtual Vcom Example Code</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1774278#M28003</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;The uTasker project allows dual CDC device on both of the HSUSBs (as well as CDC device/host mixtures).&lt;/P&gt;&lt;P&gt;The attached binary is a complete project which shows two CDC devices on the MIMXRT1060-EVK - loadable via ISP:&lt;BR /&gt;- HSUSB1 can be connected to a terminal emulator and has a command line interface on it (in the USB menu the command "usb-serial" will also transform it into a USB-LPUART bridge with LPUART speed control via the terminal emulator setting - the LPUART is the one on the MIMXRT1060-EVK VCOM port).&lt;BR /&gt;- HSUSB2 can be connected to and just does a simple echo back of all received input.&lt;BR /&gt;&lt;BR /&gt;The complete solution is included in the project - &lt;A href="https://www.utasker.com/index.html" target="_blank"&gt;https://www.utasker.com/index.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;For our discounted i.MX and Kinetis stock availability see &lt;A href="https://www.utasker.com/Shop/semi.html" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.utasker.com/Shop/semi.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 00:49:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1060-Dual-USB-CDC-Virtual-Vcom-Example-Code/m-p/1774278#M28003</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2023-12-14T00:49:42Z</dc:date>
    </item>
  </channel>
</rss>