<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックimxrt1170 embedded wizard example issue</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1170-embedded-wizard-example-issue/m-p/1772223#M27938</link>
    <description>&lt;P&gt;I am using a custom board with IMXrt1170. I have run the graphics accelerator example in SDK 2.14.0&lt;/P&gt;&lt;P&gt;When EW_USE_FREE_RTOS flag is enabled, example runs very well. However, when the flag is disabled, it not.&lt;/P&gt;&lt;P&gt;I need that example with no FreeRtos. I want GPU2D, VGLite, to use directly on bare metal without RTOS.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Dec 2023 10:25:13 GMT</pubDate>
    <dc:creator>burhanhagi</dc:creator>
    <dc:date>2023-12-11T10:25:13Z</dc:date>
    <item>
      <title>imxrt1170 embedded wizard example issue</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1170-embedded-wizard-example-issue/m-p/1772223#M27938</link>
      <description>&lt;P&gt;I am using a custom board with IMXrt1170. I have run the graphics accelerator example in SDK 2.14.0&lt;/P&gt;&lt;P&gt;When EW_USE_FREE_RTOS flag is enabled, example runs very well. However, when the flag is disabled, it not.&lt;/P&gt;&lt;P&gt;I need that example with no FreeRtos. I want GPU2D, VGLite, to use directly on bare metal without RTOS.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 10:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1170-embedded-wizard-example-issue/m-p/1772223#M27938</guid>
      <dc:creator>burhanhagi</dc:creator>
      <dc:date>2023-12-11T10:25:13Z</dc:date>
    </item>
    <item>
      <title>Re: imxrt1170 embedded wizard example issue</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1170-embedded-wizard-example-issue/m-p/1772481#M27940</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201543"&gt;@burhanhagi&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Unfortunately, the Embedded Wizard examples for the RT1170 uses FreeRTOS.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Nonetheless, according to &lt;A href="https://doc.embedded-wizard.de/getting-started-mimxrt1170-evk" target="_blank"&gt;i.MX RT1170 - Embedded Wizard&lt;/A&gt;: "[…]a few additional settings can be configured directly within the&amp;nbsp;Makefile, like the usage of the FreeRTOS operating system."&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please take a look at the following community post: &lt;A href="https://ask.embedded-wizard.de/5911/choose-freertos-used-the-pxp-version-the-software-for-rt1170" target="_blank"&gt;How do I choose if FreeRTOS is used or not in the PXP version of the software for RT1170? - Ask Embedded Wizard&lt;/A&gt;?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;In case you still have some issues changing the EW_USE_FREE_RTOS=0 you could go to the .cproject and change it there.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Warm regards, Raul.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 18:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1170-embedded-wizard-example-issue/m-p/1772481#M27940</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-12-11T18:43:48Z</dc:date>
    </item>
  </channel>
</rss>