<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMXRT1052 eMMC 5.0 interface in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1052-eMMC-5-0-interface/m-p/1765176#M27781</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/185819"&gt;@AkshayPatil&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Technically the RT1052 does support eMMC 5.0 and 5.1, but only because of the fact that these standards are backward compatible. As stated on the following knowledge base article:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/EMMC-5-0-and-EMMC-5-1-work-on-i-MX6/ta-p/1118941" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/EMMC-5-0-and-EMMC-5-1-work-on-i-MX6/ta-p/1118941&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;The EMMC 4.5 or EMMC 5.0 /5.1 is backward-compatible with eMMC4.4, we can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance" "Booting from a eMMC 4.5 device or high version is not supported, boot ROM will fall back to the eMMC4.4 standard when a eMMC4.5 or high version capable device is detected.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;This was written in the context of a i.MX6 platform, but is also applicable to the i.MX RT family.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Tue, 28 Nov 2023 21:05:56 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2023-11-28T21:05:56Z</dc:date>
    <item>
      <title>iMXRT1052 eMMC 5.0 interface</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1052-eMMC-5-0-interface/m-p/1764833#M27776</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Does the iMXRT1052 chipset support or have compatibility with the eMMC 5.0 and 5.1 standard for embedded flash storage (eMMC)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;datasheet syas "Fully compliant with MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.5/4.2/4.3/4.4/4.41/ including high-capacity (size &amp;gt; 2 GB) cards HC MMC. "&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 10:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1052-eMMC-5-0-interface/m-p/1764833#M27776</guid>
      <dc:creator>AkshayPatil</dc:creator>
      <dc:date>2023-11-28T10:21:11Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1052 eMMC 5.0 interface</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1052-eMMC-5-0-interface/m-p/1765176#M27781</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/185819"&gt;@AkshayPatil&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Technically the RT1052 does support eMMC 5.0 and 5.1, but only because of the fact that these standards are backward compatible. As stated on the following knowledge base article:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/EMMC-5-0-and-EMMC-5-1-work-on-i-MX6/ta-p/1118941" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/EMMC-5-0-and-EMMC-5-1-work-on-i-MX6/ta-p/1118941&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;The EMMC 4.5 or EMMC 5.0 /5.1 is backward-compatible with eMMC4.4, we can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance" "Booting from a eMMC 4.5 device or high version is not supported, boot ROM will fall back to the eMMC4.4 standard when a eMMC4.5 or high version capable device is detected.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;This was written in the context of a i.MX6 platform, but is also applicable to the i.MX RT family.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 21:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1052-eMMC-5-0-interface/m-p/1765176#M27781</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-11-28T21:05:56Z</dc:date>
    </item>
  </channel>
</rss>