<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Setting Timer in Low Power Mode</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Setting-Timer-in-Low-Power-Mode/m-p/1763456#M27740</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;&lt;P&gt;Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note &lt;A href="https://www.nxp.com/docs/en/application-note/AN13104.pdf" target="_blank" rel="noopener"&gt;AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature&lt;/A&gt;. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.&lt;/P&gt;&lt;P&gt;Hope it helps you.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
    <pubDate>Fri, 24 Nov 2023 17:08:41 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2023-11-24T17:08:41Z</dc:date>
    <item>
      <title>Setting Timer in Low Power Mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Setting-Timer-in-Low-Power-Mode/m-p/1762760#M27708</link>
      <description>&lt;P&gt;I use imxrt1176, can I set timer to wake up mcu for 24 hours ?&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 13:49:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Setting-Timer-in-Low-Power-Mode/m-p/1762760#M27708</guid>
      <dc:creator>frozen</dc:creator>
      <dc:date>2023-11-23T13:49:44Z</dc:date>
    </item>
    <item>
      <title>Re: Setting Timer in Low Power Mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Setting-Timer-in-Low-Power-Mode/m-p/1763456#M27740</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;&lt;P&gt;Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note &lt;A href="https://www.nxp.com/docs/en/application-note/AN13104.pdf" target="_blank" rel="noopener"&gt;AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature&lt;/A&gt;. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.&lt;/P&gt;&lt;P&gt;Hope it helps you.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 17:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Setting-Timer-in-Low-Power-Mode/m-p/1763456#M27740</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-11-24T17:08:41Z</dc:date>
    </item>
  </channel>
</rss>