<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックUsing FlexSPI driver with edma and polling</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-FlexSPI-driver-with-edma-and-polling/m-p/1755444#M27525</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using MIMXRT1170-EVK board with MCUXpresso IDE. I want to use FlexSPI driver with edma and polling.&amp;nbsp;I will use edma and polling under different conditions. That's why I need to create an init process suitable for both of them.After DMA init, I disable the I and D cache memories to init the nor flash. Afterwards, I check whether the flexspi bus is idle or not. However, although there is never an idle when the I and D cache are disabled, it becomes an idle only if the D cache is disabled and the code continues. What could be the reason for this?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-11-10 10-47-56.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249355iFFD23FE50165C220/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot from 2023-11-10 10-47-56.png" alt="Screenshot from 2023-11-10 10-47-56.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SpeedyGonzalesss_0-1699602504057.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249356i7C158F580D9AE7A4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SpeedyGonzalesss_0-1699602504057.png" alt="SpeedyGonzalesss_0-1699602504057.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
    <pubDate>Fri, 10 Nov 2023 07:49:28 GMT</pubDate>
    <dc:creator>SpeedyGonzalesss</dc:creator>
    <dc:date>2023-11-10T07:49:28Z</dc:date>
    <item>
      <title>Using FlexSPI driver with edma and polling</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-FlexSPI-driver-with-edma-and-polling/m-p/1755444#M27525</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using MIMXRT1170-EVK board with MCUXpresso IDE. I want to use FlexSPI driver with edma and polling.&amp;nbsp;I will use edma and polling under different conditions. That's why I need to create an init process suitable for both of them.After DMA init, I disable the I and D cache memories to init the nor flash. Afterwards, I check whether the flexspi bus is idle or not. However, although there is never an idle when the I and D cache are disabled, it becomes an idle only if the D cache is disabled and the code continues. What could be the reason for this?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-11-10 10-47-56.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249355iFFD23FE50165C220/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot from 2023-11-10 10-47-56.png" alt="Screenshot from 2023-11-10 10-47-56.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SpeedyGonzalesss_0-1699602504057.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249356i7C158F580D9AE7A4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SpeedyGonzalesss_0-1699602504057.png" alt="SpeedyGonzalesss_0-1699602504057.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Fri, 10 Nov 2023 07:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-FlexSPI-driver-with-edma-and-polling/m-p/1755444#M27525</guid>
      <dc:creator>SpeedyGonzalesss</dc:creator>
      <dc:date>2023-11-10T07:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using FlexSPI driver with edma and polling</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-FlexSPI-driver-with-edma-and-polling/m-p/1761372#M27682</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I suggest you disable I-cache after calling flash init so it functions like the SDK example.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 01:23:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-FlexSPI-driver-with-edma-and-polling/m-p/1761372#M27682</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-11-22T01:23:26Z</dc:date>
    </item>
  </channel>
</rss>