<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: After HyperRAM initialization,the initial values in memory are not 0</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/After-HyperRAM-initialization-the-initial-values-in-memory-are/m-p/1754075#M27484</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I just initialized the SDRAM on my board with the SEMC interface, and I'm facing the same issue where the initial value is not zero. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, what's strange is that on another boards I designed with the same SDRAM circuit, after initialization, the initial value was always zero. This makes me think it might be a hardware issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But in fact, this does not affect the normal use of these memories, and they can be read and written correctly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 08 Nov 2023 08:59:27 GMT</pubDate>
    <dc:creator>Vinos</dc:creator>
    <dc:date>2023-11-08T08:59:27Z</dc:date>
    <item>
      <title>After HyperRAM initialization,the initial values in memory are not 0</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/After-HyperRAM-initialization-the-initial-values-in-memory-are/m-p/1744971#M27303</link>
      <description>&lt;P&gt;Chip: I.MX RT1176&lt;/P&gt;&lt;P&gt;I'm using two HyperRAM modules, one from Cypress with 32M and the other from ISSI with 64M. They are pin-to-pin compatible and both are connected to the FlexSPI1's Secondary Group. After initialization, the initial values in memory are not all zeros; most are zero, but some have values like 0x0a0a0a0a. The initial memory values for both chips seem similar.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Now, I have connected a 64M HyperRAM module of the same model as the 32M Cypress&amp;nbsp;one(the only difference is the memory size) to FlexSPI1's Primary Group. After initialization, the memory is mostly filled with 0xAAAAAAAA and some 0x5A5A5A5A, with very few zeros.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Although the initial values appear unusual, I have tested write-read operations on the HyperRAM, and there don't seem to be any issues. The memory can be read from and written to normally.&lt;/P&gt;&lt;P&gt;So, I'm suspecting if the initial memory values of the HyperRAM are related to the FlexSPI configuration?&lt;/P&gt;</description>
      <pubDate>Tue, 24 Oct 2023 03:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/After-HyperRAM-initialization-the-initial-values-in-memory-are/m-p/1744971#M27303</guid>
      <dc:creator>Vinos</dc:creator>
      <dc:date>2023-10-24T03:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: After HyperRAM initialization,the initial values in memory are not 0</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/After-HyperRAM-initialization-the-initial-values-in-memory-are/m-p/1750601#M27400</link>
      <description>&lt;P&gt;It is likely that this is done during initialization. Is there any other device connected to the same FlexSPI interface?&amp;nbsp;&lt;BR /&gt;Specifically, how is init implemented? Are you using SDK API?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 02 Nov 2023 00:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/After-HyperRAM-initialization-the-initial-values-in-memory-are/m-p/1750601#M27400</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-11-02T00:11:13Z</dc:date>
    </item>
    <item>
      <title>Re: After HyperRAM initialization,the initial values in memory are not 0</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/After-HyperRAM-initialization-the-initial-values-in-memory-are/m-p/1754075#M27484</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I just initialized the SDRAM on my board with the SEMC interface, and I'm facing the same issue where the initial value is not zero. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, what's strange is that on another boards I designed with the same SDRAM circuit, after initialization, the initial value was always zero. This makes me think it might be a hardware issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But in fact, this does not affect the normal use of these memories, and they can be read and written correctly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 08:59:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/After-HyperRAM-initialization-the-initial-values-in-memory-are/m-p/1754075#M27484</guid>
      <dc:creator>Vinos</dc:creator>
      <dc:date>2023-11-08T08:59:27Z</dc:date>
    </item>
  </channel>
</rss>